1. Usage[edit source]
The EcosystemRelease/Components template returns the version of all software components delivered by an ecosystem release revision of the flow associated with this wiki (e.g. v1.y.z ,or v2.y.z, or...).
Usage: {{EcosystemRelease/Components | revision=<revision>}}
Where:
- <revision> is the mandatory revision of the ecosystem release, for which the version of all software components is requested.
- The possible values for this parameter are available in the EcosystemRelease/Revision template.
The returned value is:
- a string that contains the version of all the software components delivered by the ecosystem release revision, in a form that is usable by a tooltip.
- "unknown revision", if <revision> is not supported.
This template relies on the EcosystemRelease/Component template.
2. Basic examples[edit source]
You type | You get |
---|---|
Components version for v5.0.0 revision requested
{{EcosystemRelease/Components | revision=5.0.0}} |
Main software components: Linux kernel v6.1-stm32mp-r1 (v6.1.28) U-Boot v2022.10-stm32mp-r1 TF-A v2.8-stm32mp-r1 OP-TEE 3.19.0-stm32mp-r1 STM32CubeMP1 Package v1.6.0 OpenEmbedded v4.2.1 (Mickledore) |
Components version for v4.1.0 revision requested
{{EcosystemRelease/Components | revision=4.1.0}} |
Main software components: Linux kernel v5.15-stm32mp-r2 (v5.15.67) U-Boot v2021.10-stm32mp-r2 TF-A v2.6-stm32mp-r2 OP-TEE 3.16.0-stm32mp-r2 STM32CubeMP1 Package v1.6.0 OpenEmbedded v4.0.4 (Kirkstone) |
Components version for the latest revision requested
{{EcosystemRelease/Components | revision=latest}} |
Main software components: Linux kernel v6.1-stm32mp-r2 (v6.1.82) U-Boot v2022.10-stm32mp-r2 TF-A v2.8-stm32mp-r2 OP-TEE 3.19.0-stm32mp-r2 unknown revision OpenEmbedded v4.2.4 (Mickledore) |
3. More examples[edit source]
You type | You get |
---|---|
Components version for vx.0.0 revision (legacy) requested
{{EcosystemRelease/Components | revision=x.0.0}} |
Main software components: Linux kernel vx.y-stm32mp-r0 (vx.y.z) U-Boot vx.y-stm32mp-r0 TF-A vx.y-stm32mp-r0 OP-TEE vx.y.z-stm32mp-r0 STM32CubeMP1 Package vx.y.z OpenEmbedded vx.y.z (codename) Android vx.y.z |
Components version for vx.1.0 revision (latest) requested
{{EcosystemRelease/Components | revision=x.1.0}} |
Main software components: Linux kernel vx.y-stm32mp-r0 (vx.y.z) U-Boot vx.y-stm32mp-r0 TF-A vx.y-stm32mp-r0 OP-TEE vx.y.z-stm32mp-r0 STM32CubeMP1 Package vx.y.z OpenEmbedded vx.y.z (codename) Android vx.y.z |
Components version for vx.2.0 revision (next) requested
{{EcosystemRelease/Components | revision=x.2.0}} |
Main software components: Linux kernel vx.y-stm32mp-r0 (vx.y.z) U-Boot vx.y-stm32mp-r0 TF-A vx.y-stm32mp-r0 OP-TEE vx.y.z-stm32mp-r0 STM32CubeMP1 Package vx.y.z OpenEmbedded vx.y.z (codename) Android vx.y.z |
Components version for v0.y.0 revision (former) requested
{{EcosystemRelease/Components | revision=0.y.0}} |
Main software components: unknown revision unknown revision unknown revision unknown revision unknown revision unknown revision unknown revision |
Unspecified revision
{{EcosystemRelease/Components}} |
Main software components: unknown revision |
Unknown revision
{{EcosystemRelease/Components | revision=10.20.30}} |
Main software components: unknown revision |
4. Code[edit source]
Main software components: unknown revision