STM32MP135x-DK - board connections

Revision as of 15:42, 30 March 2022 by Registered User
Renaming.png This page is a candidate for renaming (move).
The requested new name is: STM32MP135F-DK - board connections .
The supplied reason is: As far as I could understand, there will be no other tiny wildcat Discovery kit. This is of course only my tech writer's opinion and must probably be verified. Last minute!!! The RPN STM32MP135D-DK was just created in PRMIS. Contrary to the guidance given by the STM32MP135F-DK doc owner, there might be several kits in the line after all. The page renaming is probably not needed. .
-- Registered User (-) 20:51, 29 March 2022 (CEST).
Wiki maintainers: remember to update the pages that link this page before renaming (moving) it.

This article presents the recommended connections to start with the STM32MP135x-DK Discovery kit. It is valid for the STM32MP135F-DK Discovery kit: the part numbers are specified in the STM32MP13 microprocessor part numbers article.

Warning white.png Warning
To start the board successfully, it is recommended to go through the corresponding Starter Package article: Category:Starter Package


MB1635 mother board :STM32MP135F 11x11, PMIC, DDR3MB1723 camera moduleCamera module flat cablemicroSD™ card slotEthernet 2 → NetworkEthernet 1 → NetworkUSB Micro-B (STLINK-V3E) → PC Virtual COM port and debugUSB Type-C© (power 5V-3A)USB Type-C© (DRP)1st dual USB Type-A (host) → keyboard, mouse or USB driver2nd dual USB Type-A (host) → keyboard, mouse or USB driverReset button
STM32MP135F-DK Discovery kit connections. (picture is not contractual)