![]() |
Coming soon |
1. Generate X-LINUX-AZURE OpenSTLinux distribution[edit source]
With the following procedure, you can generate the complete distribution enabling the X-LINUX-AZURE Expansion Package.
This procedure is mandatory to use TPM on the X-LINUX-AZURE Expansion Package.
1.1. Download the Distribution Package[edit source]
- Install the OpenSTLinux Distribution Package by following the dedicated article (STM32MPU Distribution Package) but do not initialize the OpenEmbedded environment (do not source the envsetup.sh).
1.2. Install X-LINUX-AZURE environment[edit source]
- Clone the meta-st-x-linux-azure git repository
cd <Distribution Package installation directory>/layers/meta-st git clone https://github.com/STMicroelectronics/meta-st-x-linux-azure.git -b v5.1.0
- Clone the meta-st-x-linux-tpm git repository
cd <Distribution Package installation directory>/layers/meta-st git clone https://github.com/STMicroelectronics/meta-st-x-linux-tpm.git -b 5.1.0
- Clone the meta-iotedge git repository and change layer compatibility
cd <Distribution Package installation directory>/layers git clone https://github.com/Azure/meta-iotedge.git -b main sed -i "s/kirkstone/mickledore/g" meta-iotedge/conf/layer.conf
- Clone the meta-virtualization git repository
cd <Distribution Package installation directory>/layers git clone https://git.yoctoproject.org/meta-virtualization -b mickledore
- Clone the meta-rust git repository
cd <Distribution Package installation directory>/layers git clone https://github.com/meta-rust/meta-rust -b master
- Clone the meta-security git repository
cd <Distribution Package installation directory>/layers git clone https://git.yoctoproject.org/meta-security -b mickledore
- For a new environment
Source the build environment with the correct board and layers:
cd <Distribution Package installation directory>
MACHINE=stm32mp2 DISTRO=openstlinux-weston BSP_DEPENDENCY='layers/meta-st/meta-st-x-linux-tpm layers/meta-st/meta-st-x-linux-azure layers/meta-iotedge layers/meta-virtualization layers/meta-rust' source layers/meta-st/scripts/envsetup.sh
- For an already installed environment
Add the layers to the Yocto environment:
cd <Distribution Package installation directory> source layers/meta-st/scripts/envsetup.sh bitbake-layers add-layer ../layers/meta-st/meta-st-x-linux-azure/ ../layers/meta-st/meta-st-x-linux-tpm/ ../layers/meta-iotedge/ ../layers/meta-security ../layers/meta-virtualization ../layers/meta-rust
1.3. Build the image[edit source]
bitbake st-image-azure
1.4. Program the built image[edit source]
Follow this link to see how to program the built image.
2. Main software modifications[edit source]
Through the X-LINUX-AZURE Distribution Package, the OpenSTLinux distribution is mainly changed at two levels:
- The Linux® kernel configuration and Device tree level with the X-LINUX-TPM Expansion Package integration.
- User space bringing necessary libraries and tools to use Azure IoT Edge, OP-TEE, and the TPM expansion board features.