1. Usage[edit source]
The X-LINUXRelease/Revision template returns the version of an expansion package delivered on top of an ecosystem release revision of the flow associated with this wiki.
Usage: {{X-LINUXRelease/Revision | revision=<revision> | name=<name> | type=<type>}}
Where:
- <revision> is the mandatory revision of the ecosystem release, on top of which the expansion package is delivered.
- The possible values for this parameter are available in the EcosystemRelease/Revision template.
- <name> is the mandatory name of the expansion package delivered on top of the ecosystem release revision, for which the version is requested. The possible values are:
- AI
- AWS
- <type> is the optional parameter that allows to select the way the version is displayed. Per default (if <type> is not set), the full name of the expansion package version (e.g., "X-LINUX-AI vx.y.z") is displayed. The possible values for <type> are:
- tag: the expansion package tag (e.g., "vx.y.z") is displayed
- release: the expansion package release (e.g., "x.y.z") is displayed
The returned value is:
- a string that contains the version of the expansion package delivered on top of the ecosystem release revision.
- an empty string, if the expansion package is not delivered on top of the ecosystem release revision.
- "unknown revision", if <revision> is not supported.
- "unknown expansion package", if <name> is not supported.
2. Basic examples[edit source]
You type | You get |
---|---|
All expansion packages on top of the v5.0.0 revision requested
Full names:<br /> {{X-LINUXRelease/Revision | revision=5.0.0 | name=AI}}<br /> Tag names:<br /> {{X-LINUXRelease/Revision | revision=5.0.0 | name=AI | type=tag}}<br /> Release names:<br /> {{X-LINUXRelease/Revision | revision=5.0.0 | name=AI | type=release}} |
Full names: |
All expansion packages on top of the latest revision requested
Full names:<br /> {{X-LINUXRelease/Revision | revision=latest | name=AI}}<br /> Tag names:<br /> {{X-LINUXRelease/Revision | revision=latest | name=AI | type=tag}}<br /> Release names:<br /> {{X-LINUXRelease/Revision | revision=latest | name=AI | type=release}} |
Full names: |
All expansion packages on top of the v5.0.0 revision requested
Full names:<br /> {{X-LINUXRelease/Revision | revision=5.0.0 | name=AWS}}<br /> Tag names:<br /> {{X-LINUXRelease/Revision | revision=5.0.0 | name=AWS | type=tag}}<br /> Release names:<br /> {{X-LINUXRelease/Revision | revision=5.0.0 | name=AWS | type=release}} |
Full names: |
All expansion packages on top of the latest revision requested
Full names:<br /> {{X-LINUXRelease/Revision | revision=latest | name=AWS}}<br /> Tag names:<br /> {{X-LINUXRelease/Revision | revision=latest | name=AWS | type=tag}}<br /> Release names:<br /> {{X-LINUXRelease/Revision | revision=latest | name=AWS | type=release}} |
Full names: |
All expansion packages on top of the v1.0.0 revision requested
Full names:<br /> {{X-LINUXRelease/Revision | revision=1.0.0 | name=QT}}<br /> Tag names:<br /> {{X-LINUXRelease/Revision | revision=1.0.0 | name=QT| type=tag}}<br /> Release names:<br /> {{X-LINUXRelease/Revision | revision=1.0.0 | name=QT| type=release}} |
Full names: |
All expansion packages on top of the latest revision requested
Full names:<br /> {{X-LINUXRelease/Revision | revision=latest | name=QT}}<br /> Tag names:<br /> {{X-LINUXRelease/Revision | revision=latest | name=QT| type=tag}}<br /> Release names:<br /> {{X-LINUXRelease/Revision | revision=latest | name=QT| type=release}} |
Full names: |
3. More examples[edit source]
You type | You get |
---|---|
All expansion packages on top of the vx.0.0 revision (legacy) requested
{{X-LINUXRelease/Revision | revision=x.0.0 | name=AI}}<br /> {{X-LINUXRelease/Revision | revision=x.0.0 | name=AI | type=tag}}<br /> {{X-LINUXRelease/Revision | revision=x.0.0 | name=AI | type=release}} |
Full names: |
All expansion packages on top of the vx.1.0 revision (latest) requested
{{X-LINUXRelease/Revision | revision=x.1.0 | name=AI}}<br /> {{X-LINUXRelease/Revision | revision=x.1.0 | name=AI | type=tag}}<br /> {{X-LINUXRelease/Revision | revision=x.1.0 | name=AI | type=release}} |
X-LINUX-AI vx.y.z |
All expansion packages on top of the vx.2.0 revision (next) requested
{{X-LINUXRelease/Revision | revision=x.2.0 | name=AI}}<br /> {{X-LINUXRelease/Revision | revision=x.2.0 | name=AI | type=tag}}<br /> {{X-LINUXRelease/Revision | revision=x.2.0 | name=AI | type=release}} |
X-LINUX-AI vx.y.z |
All expansion packages on top of the v0.y.0 revision (former) requested
{{X-LINUXRelease/Revision | revision=0.y.0 | name=AI}}<br /> {{X-LINUXRelease/Revision | revision=0.y.0 | name=AI | type=tag}}<br /> {{X-LINUXRelease/Revision | revision=0.y.0 | name=AI | type=release}} |
unknown revision |
All expansion packages on top of an unspecified revision requested
{{X-LINUXRelease/Revision | name=AI}}<br /> {{X-LINUXRelease/Revision | name=AI | type=tag}}<br /> {{X-LINUXRelease/Revision | name=AI | type=release}} |
unknown revision |
All expansion packages on top of an unknown revision requested
{{X-LINUXRelease/Revision | revision=10.20.30 | name=AI}}<br /> {{X-LINUXRelease/Revision | revision=10.20.30 | name=AI | type=tag}}<br /> {{X-LINUXRelease/Revision | revision=10.20.30 | name=AI | type=release}} |
unknown revision |
Unspecified expansion package
{{X-LINUXRelease/Revision | revision=x.0.0}}<br /> {{X-LINUXRelease/Revision | revision=x.0.0 | type=tag}}<br /> {{X-LINUXRelease/Revision | revision=x.0.0 | type=release}} |
unknown expansion package |
Unknown expansion package
{{X-LINUXRelease/Revision | revision=x.0.0 | name=not supported}}<br /> {{X-LINUXRelease/Revision | revision=x.0.0 | name=not supported | type=tag}}<br /> {{X-LINUXRelease/Revision | revision=x.0.0 | name=not supported | type=release}} |
unknown expansion package |
Unknown value for type: the full name is displayed
{{X-LINUXRelease/Revision | revision=x.0.0 | name=AI | type=version}}
|
X-LINUX-AI vx.y.z |
4. Code[edit source]
unknown expansion package