1. Usage
The PC$ template is used to prefix a command that must be executed on an host PC, with an host-specific prompt.
Thanks to the pc-prompt
class defined in MediaWiki:Common.css, a double (or triple) click to select the command doesn't select the prompt.
Usage: {{PC$}}
2. Basic examples
You type | You get |
---|---|
ls test command executed on the host PC
{{PC$}}ls test<br>
test1.txt test2.txt
|
ls test |
3. More examples
You type | You get | ||
---|---|---|---|
2 commands executed on the host PC and preformatted text block (space at the beginning of each line)
{{PC$}}ls test
test1.txt test2.txt
{{PC$}}cat test/test1.txt
This is a test
|
ls test
test1.txt test2.txt
cat test/test1.txt
This is a test
| ||
Command executed on the host PC and preformatted text block (space at the beginning of each line)
{{PC$}}ls test
test1.txt test2.txt
|
ls test
test1.txt test2.txt
| ||
Long command executed on the host PC and preformatted text block (space at the beginning of each line)
{{PC$}}this is a so long command executed on the host PC that a horizontal scrolling bar is needed
|
this is a so long command executed on the host PC that a horizontal scrolling bar is needed
| ||
Template used within another public message box template
{{Info |
Message before the command
{{PC$}}ls test
test1.txt test2.txt
Message after the command
}}
|
| ||
Template used within another protected message box template
{{InternalInfo |
Message before the command
{{PC$}}ls test
test1.txt test2.txt
Message after the command
}}
|
4. Maintenance
This template is a template common to all ST wikis.
Modifications must be done into the WikiModel. They must be reviewed by all ST wikis maintainers.
When approved, the template can be pushed/merged towards all ST wikis.
5. Code