1. Usage[edit source]
The GDB$ template is used to prefix a command that must be executed on GDB, with a GDB-specific prompt.
Thanks to the gdb-prompt
class defined in MediaWiki:Common.css, a double (or triple) click to select the command doesn't select the prompt.
GDB$}}Usage: {{
2. Basic examples[edit source]
You type | You get |
---|---|
info break command executed on GDB
GDB$}}show listsize<br> Number of source lines gdb will list by default is 10.{{ |
show listsize |
3. More examples[edit source]
You type | You get | ||
---|---|---|---|
2 commands executed on GDB and preformatted text block (space at the beginning of each line)
GDB$}}show listsize Number of source lines gdb will list by default is 10. {{GDB$}}continue{{ |
show listsize
Number of source lines gdb will list by default is 10.
continue
| ||
Command executed on GDB and preformatted text block (space at the beginning of each line)
GDB$}}show listsize Number of source lines gdb will list by default is 10.{{ |
show listsize
Number of source lines gdb will list by default is 10.
| ||
Long command executed on GDB and preformatted text block (space at the beginning of each line)
GDB$}}this is a so long command executed on GDB that a horizontal scrolling bar is needed{{ |
GDB that a horizontal scrolling bar is neededthis is a so long command executed on | ||
Template used within another public message box template
GDB$}}show listsize Number of source lines gdb will list by default is 10. Message after the command }}{{Info | Message before the command {{ |
| ||
Template used within another protected message box template
GDB$}}show listsize Number of source lines gdb will list by default is 10. Message after the command }}{{InternalInfo | Message before the command {{ |
4. Maintenance[edit source]
This template is a template common to all ST wikis.
Modifications must be done into the WikiModel. They must be reviewed by all ST wikis maintainers.
When approved, the template can be pushed/merged towards all ST wikis.
5. Code[edit source]