Registered User mNo edit summary |
Registered User (Merge articles) |
||
Line 14: | Line 14: | ||
* {{HighlightParam|<path>}} is the '''mandatory''' relative path of the document from the root URL of the domain. The root URLs are: | * {{HighlightParam|<path>}} is the '''mandatory''' relative path of the document from the root URL of the domain. The root URLs are: | ||
** '''https://www.kernel.org/doc/html/''' for the Linux kernel domain | ** '''https://www.kernel.org/doc/html/''' for the Linux kernel domain | ||
** '''https:// | ** '''https://docs.yoctoproject.org/''' for the Yocto Project domain | ||
** '''https://docs.aws.amazon.com/greengrass/''' for the AWS IoT Greengrass domain | ** '''https://docs.aws.amazon.com/greengrass/''' for the AWS IoT Greengrass domain | ||
** '''https://u-boot.readthedocs.io/en''' for the U-Boot domain | ** '''https://u-boot.readthedocs.io/en''' for the U-Boot domain | ||
* {{HighlightParam|<link text>}} is an '''optional''' link text (text that is displayed instead of the URL). | * {{HighlightParam|<link text>}} is an '''optional''' link text (text that is displayed instead of the URL). | ||
Line 24: | Line 22: | ||
* {{HighlightParam|<version>}} is an '''optional''' version number (branch or tag) if the default one doesn't fit. Per default, the URL points to: | * {{HighlightParam|<version>}} is an '''optional''' version number (branch or tag) if the default one doesn't fit. Per default, the URL points to: | ||
** the '''v5.10''' branch of the Linux kernel | ** the '''v5.10''' branch of the Linux kernel | ||
** the '''3.1. | ** the '''3.1.11''' branch of the Yocto Project | ||
** the '''latest''' branch of the AWS IoT Greengrass | ** the '''latest''' branch of the AWS IoT Greengrass | ||
** the '''v2020.10''' branch of the U-Boot Documentation | ** the '''v2020.10''' branch of the U-Boot Documentation | ||
Line 154: | Line 152: | ||
'''Yocto Project''': | '''Yocto Project''': | ||
<nowiki> | <nowiki> | ||
[https:// | [https://docs.yoctoproject.org/{{#if: {{{version|}}}|{{#replace:{{{version|}}}| |}}|3.1.11}}/{{#replace:{{{path|}}}| |}} {{#if: {{{text|}}}|{{{text}}}|{{{path}}}}}{{#if: {{{version|}}}| (v{{#replace:{{{version|}}}| |}})}}] | ||
</nowiki> | </nowiki> | ||
Line 169: | Line 167: | ||
</noinclude>{{#switch: {{{domain}}} | </noinclude>{{#switch: {{{domain}}} | ||
| Linux kernel = [https://www.kernel.org/doc/html/{{#if: {{{version|}}}|v{{#replace:{{{version|}}}| |}}|v5.10}}/{{#replace:{{{path|}}}| |}} {{#if: {{{text|}}}|{{{text}}}|{{{path}}}}}{{#if: {{{version|}}}| (v{{#replace:{{{version|}}}| |}})}}] | | Linux kernel = [https://www.kernel.org/doc/html/{{#if: {{{version|}}}|v{{#replace:{{{version|}}}| |}}|v5.10}}/{{#replace:{{{path|}}}| |}} {{#if: {{{text|}}}|{{{text}}}|{{{path}}}}}{{#if: {{{version|}}}| (v{{#replace:{{{version|}}}| |}})}}] | ||
| Yocto Project = [https:// | | Yocto Project = [https://docs.yoctoproject.org/{{#if: {{{version|}}}|{{#replace:{{{version|}}}| |}}|3.1.11}}/{{#replace:{{{path|}}}| |}} {{#if: {{{text|}}}|{{{text}}}|{{{path}}}}}{{#if: {{{version|}}}| (v{{#replace:{{{version|}}}| |}})}}] | ||
| AWS Greengrass = [https://docs.aws.amazon.com/greengrass/{{#if: {{{version|}}}|{{#replace:{{{version|}}}| |}}|latest}}/{{#replace:{{{path|}}}| |}} {{#if: {{{text|}}}|{{{text}}}|{{{path}}}}}{{#if: {{{version|}}}| (v{{#replace:{{{version|}}}| |}})}}] | | AWS Greengrass = [https://docs.aws.amazon.com/greengrass/{{#if: {{{version|}}}|{{#replace:{{{version|}}}| |}}|latest}}/{{#replace:{{{path|}}}| |}} {{#if: {{{text|}}}|{{{text}}}|{{{path}}}}}{{#if: {{{version|}}}| (v{{#replace:{{{version|}}}| |}})}}] | ||
| U-Boot= [https://u-boot.readthedocs.io/en/{{#if: {{{version|}}}|{{#replace:{{{version|}}}| |}}|v2020.10}}/{{#replace:{{{path|}}}| |}} {{#if: {{{text|}}}|{{{text}}}|{{{path}}}}}{{#if: {{{version|}}}| (v{{#replace:{{{version|}}}| |}})}}] | | U-Boot= [https://u-boot.readthedocs.io/en/{{#if: {{{version|}}}|{{#replace:{{{version|}}}| |}}|v2020.10}}/{{#replace:{{{path|}}}| |}} {{#if: {{{text|}}}|{{{text}}}|{{{path}}}}}{{#if: {{{version|}}}| (v{{#replace:{{{version|}}}| |}})}}] | ||
| {{Highlight| Unsupported domain!}} | | {{Highlight| Unsupported domain!}} | ||
}} | }} |
Revision as of 17:48, 22 November 2021
1. Usage[edit source]
The DocSource template is used to indicate the URL of any Linux® kernel, Yocto Project, and AWS IoT Greengrass document used in this wiki.
<domain> | path=<path> | text=<link text> | version=<version>}}Usage: {{DocSource | domain=
- Where:
- <domain> is the mandatory string that identifies the domain of the document. The possible values are:
- Linux kernel: the document belongs to the Linux kernel domain.
- Yocto Project: the document belongs to the Yocto Project domain.
- AWS Greengrass: the document belongs to the AWS IoT Greengrass domain.
- U-Boot: the document belongs to U-Boot domain
- <path> is the mandatory relative path of the document from the root URL of the domain. The root URLs are:
- https://www.kernel.org/doc/html/ for the Linux kernel domain
- https://docs.yoctoproject.org/ for the Yocto Project domain
- https://docs.aws.amazon.com/greengrass/ for the AWS IoT Greengrass domain
- https://u-boot.readthedocs.io/en for the U-Boot domain
- <link text> is an optional link text (text that is displayed instead of the URL).
- <version> is an optional version number (branch or tag) if the default one doesn't fit. Per default, the URL points to:
- the v5.10 branch of the Linux kernel
- the 3.1.11 branch of the Yocto Project
- the latest branch of the AWS IoT Greengrass
- the v2020.10 branch of the U-Boot Documentation
2. Basic examples[edit source]
You type | You get |
---|---|
Linux kernel
Linux kernel | path=crypto/index.html}}<br /> 2- {{DocSource | domain=Linux kernel | path=gpu/drm-uapi.html}}1- {{DocSource | domain= |
|
Yocto Project
Yocto Project | path=overview-manual/overview-manual.html}}<br /> 2- {{DocSource | domain=Yocto Project | path=brief-yoctoprojectqs/brief-yoctoprojectqs.html}}1- {{DocSource | domain= |
1- overview-manual/overview-manual.html |
AWS IoT Greengrass
1- {{DocSource | domain=AWS Greengrass | path=developerguide/what-is-gg.html}}<br />
2- {{DocSource | domain=AWS Greengrass | path=developerguide/device-config-setup.html}}
|
1- developerguide/what-is-gg.html |
U-Boot
U-Boot | path=index.html}}<br /> 2- {{DocSource | domain=U-Boot | path=build/index.html}}1- {{DocSource | domain= |
1- index.html |
3. More examples[edit source]
You type | You get |
---|---|
Linux kernel
Linux kernel | path=crypto/index.html}}<br /> 2- {{DocSource | domain=Linux kernel | path=crypto/index.html | text=Linux Kernel Crypto API}}<br /> 3- {{DocSource | domain=Linux kernel | path=crypto/index.html | version=4.19}}<br /> 4- {{DocSource | domain=Linux kernel | path=crypto/index.html | text=Linux Kernel Crypto API | version=4.19}}1- {{DocSource | domain= |
1- crypto/index.html |
Yocto Project
Yocto Project | path=overview-manual/overview-manual.html}}<br /> 2- {{DocSource | domain=Yocto Project | path=overview-manual/overview-manual.html | text=Yocto Project Overview and Concepts Manual}}<br /> 3- {{DocSource | domain=Yocto Project | path=overview-manual/overview-manual.html | version=3.0}}<br /> 4- {{DocSource | domain=Yocto Project | path=overview-manual/overview-manual.html | text=Yocto Project Overview and Concepts Manual | version=3.0}}1- {{DocSource | domain= |
1- overview-manual/overview-manual.html |
AWS IoT Greengrass
IoT Greengrass?}}<br /> 3- {{DocSource | domain=AWS Greengrass | path=developerguide/what-is-gg.html | version=2.0}}<br /> 4- {{DocSource | domain=AWS Greengrass | path=developerguide/what-is-gg.html | text=What is AWS IoT Greengrass? | version=2.0}}1- {{DocSource | domain=AWS Greengrass | path=developerguide/what-is-gg.html}}<br /> 2- {{DocSource | domain=AWS Greengrass | path=developerguide/what-is-gg.html | text=What is AWS |
1- developerguide/what-is-gg.html |
U-Boot
U-Boot | path=build/index.html}}<br /> 2- {{DocSource | domain=U-Boot | path=build/index.html | text=How to build U-Boot?}}<br /> 3- {{DocSource | domain=U-Boot | path=build/index.html | version=2021.01}}<br /> 4- {{DocSource | domain=U-Boot | path=build/index.html | text=How to build U-Boot? | version=2021.01}}1- {{DocSource | domain= |
1- build/index.html |
Check that there's no space before and after the text
Linux kernel | path=crypto/index.html}}AFTER<br /> 2- BEFORE{{DocSource | domain=Linux kernel | path=crypto/index.html | text=Linux Kernel Crypto API}}AFTER<br /> 3- BEFORE{{DocSource | domain=Linux kernel | path=crypto/index.html | version=4.19}}AFTER<br /> 4- BEFORE{{DocSource | domain=Linux kernel | path=crypto/index.html | text=Linux Kernel Crypto API | version=4.19}}AFTER1- BEFORE{{DocSource | domain= |
1- BEFOREcrypto/index.htmlAFTER |
Unsupported domain
{{DocSource | domain=Unsupported domain | path=Document}}
|
Unsupported domain! |
4. Code[edit source]
Linux kernel: [https://www.kernel.org/doc/html/{{#if: {{{version|}}}|v{{#replace:{{{version|}}}| |}}|v5.10}}/{{#replace:{{{path|}}}| |}} {{#if: {{{text|}}}|{{{text}}}|{{{path}}}}}{{#if: {{{version|}}}| (v{{#replace:{{{version|}}}| |}})}}]
Yocto Project: [https://docs.yoctoproject.org/{{#if: {{{version|}}}|{{#replace:{{{version|}}}| |}}|3.1.11}}/{{#replace:{{{path|}}}| |}} {{#if: {{{text|}}}|{{{text}}}|{{{path}}}}}{{#if: {{{version|}}}| (v{{#replace:{{{version|}}}| |}})}}]
AWS IoT Greengrass [https://docs.aws.amazon.com/greengrass/{{#if: {{{version|}}}|{{#replace:{{{version|}}}| |}}|latest}}/{{#replace:{{{path|}}}| |}} {{#if: {{{text|}}}|{{{text}}}|{{{path}}}}}{{#if: {{{version|}}}| v({{#replace:{{{version|}}}| |}})}}]
U-Boot: [https://u-boot.readthedocs.io/en/{{#if: {{{version|}}}|{{#replace:{{{version|}}}| |}}|v2020.10}}/{{#replace:{{{path|}}}| |}} {{#if: {{{text|}}}|{{{text}}}|{{{path}}}}}{{#if: {{{version|}}}| (v{{#replace:{{{version|}}}| |}})}}]
Unsupported domain!