Registered User mNo edit summary |
Registered User (Merge articles) |
||
(3 intermediate revisions by the same user not shown) | |||
Line 4: | Line 4: | ||
It puts a message box with a "pink garbage can" icon in the page, and adds this page to the [[:Category:Candidates for deletion|Candidates for deletion]] category. | It puts a message box with a "pink garbage can" icon in the page, and adds this page to the [[:Category:Candidates for deletion|Candidates for deletion]] category. | ||
'''Only logged-in users who have writing permissions, can see this box'''. {{Highlight|However, do not put any confidential information in the parameters of this template}}. | |||
Wiki maintainers periodically have a look at this category, and delete the pages that belong to it. | Wiki maintainers periodically have a look at this category, and delete the pages that belong to it. | ||
Line 69: | Line 71: | ||
AFTER | AFTER | ||
|} | |} | ||
==Maintenance== | |||
This template is a template common to all ST wikis. <br> | |||
Modifications must be done into the [[stwikimodel:Template:ArticleToDelete|WikiModel]]. They must be reviewed by all ST wikis maintainers.<br> | |||
When approved, the template can be pushed/merged towards all ST wikis. | |||
==Code== | ==Code== | ||
</noinclude>{ | </noinclude>{{#tag:secureTransclude|| | ||
src=ProtectedTemplate:ArticleToDelete| | |||
params={{{1|}}} {{!}} {{{2|}}} | |||
}} |
Latest revision as of 18:07, 12 December 2024
1. Usage
The ArticleToDelete template is used to request the deletion of a page. It should be added as the very first line on the page that you believe should be deleted from the wiki.
It puts a message box with a "pink garbage can" icon in the page, and adds this page to the Candidates for deletion category.
Only logged-in users who have writing permissions, can see this box. However, do not put any confidential information in the parameters of this template.
Wiki maintainers periodically have a look at this category, and delete the pages that belong to it.
<reason> | <signature>}}Usage: {{ArticleToDelete |
Where <reason> and <signature> are mandatory parameters:
- <reason> is the reason supplied for the deletion
- <signature> is the signature of the requester. It is recommended to use
~~~~
wiki markup to sign the request
2. Basic examples
You type | You get |
---|---|
Deletion requested: reason and signature supplied
{{ArticleToDelete | This is the reason for this request | ~~~~}}
|
3. More examples
You type | You get |
---|---|
Deletion requested: no reason supplied, no signature supplied
{{ArticleToDelete}}
|
|
Deletion requested: reason supplied with few words, no signature supplied
{{ArticleToDelete | This is the reason for this request}}
|
|
Deletion requested: no reason supplied, signature supplied
{{ArticleToDelete | | ~~~~}}
|
|
Deletion requested: reason supplied with a long sentence, signature supplied
{{ArticleToDelete | The reason is a long sentence. Lorem ipsum: isdem diebus Apollinaris Domitiani gener, paulo ante agens palatii Caesaris curam, ad Mesopotamiam missus a socero per militares numeros immodice scrutabatur, an quaedam altiora meditantis iam Galli. | ~~~~}}
|
|
Check that the spaces before and after the message
BEFORE{{ArticleToDelete | Check spaces | ~~~~}}AFTER<br>
BEFORE
{{ArticleToDelete | Check spaces | ~~~~}}
AFTER
|
BEFOREAFTER AFTER |
4. Maintenance
This template is a template common to all ST wikis.
Modifications must be done into the WikiModel. They must be reviewed by all ST wikis maintainers.
When approved, the template can be pushed/merged towards all ST wikis.