Registered User mNo edit summary Tag: 2017 source edit |
Registered User Tag: 2017 source edit |
||
Line 11: | Line 11: | ||
The STM32MP257x-EV1 Evaluation boards packages ({{Board | type=257F-EV1 | name=short}}), completed by the B-CAMS-IMX package, include all the items listed below. | The STM32MP257x-EV1 Evaluation boards packages ({{Board | type=257F-EV1 | name=short}}), completed by the B-CAMS-IMX package, include all the items listed below. | ||
[[File:STM32MP257x-EV1 split.jpg | 800px| left | link= | '''STM32MP257F-EV1''' shown here (picture is not contractual)]] | [[File:STM32MP257x-EV1 split.jpg | 800px| left| link= | '''STM32MP257F-EV1''' shown here (picture is not contractual)]] | ||
{| | {| | ||
|+ | |+ | ||
Line 31: | Line 31: | ||
To complete the basic set up, you can buy an LVDS display and a CSI camera. The complete set will be then : | To complete the basic set up, you can buy an LVDS display and a CSI camera. The complete set will be then : | ||
[[File: STM32MP257x-EV1_assembly.png| thumb | 800px | center | link= | STM32MP257x-EV1 Evaluation board assembly <br> '''STM32MP257F-EV1''' shown here (picture is not contractual)]] | [[File: STM32MP257x-EV1_assembly.png| thumb | 800px | center | link= | STM32MP257x-EV1 Evaluation board assembly <br> '''STM32MP257F-EV1''' shown here (picture is not contractual)]] | ||
===How to connect LVDS display to ST board=== | ===How to connect LVDS display to ST board=== | ||
[[File: STM32MP257x-EV1_DisplayBoardAssembly1.jpg| thumb | 800px | center | link= | Display board assembly (picture is not contractual)]] | [[File: STM32MP257x-EV1_DisplayBoardAssembly1.jpg| thumb | 800px | center | link= | Display board assembly (picture is not contractual)]] | ||
* Check the above cable orientation thanks to the black mark and the white twisted pairs. | * Check the above cable orientation thanks to the black mark and the white twisted pairs. | ||
Line 40: | Line 40: | ||
* On each port, insert the cable as described: | * On each port, insert the cable as described: | ||
[[File: STM32MP257x-EV1_DisplayBoardAssembly2.jpg| thumb | 800px | center | link= | Display board assembly (picture is not contractual)]] | [[File: STM32MP257x-EV1_DisplayBoardAssembly2.jpg| thumb | 800px | center | link= | Display board assembly (picture is not contractual)]] | ||
===How to connect MB1854 camera board to ST board=== | ===How to connect MB1854 camera board to ST board=== | ||
[[File: STM32MP257x-EV1_CameraBoardAssembly1.jpg| thumb | | [[File: STM32MP257x-EV1_CameraBoardAssembly1.jpg| thumb | 500px | center | link= |Camera board assembly (picture is not contractual)]] | ||
*Find the camera port on STM32MP257x-EV1 Evaluation board (CN4) and the one on MB1854 (CN1). One FFC is provided in the camera box. | *Find the camera port on STM32MP257x-EV1 Evaluation board (CN4) and the one on MB1854 (CN1). One FFC is provided in the camera box. | ||
*On each port, carefully: | *On each port, carefully: | ||
**lightly pull the black plastic (1) to insert the contact side of the FFC towards the board (2). | **lightly pull the black plastic (1) to insert the contact side of the FFC towards the board (2). | ||
**Push the black plastic to hold the FFC (3). | **Push the black plastic to hold the FFC (3). | ||
[[File: STM32MP257x-EV1_CameraBoardAssembly2.jpg| thumb | 800px | center | link= | Camera board assembly (picture is not contractual)]] | [[File: STM32MP257x-EV1_CameraBoardAssembly2.jpg| thumb | 800px | center | link= | Camera board assembly (picture is not contractual)]] | ||
===STM32MP257x-EV1 Evaluation board assembled === | |||
<br clear=all> | ===STM32MP257x-EV1 Evaluation board assembled=== | ||
[[File:STM32MP257x-EV1_assembled.jpg| thumb | 700px | center | link= | STM32MP257x-EV1 Evaluation board assembled <br> '''STM32MP257F-EV1''' shown here (picture is not contractual)]] | <br clear="all"> | ||
[[File:STM32MP257x-EV1_assembled.jpg| thumb | 700px | center | link= | STM32MP257x-EV1 Evaluation board assembled <br> '''STM32MP257F-EV1''' shown here (picture is not contractual)]] | |||
<noinclude> | <noinclude> | ||
{{NoIndex}} | {{NoIndex}} |
Latest revision as of 16:07, 6 November 2024
This article aims to present how to assemble the STM32MP257x-EV1 Evaluation boards. It is valid for the STM32MP257F-EV1 Evaluation board: the part numbers are specified in the STM32MP25 microprocessor part numbers article.
The STM32MP257x-EV1 Evaluation boards packages (STM32MP257F-EV1 ), completed by the B-CAMS-IMX package, include all the items listed below.

Position | Description |
---|---|
1 | MB1936 main board |
2 | 7” LVDS WSVGA display with touch panel (EDT ETML0700Z9NDHA panel - optional) |
3 | LVDS display cable- optional |
4 | MB1854 board AI camera (not part of STM32MP257x-EV1 Evaluation boards packages , provided via B-CAMS-IMX package) optional |
5 | camera board FFC (not part of STM32MP257x-EV1 Evaluation boards packages, provided via B-CAMS-IMX package) - optional |
To complete the basic set up, you can buy an LVDS display and a CSI camera. The complete set will be then :
1. How to connect LVDS display to ST board[edit | edit source]
- Check the above cable orientation thanks to the black mark and the white twisted pairs.
- Find the LVDS port on STM32MP257x-EV1 Evaluation board (CN2) and the one on the display (CN1). One cable is provided in the LVDS display box.
- On each port, insert the cable as described:
2. How to connect MB1854 camera board to ST board[edit | edit source]
File:STM32MP257x-EV1 CameraBoardAssembly1.jpg
Camera board assembly (picture is not contractual)
- Find the camera port on STM32MP257x-EV1 Evaluation board (CN4) and the one on MB1854 (CN1). One FFC is provided in the camera box.
- On each port, carefully:
- lightly pull the black plastic (1) to insert the contact side of the FFC towards the board (2).
- Push the black plastic to hold the FFC (3).
3. STM32MP257x-EV1 Evaluation board assembled[edit | edit source]