Registered User mNo edit summary |
Registered User mNo edit summary Tag: 2017 source edit |
||
(5 intermediate revisions by the same user not shown) | |||
Line 7: | Line 7: | ||
{{Warning|To use efficiently this package, go through the Developer Package article relative to your STM32 microprocessor series: [[:Category:Developer Package]]}} | {{Warning|To use efficiently this package, go through the Developer Package article relative to your STM32 microprocessor series: [[:Category:Developer Package]]}} | ||
==STM32MP1 ecosystem v5. | ==STM32MP1 ecosystem v5.1.0 release== | ||
</noinclude> | </noinclude> | ||
<section begin=DownloadAndExtract /> | <section begin=DownloadAndExtract /> | ||
{{SoftwareLicenseAgreement | distribution=OpenSTLinux }} | |||
* The OpenSTLinux BSP package is delivered through a tarball file named '''{{EcosystemRelease/Package | device=MP1 | revision=5.1.0 | package=OpenSTLinux BSP package | request=name}}''' for {{Board | type=157x-EV1 | name=short}}, {{Board | type=157x-DKx | name=short}} and {{Board | type=135x-DK | name=short}} boards. | |||
<span id="Download"></span> | |||
* Download and install the STM32MP1 OpenSTLinux BSP package. | |||
{| class="st-table" | |||
|- | |||
! !! style="text-align:center;"|STM32MP1 Developer Package - STM32MP1 ecosystem v5.1.0 release | |||
|- | |||
| Download || | |||
* Go on [https://www.st.com/en/embedded-software/stm32mp1dev.html#get-software st.com] to download the STM32MP1 Developer Package, ''{{EcosystemRelease/Package | device=MP1 | revision=5.1.0 | package=OpenSTLinux BSP package | request=name}}'' file. | |||
|- | |||
| Installation || | |||
* Go to the host PC directory where you extracted the package from the .jar file if you follow the [[Example of directory structure for Packages|proposition to organize the working directory]], that is: | |||
{{PC$}}cd {{HighlightParam|''<working directory path>''}}/Developer-Package | |||
{{PC$}}tar xvf {{EcosystemRelease/Package | revision=5.1.0 | package=OpenSTLinux BSP package | request=name}} | |||
|- | |||
| Release note || | |||
Details about the content of the OpenSTLinux BSP package are available in the '''associated''' [[STM32 MPU OpenSTLinux release note]]. | |||
[[File:Archive_box.png|25px|link=]] For information on older releases, go to [[STM32MP1_Developer_Package_-_OpenSTLinux_BSP#Archives|Archives]]. | |||
|} | |||
<section end=DownloadAndExtract /> | |||
* In the {{HighlightParam|''<Developer Package installation directory>''}}''/{{EcosystemRelease/Package | device=MP1 | revision=5.1.0 | package=OpenSTLinux BSP package | request=path}}'', a tarball archive of the OpenSTLinux BSP components can be found. | |||
*The '''Linux kernel installation directory''' is named ''linux-stm32mp-''{{HighlightParam|''<kernel version>''}}: | |||
{{Green|{{EcosystemRelease/Package | revision=5.1.0 | package=Linux kernel package| request=name}}}}	{{Highlight|'''Linux kernel installation directory'''}} | |||
├── [*].patch				{{Highlight|ST patches to apply during the Linux kernel preparation (see next chapter)}} | |||
├── fragment-[*].config			{{Highlight|ST configuration fragments to apply during the Linux kernel configuration (see next chapter)}} | |||
├── optional-fragment-[*].config	{{Highlight|Optional ST configuration fragments to apply during the Linux kernel configuration depending on your needs (SMP or not, signature or not, ...)}} | |||
├── {{EcosystemRelease/Package | revision=5.1.0 | package=Linux kernel source | request=name}}			{{Highlight|Tarball file of the Linux kernel source code}} | |||
├── {{Orange|README.HOW_TO.txt}}			{{Highlight|Helper file for Linux kernel management: '''reference''' for Linux kernel build}} | |||
└── series				{{Highlight|List of all ST patches to apply}} | |||
*The '''gcnano driver installation directory''' is named ''gcnano-driver-stm32mp-''{{HighlightParam|''<gcnano driver version>''}}: | |||
{{Green|{{EcosystemRelease/Package | revision=5.1.0 | package=gcnano-driver package| request=name}}}}		{{Highlight|'''gcnano-driver installation directory'''}} | |||
├── {{EcosystemRelease/Package | revision=5.1.0 | package=gcnano-driver source | request=name}}	{{Highlight|Tarball file of the gcnano-driver source code}} | |||
└── {{Orange|README.HOW_TO.txt}}					{{Highlight|Helper file for gcnano-driver management: '''reference''' for gcnano-driver build}} | |||
*The '''U-Boot installation directory''' is named ''u-boot-stm32mp-''{{HighlightParam|''<U-Boot version>''}}: | |||
{{Green|{{EcosystemRelease/Package | revision=5.1.0 | package=U-Boot package| request=name}}}}			{{Highlight|'''U-Boot installation directory'''}} | |||
├── [*].patch						{{Highlight|ST patches to apply during the U-Boot preparation (see next chapter)}} | |||
├── fiptool-stm32mp					{{Highlight|tool for fip generation}} | |||
├── {{Green|{{EcosystemRelease/Package | revision=5.1.0 | package=U-Boot source | request=path}}}}			{{Highlight|'''U-Boot source code directory'''}} | |||
├── Makefile.sdk					{{Highlight|Makefile for the U-Boot compilation}} | |||
├── {{Orange|README.HOW_TO.txt}}					{{Highlight|Helper file for U-Boot management: '''reference''' for U-Boot build}} | |||
├── series						{{Highlight|List of all ST patches to apply}} | |||
└── {{EcosystemRelease/Package | revision=5.1.0 | package=U-Boot source | request=name}}	{{Highlight|Tarball file of the U-Boot source code}} | |||
*The '''TF-A installation directory''' is named ''tf-a-stm32mp-''{{HighlightParam|''<TF-A version>''}}: | |||
{{Green|{{EcosystemRelease/Package | revision=5.1.0 | package=TF-A package| request=name}}}}		{{Highlight|'''TF-A installation directory'''}} | |||
├── [*].patch					{{Highlight|ST patches to apply during the TF-A preparation (see next chapter)}} | |||
├── fiptool-stm32mp					{{Highlight|tool for fip generation}} | |||
├── {{Green|{{EcosystemRelease/Package | revision=5.1.0 | package=TF-A source | request=path}}}}		{{Highlight|'''TF-A source code directory'''}} | |||
├── Makefile.sdk				{{Highlight|Makefile for the TF-A compilation}} | |||
├── {{Orange|README.HOW_TO.txt}}				{{Highlight|Helper file for TF-A management: '''reference''' for TF-A build}} | |||
├── series					{{Highlight|List of all ST patches to apply}} | |||
└── {{EcosystemRelease/Package | revision=5.1.0 | package=TF-A source | request=name}}	{{Highlight|Tarball file of the TF-A source code}} | |||
* The '''OP-TEE installation directory''' is named ''optee-os-stm32mp''-{{HighlightParam|''<OP-TEE version>''}}: | |||
{{Green|{{EcosystemRelease/Package | revision=5.1.0 | package=OP-TEE package| request=name}}}}			{{Highlight|'''OP-TEE installation directory'''}} | |||
├── [*].patch						{{Highlight|ST patches to apply during the OP-TEE preparation (see next chapter)}} | |||
├── fiptool-stm32mp					{{Highlight|tool for fip generation}} | |||
├── {{Green|{{EcosystemRelease/Package | revision=5.1.0 | package=OP-TEE source | request=path}}}}			{{Highlight|'''OP-TEE source code directory'''}} | |||
├── fonts.tar.gz					{{Highlight|fonts for OPTEE-OS}} | |||
├── Makefile.sdk					{{Highlight|Makefile for the OP-TEE compilation}} | |||
├── {{EcosystemRelease/Package | revision=5.1.0 | package=OP-TEE source | request=name}}	{{Highlight|Tarball file of the OP-TEE source code}} | |||
├── {{Orange|README.HOW_TO.txt}}					{{Highlight|Helper file for OP-TEE management: '''reference''' for OP-TEE build}} | |||
└── series						{{Highlight|List of all ST patches to apply}} | |||
* The '''FIP artifacts directory''' is named ''FIP_artifacts'': | |||
{{Green|FIP_artifacts}} | |||
├── {{Green|arm-trusted-firmware}} | |||
│ ├── {{Green|fwconfig}} | |||
│ │ ├── stm32mp13[*]-fw-config-optee.dtb		{{Highlight|Device tree for FW config → STM32MP13 boards}} | |||
│ │ └── stm32mp15[*]-fw-config-optee.dtb		{{Highlight|Device tree for FW config → STM32MP15 boards}} | |||
│ ├── metada.bin					{{Highlight|Store boot information}} | |||
│ ├── tf-a-stm32mp13[*].stm32				{{Highlight|FSBL binary→ STM32MP13 boards}} | |||
│ └── tf-a-stm32mp15[*].stm32				{{Highlight|FSBL binary → STM32MP15 boards}} | |||
├── {{Green|optee}} | |||
│ ├── tee-header_v2-stm32mp13[*].bin			{{Highlight|Binary file for OP-TEE OS → STM32MP13 boards}} | |||
│ ├── tee-header_v2-stm32mp15[*].bin			{{Highlight|Binary file for OP-TEE OS → STM32MP15 kits}} | |||
│ ├── tee-pageable_v2-stm32mp13[*].bin		{{Highlight|Binary file for OP-TEE OS → STM32MP13 boards}} | |||
│ ├── tee-pageable_v2-stm32mp15[*].bin		{{Highlight|Binary file for OP-TEE OS → STM32MP15 boards}} | |||
│ ├── tee-pager_v2-stm32mp13[*].bin			{{Highlight|Binary file for OP-TEE OS → STM32MP13 boards}} | |||
│ └── tee-pager_v2-stm32mp15[*].bin			{{Highlight|Binary file for OP-TEE OS → STM32MP15 boards}} | |||
└── {{Green|u-boot}} | |||
├── u-boot-nodtb-stm32mp13-default.bin | |||
├── u-boot-nodtb-stm32mp15-default.bin | |||
├── u-boot-nodtb-stm32mp13-fastboot-sdcard.bin	{{Highlight|Binary file for fastboot on SD-Card for STM32MP13 boards}} | |||
├── u-boot-nodtb-stm32mp15-fastboot-emmc.bin	{{Highlight|Binary file for fastboot on eMMC for STM32MP15 boards}} | |||
├── u-boot-nodtb-stm32mp15-fastboot-sdcard.bin	{{Highlight|Binary file for fastboot on SD-Card for STM32MP15 boards}} | |||
├── u-boot-stm32mp13[*].dtb				{{Highlight|Device tree for U-Boot → STM32MP13 boards}} | |||
└── u-boot-stm32mp15[*].dtb				{{Highlight|Device tree for U-Boot → STM32MP15 boards}} | |||
* The debug symbol files are located under the {{HighlightParam|''<Developer Package installation directory>''}}/{{EcosystemRelease/Package | device=MP1 | revision=5.1.0 | package=Debug symbol files | request=path}}'' directory: | |||
<div style="overflow: auto;" > | |||
{| class="st-table specialpre" | |||
|- | |||
| style="border-style: hidden; padding-right: 0;" | | |||
{{Green|stm32mp1}} | |||
├── {{Green|arm-trusted-firmware}} | |||
│ └── {{Green|debug}} | |||
│ ├── debug-tf-a-stm32mp13[*].stm32	{{Highlight|Debug file for FSBL → STM32MP13 boards}} | |||
│ ├── debug-tf-a-stm32mp15[*].stm32	{{Highlight|Debug file for FSBL → STM32MP15 boards}} | |||
│ ├── tf-a-bl2-stm32mp13-sdcard.elf 	{{Highlight|Debug symbol file for TF-A → TF-A for STM32MP13 boards for emmc boot stage}} | |||
│ ├── tf-a-bl2-stm32mp13-uart.elf 	{{Highlight|Debug symbol file for TF-A → TF-A for STM32MP13 boards for UART downloading boot stage}} | |||
│ ├── tf-a-bl2-stm32mp13-usb.elf 		{{Highlight|Debug symbol file for TF-A → TF-A for STM32MP13 boards for USB downloading boot stage}} | |||
│ ├── tf-a-bl2-stm32mp15-emmc.elf 	{{Highlight|Debug symbol file for TF-A → TF-A for STM32MP15 for emmc boot stage}} | |||
│ ├── tf-a-bl2-stm32mp15-nand.elf 	{{Highlight|Debug symbol file for TF-A → TF-A for STM32MP15 for nand boot stage}} | |||
│ ├── tf-a-bl2-stm32mp15-nor.elf 		{{Highlight|Debug symbol file for TF-A → TF-A for STM32MP15 for nor boot stage}} | |||
│ ├── tf-a-bl2-stm32mp15-sdcard.elf 	{{Highlight|Debug symbol file for TF-A → TF-A for STM32MP15 for SDcard boot stage}} | |||
│ ├── tf-a-bl2-stm32mp15-uart.elf 	{{Highlight|Debug symbol file for TF-A → TF-A for STM32MP15 for UART downloading boot stage}} | |||
│ └── tf-a-bl2-stm32mp15-usb.elf 		{{Highlight|Debug symbol file for TF-A → TF-A for STM32MP15 for USB downloading boot stage}} | |||
├── {{Green|kernel}} | |||
│ ├── config-6.1.82				{{Highlight|Reference Config file for Linux kernel}} | |||
│ ├── vmlinux					{{Highlight|Image of the Linux kernel}} | |||
├── {{Green|optee}} | |||
│ └── {{Green|debug}} | |||
│ ├── tee-stm32mp135f-dk.elf 		{{Highlight|Debug symbol file for OP-TEE OS → STM32MP13 Discovery kits}} | |||
│ ├── tee-stm32mp157a-dk1.elf 		{{Highlight|Debug symbol file for OP-TEE OS → STM32MP15 Discovery kits}} | |||
│ ├── tee-stm32mp157a-ev1.elf 		{{Highlight|Debug symbol file for OP-TEE OS → STM32MP15 Evaluation boards}} | |||
│ ├── tee-stm32mp157c-dk2.elf 		{{Highlight|Debug symbol file for OP-TEE OS → STM32MP15 Discovery kits}} | |||
│ ├── tee-stm32mp157c-ed1.elf 		{{Highlight|Debug symbol file for OP-TEE OS → STM32MP15 Evaluation boards}} | |||
│ ├── tee-stm32mp157c-ev1.elf 		{{Highlight|Debug symbol file for OP-TEE OS → STM32MP15 Evaluation boards}} | |||
│ ├── tee-stm32mp157d-dk1.elf 		{{Highlight|Debug symbol file for OP-TEE OS → STM32MP15 Discovery kits}} | |||
│ ├── tee-stm32mp157d-ev1.elf 		{{Highlight|Debug symbol file for OP-TEE OS → STM32MP15 Evaluation boards}} | |||
│ ├── tee-stm32mp157f-dk2.elf 		{{Highlight|Debug symbol file for OP-TEE OS → STM32MP15 Discovery kits}} | |||
│ ├── tee-stm32mp157f-ed1.elf 		{{Highlight|Debug symbol file for OP-TEE OS → STM32MP15 Evaluation boards}} | |||
│ └── tee-stm32mp157f-ev1.elf 		{{Highlight|Debug symbol file for OP-TEE OS → STM32MP15 Evaluation boards}} | |||
└── {{Green|u-boot}} | |||
└── {{Green|debug}} | |||
├── u-boot-stm32mp13-default.elf 		{{Highlight|Debug symbol file for U-Boot → STM32MP13 Discovery kits}} | |||
├── u-boot-stm32mp*-fastboot*.elf 		{{Highlight|Debug symbol file for U-Boot with fastboot enabled}} | |||
└── u-boot-stm32mp13-default.elf 		{{Highlight|Debug symbol file for U-Boot → STM32MP13 Discovery kits}} | |||
|} | |||
</div> | |||
<noinclude> | |||
==Archives [[File:Archive_box.png|25px|link=]]== | |||
{{EcosystemFlow/Archives}} | |||
<div class="mw-collapsible mw-collapsed"> | |||
===STM32MPU-Ecosystem-v5.0.0 release === | |||
<div class="mw-collapsible-content"> | |||
{{SoftwareLicenseAgreement | distribution=OpenSTLinux }} | {{SoftwareLicenseAgreement | distribution=OpenSTLinux }} | ||
* The OpenSTLinux BSP package is delivered through a tarball file named '''{{EcosystemRelease/Package | revision=5.0.0 | package=OpenSTLinux BSP package | request=name}}''' for {{Board | type=157x-EV1 | name=short}}, {{Board | type=157x-DKx | name=short}} and {{Board | type=135x-DK | name=short}} boards. | * The OpenSTLinux BSP package is delivered through a tarball file named '''{{EcosystemRelease/Package | revision=5.0.0 | package=OpenSTLinux BSP package | request=name}}''' for {{Board | type=157x-EV1 | name=short}}, {{Board | type=157x-DKx | name=short}} and {{Board | type=135x-DK | name=short}} boards. | ||
Line 25: | Line 170: | ||
| Installation || | | Installation || | ||
* Go to the host PC directory where you extracted the package from the .jar file if you follow the [[Example of directory structure for Packages|proposition to organize the working directory]], that is: | * Go to the host PC directory where you extracted the package from the .jar file if you follow the [[Example of directory structure for Packages|proposition to organize the working directory]], that is: | ||
{{PC$}} cd {{HighlightParam|''<working directory path>''}}/Developer-Package | {{PC$}}cd {{HighlightParam|''<working directory path>''}}/Developer-Package | ||
{{PC$}} tar xvf {{EcosystemRelease/Package | revision=5.0.0 | package=OpenSTLinux BSP package | request=name}} | {{PC$}}tar xvf {{EcosystemRelease/Package | revision=5.0.0 | package=OpenSTLinux BSP package | request=name}} | ||
|- | |- | ||
| Release note || | | Release note || | ||
Line 121: | Line 266: | ||
│ └── tf-a-bl2-stm32mp15-usb.elf 		{{Highlight|Debug symbol file for TF-A → TF-A for STM32MP15 for USB downloading boot stage}} | │ └── tf-a-bl2-stm32mp15-usb.elf 		{{Highlight|Debug symbol file for TF-A → TF-A for STM32MP15 for USB downloading boot stage}} | ||
├── {{Green|kernel}} | ├── {{Green|kernel}} | ||
│ ├── config-6.1. | │ ├── config-6.1.82				{{Highlight|Reference Config file for Linux kernel}} | ||
│ ├── vmlinux					{{Highlight|Image of the Linux kernel}} | │ ├── vmlinux					{{Highlight|Image of the Linux kernel}} | ||
├── {{Green|optee}} | ├── {{Green|optee}} | ||
Line 141: | Line 286: | ||
└── u-boot-stm32mp15.elf 		{{Highlight|Debug symbol file for U-Boot → STM32MP15 boards}} | └── u-boot-stm32mp15.elf 		{{Highlight|Debug symbol file for U-Boot → STM32MP15 boards}} | ||
|} | |} | ||
</div> | </div></div></div> | ||
< | |||
{{NoIndex}} | {{NoIndex}} |
Latest revision as of 14:52, 21 June 2024
This article aims at giving the following information:
- How to get the latest OP-TEE, TF-A, U-Boot, Linux® kernel, gcnano-driver and debug symbols for the STM32 microprocessor series
- Where to find the associated release note
- Where to find the previous releases (archives)
1. STM32MP1 ecosystem v5.1.0 release[edit | edit source]
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here.
- The OpenSTLinux BSP package is delivered through a tarball file named unknown revision for STM32MP157x-EV1
, STM32MP157x-DKx
and STM32MP135x-DK
boards.
- Download and install the STM32MP1 OpenSTLinux BSP package.
STM32MP1 Developer Package - STM32MP1 ecosystem v5.1.0 release | |
---|---|
Download |
|
Installation |
<working directory path>/Developer-Packagecd unknown revisiontar xvf |
Release note |
Details about the content of the OpenSTLinux BSP package are available in the associated STM32 MPU OpenSTLinux release note.
|
- In the <Developer Package installation directory>/unknown revision , a tarball archive of the OpenSTLinux BSP components can be found.
- The Linux kernel installation directory is named linux-stm32mp-<kernel version>:
unknown revision Linux kernel installation directory ├── [*].patch ST patches to apply during the Linux kernel preparation (see next chapter) ├── fragment-[*].config ST configuration fragments to apply during the Linux kernel configuration (see next chapter) ├── optional-fragment-[*].config Optional ST configuration fragments to apply during the Linux kernel configuration depending on your needs (SMP or not, signature or not, ...) ├── unknown revision Tarball file of the Linux kernel source code ├── README.HOW_TO.txt Helper file for Linux kernel management: reference for Linux kernel build └── series List of all ST patches to apply
- The gcnano driver installation directory is named gcnano-driver-stm32mp-<gcnano driver version>:
unknown revision gcnano-driver installation directory ├── unknown revision Tarball file of the gcnano-driver source code └── README.HOW_TO.txt Helper file for gcnano-driver management: reference for gcnano-driver build
- The U-Boot installation directory is named u-boot-stm32mp-<U-Boot version>:
unknown revision U-Boot installation directory ├── [*].patch ST patches to apply during the U-Boot preparation (see next chapter) ├── fiptool-stm32mp tool for fip generation ├── unknown revision U-Boot source code directory ├── Makefile.sdk Makefile for the U-Boot compilation ├── README.HOW_TO.txt Helper file for U-Boot management: reference for U-Boot build ├── series List of all ST patches to apply └── unknown revision Tarball file of the U-Boot source code
- The TF-A installation directory is named tf-a-stm32mp-<TF-A version>:
unknown revision TF-A installation directory ├── [*].patch ST patches to apply during the TF-A preparation (see next chapter) ├── fiptool-stm32mp tool for fip generation ├── unknown revision TF-A source code directory ├── Makefile.sdk Makefile for the TF-A compilation ├── README.HOW_TO.txt Helper file for TF-A management: reference for TF-A build ├── series List of all ST patches to apply └── unknown revision Tarball file of the TF-A source code
- The OP-TEE installation directory is named optee-os-stm32mp-<OP-TEE version>:
unknown revision OP-TEE installation directory ├── [*].patch ST patches to apply during the OP-TEE preparation (see next chapter) ├── fiptool-stm32mp tool for fip generation ├── unknown revision OP-TEE source code directory ├── fonts.tar.gz fonts for OPTEE-OS ├── Makefile.sdk Makefile for the OP-TEE compilation ├── unknown revision Tarball file of the OP-TEE source code ├── README.HOW_TO.txt Helper file for OP-TEE management: reference for OP-TEE build └── series List of all ST patches to apply
- The FIP artifacts directory is named FIP_artifacts:
FIP_artifacts ├── arm-trusted-firmware │ ├── fwconfig │ │ ├── stm32mp13[*]-fw-config-optee.dtb Device tree for FW config → STM32MP13 boards │ │ └── stm32mp15[*]-fw-config-optee.dtb Device tree for FW config → STM32MP15 boards │ ├── metada.bin Store boot information │ ├── tf-a-stm32mp13[*].stm32 FSBL binary→ STM32MP13 boards │ └── tf-a-stm32mp15[*].stm32 FSBL binary → STM32MP15 boards ├── optee │ ├── tee-header_v2-stm32mp13[*].bin Binary file for OP-TEE OS → STM32MP13 boards │ ├── tee-header_v2-stm32mp15[*].bin Binary file for OP-TEE OS → STM32MP15 kits │ ├── tee-pageable_v2-stm32mp13[*].bin Binary file for OP-TEE OS → STM32MP13 boards │ ├── tee-pageable_v2-stm32mp15[*].bin Binary file for OP-TEE OS → STM32MP15 boards │ ├── tee-pager_v2-stm32mp13[*].bin Binary file for OP-TEE OS → STM32MP13 boards │ └── tee-pager_v2-stm32mp15[*].bin Binary file for OP-TEE OS → STM32MP15 boards └── u-boot ├── u-boot-nodtb-stm32mp13-default.bin ├── u-boot-nodtb-stm32mp15-default.bin ├── u-boot-nodtb-stm32mp13-fastboot-sdcard.bin Binary file for fastboot on SD-Card for STM32MP13 boards ├── u-boot-nodtb-stm32mp15-fastboot-emmc.bin Binary file for fastboot on eMMC for STM32MP15 boards ├── u-boot-nodtb-stm32mp15-fastboot-sdcard.bin Binary file for fastboot on SD-Card for STM32MP15 boards ├── u-boot-stm32mp13[*].dtb Device tree for U-Boot → STM32MP13 boards └── u-boot-stm32mp15[*].dtb Device tree for U-Boot → STM32MP15 boards
- The debug symbol files are located under the <Developer Package installation directory>/unknown revision directory:
2. Archives
[edit | edit source]
This wiki is for the v5 ecosystem releases. For information about the previous ecosystem releases, go through the Wiki archives.
2.1. STM32MPU-Ecosystem-v5.0.0 release[edit | edit source]