Registered User |
Registered User Tag: 2017 source edit |
||
(15 intermediate revisions by 2 users not shown) | |||
Line 3: | Line 3: | ||
|MPUs checklist=STM32MP13x, STM32MP15x | |MPUs checklist=STM32MP13x, STM32MP15x | ||
}}</noinclude> | }}</noinclude> | ||
==Overview== | ==Overview== | ||
This stage explains how to modify, rebuild and reload an STM32MP1 Arm® Cortex®-M4 coprocessor firmware. | This stage explains how to modify, rebuild and reload an STM32MP1 Arm® Cortex®-M4 coprocessor firmware. | ||
Line 37: | Line 38: | ||
* Browse and select '''OpenAMP_TTY_echo''' application example in the folder matching your board : | * Browse and select '''OpenAMP_TTY_echo''' application example in the folder matching your board : | ||
''$HOME/STM32MPU_workspace/ | ''$HOME/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Developer-Package/{{EcosystemRelease/Package | revision=latest | package=STM32CubeMP1 | request=path}}/Projects/'''STM32MP157C-DK2'''/Applications/OpenAMP/OpenAMP_TTY_echo/STM32CubeIDE'' | ||
or | or | ||
''$HOME/STM32MPU_workspace/ | ''$HOME/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Developer-Package/{{EcosystemRelease/Package | revision=latest | package=STM32CubeMP1 | request=path}}/Projects/'''STM32MP157C-EV1'''/Applications/OpenAMP/OpenAMP_TTY_echo/STM32CubeIDE'' | ||
Line 54: | Line 55: | ||
==Build the firmware== | ==Build the firmware== | ||
{{Warning | A compilation issue occurs with STM32CubeMP1 Package v1.6.0. STM32CubeMP1 Package v1.6.0 is compliant with 10.3 GCC toolchain whereas STM32CubeIDE-v1.13.0 is embedded by default 11.3 GCC toolchain. The toolchain has to be updated to 10.3 with Toolchain manager tool to compile STM32CubeMP1 Package v1.6.0, See [[STM32_MPU_resources#UM2609 | UM2609 - STM32CubeIDE user manual]], section 2.3.1 for details.}} | |||
* Select project '''OpenAMP_TTY_Echo_CM4''' and click the '''Build''' button (the little hammer in the toolbar) | * Select project '''OpenAMP_TTY_Echo_CM4''' and click the '''Build''' button (the little hammer in the toolbar) | ||
[[File:STM32CubeIDE Build.png|800px|center|link=|STM32CubeIDE build the project]] | [[File:STM32CubeIDE Build.png|800px|center|link=|STM32CubeIDE build the project]] | ||
Line 72: | Line 77: | ||
Connection is correct if Linux log or prompt are displayed in the console windows. | Connection is correct if Linux log or prompt are displayed in the console windows. | ||
[[File:STM32CubeIDE prompt.png|600px|center|link=|STM32CubeIDE Linux Prompt]] | [[File:STM32CubeIDE prompt.png|600px|center|link=|STM32CubeIDE Linux Prompt]] | ||
Your board might be connected to the PC by Ethernet, either using RJ45 (point to point or VLAN) or USB0 EthernetOverUSB gadget (point to point connection with PC using TypeA-TypeC cable). Screenshot below uses the second solution. | Your board might be connected to the PC by Ethernet, either using RJ45 (point to point or VLAN) or USB0 EthernetOverUSB gadget (point to point connection with PC using TypeA-TypeC cable). Screenshot below uses the second solution. | ||
Line 81: | Line 85: | ||
In case different status such as "busy" or "console in use", check you have no other terminal connected and close the console. | In case different status such as "busy" or "console in use", check you have no other terminal connected and close the console. | ||
In case different status such as "Stopped", right click on it and select "Start". | |||
==Start Debug Session == | ==Start Debug Session == | ||
* | * Click on your '''OpenAMP_TTY_echo_CM4''' project to select it | ||
*If not already created, create your debug configuration by | *If not already created, create your debug configuration by doing a clicking on right click on "'''OpenAMP_TTY_echo_CM4''' and Select "'''Debug As'''" and "'''STM32 C/C++ Application'''". It will open the "Edit Configuration" window. | ||
[[File:STM32CubeIDE Debug conf | [[File:STM32CubeIDE Edit Debug conf.png|800px|center|link=|Select Production mode in Startup pane of Debug Configuration]] | ||
* Check IP address is correctly filled (1). Else, you can force detection using button on the right (2). | * Check IP address is correctly filled (1). Else, you can force detection using button on the right (2). | ||
Line 144: | Line 148: | ||
==Modify the firmware== | ==Modify the firmware== | ||
The original firmware example receives a message for the host on one channel and | The original firmware example receives a message for the host on one channel and acknowledge by returning the same message to the host on the same channel. | ||
As this is not so obvious on which channel the message is received, we propose you to modify the firmware in order to add an indication to know what is the channel that is receiving the message. | As this is not so obvious on which channel the message is received, we propose you to modify the firmware in order to add an indication to know what is the channel that is receiving the message. |
Latest revision as of 12:47, 20 June 2024
1. Overview[edit | edit source]
This stage explains how to modify, rebuild and reload an STM32MP1 Arm® Cortex®-M4 coprocessor firmware.
It proposes to customize the STM32MP1 Cube Package application example "OpenAMP_TTY_Echo" using STM32CubeIDE.
2. Disconnect the "minicom" console[edit | edit source]
- If "minicom" is already opened, please disconnect it to use the STM32CubeIDE built-in serial console.
Ctrl + A then Q
3. Open STM32CubeIDE[edit | edit source]
- Start STM32CubeIDE
- Choose a workspace (default is fine)
- Notice information provided in the "Information Center page" and close it. (you can open it later on)

- Go into your workspace projet view

4. Import an existing example in STM32CubeIDE[edit | edit source]
- Open the import screen File > Import... and select Existing Project into Workspace
- Browse and select OpenAMP_TTY_echo application example in the folder matching your board :
$HOME/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Developer-Package/STM32Cube_FW_MP1_V1.6.0/Projects/STM32MP157C-DK2/Applications/OpenAMP/OpenAMP_TTY_echo/STM32CubeIDE
or
$HOME/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Developer-Package/STM32Cube_FW_MP1_V1.6.0/Projects/STM32MP157C-EV1/Applications/OpenAMP/OpenAMP_TTY_echo/STM32CubeIDE
- STM32CubeIDE brings a specific project structure for dual core devices such as STM32MP1. A top level project contains sub-projects for each core.
- Here OpenAMP_TTY_echo top project contains OpenAMP_TTY_echo_CM4 sub project. Keep the 2 projects selected and click on "Finish".
- The OpenAMP_TTY_echo project is opened and you can browse inside using the left pan.
5. Build the firmware[edit | edit source]
- Select project OpenAMP_TTY_Echo_CM4 and click the Build button (the little hammer in the toolbar)

- "Build" is finished with no error

6. Check connection to the target[edit | edit source]
STM32CubeIDE requires to be connected to Linux running on STM32MP1 device though serial connection.
This connection is automatically detected and configured when you have put cable on ST-Link port and board has booted.
You can check you can get Linux log and prompt by clicking on the "STM32 butterfly" button :
Connection is correct if Linux log or prompt are displayed in the console windows.

Your board might be connected to the PC by Ethernet, either using RJ45 (point to point or VLAN) or USB0 EthernetOverUSB gadget (point to point connection with PC using TypeA-TypeC cable). Screenshot below uses the second solution.
When serial connection is established, STM32CubeIDE automatically detects the board IP address and displays sit in the "Serial Target widget status" window in bottom right part of the screen.
In case different status such as "busy" or "console in use", check you have no other terminal connected and close the console.
In case different status such as "Stopped", right click on it and select "Start".
7. Start Debug Session[edit | edit source]
- Click on your OpenAMP_TTY_echo_CM4 project to select it
- If not already created, create your debug configuration by doing a clicking on right click on "OpenAMP_TTY_echo_CM4 and Select "Debug As" and "STM32 C/C++ Application". It will open the "Edit Configuration" window.

- Check IP address is correctly filled (1). Else, you can force detection using button on the right (2).
- Make sure the "Thru Linux core (production mode)" is selected (3)
- When configuration is correct, the "Debug" button (5) turns to active and you can launch the debug session. Else, error message appears in area (4).
STM32CubeIDE needs to use serial connection to the board to manage firmware download.
If the console is opened, it will request your approval to close it. Answer "yes".
The debug in "production mode" adds the cortex-M firmware transfer to the embedded Linux. In case of network usage, some specific pop-up appears:
- the SSH Password must be completed: the default one is "root".
- the RSA key must be approved.
After, firmware download, STM32CubeIDE switches into Debug Perspective.
In "production mode", the firmware is not break at main. GDB is simply attached to the running target. You can then use all features of the debugger.
For further information, refer to STM32CubeIDE documentation avaialble in my.st.com
8. Test the firmware[edit | edit source]
The OpenAMP_TTY_echo_CM firmware do the following:
- CPU2(CM4) initializes OpenAMP MW which initializes/configures IPCC peripheral through HAL and setup openamp-rpmsg framework infrastructure,
- CPU2(CM4) creates 2 rpmsg channels for 2 virtual UART instances (UART0 and UART1),
- CPU2(CM4) is waiting for messages from CPU1(CA7) on these both channels,
- When CPU2(CM4) receives a message on 1 Virtual UART instance/rpmsg channel, it sends the message back to CPU1(CA7) on the same Virtual UART instance
Reopen the Serial console of STM32CubeIDE and enter following commands :
- Initialize the ttyRPMSG0 configuration
stty -onlcr -echo -F /dev/ttyRPMSG0
- Read constantly the ttyRPMSG0 channel in background
cat /dev/ttyRPMSG0 &
- Send a message on one ttyRPMSG0 channel and receive the echo on the same ttyRPMSG0 channel
echo "Hello Virtual UART0" > /dev/ttyRPMSG0
Hello Virtual UART0
- You can perform the same steps with the ttyRPMSG1 channel
- Terminate the STM32CubeIDE debug session will stop the firmware.
9. Modify the firmware[edit | edit source]
The original firmware example receives a message for the host on one channel and acknowledge by returning the same message to the host on the same channel.
As this is not so obvious on which channel the message is received, we propose you to modify the firmware in order to add an indication to know what is the channel that is receiving the message.
For that, please modify main.c original code as follow:
char msg_to_transmit[MAX_BUFFER_SIZE]; int msg_size = 0; VirtUart0RxMsg = RESET; msg_size = snprintf(msg_to_transmit, MAX_BUFFER_SIZE, "Channel RPMSG0: "); msg_size += snprintf(msg_to_transmit + msg_size, MAX_BUFFER_SIZE, "%s\n", VirtUart0ChannelBuffRx); log_info("size of the message to transmit = %d bytes\n", msg_size); VIRT_UART_Transmit(&huart0, (uint8_t*)msg_to_transmit, msg_size); } if (VirtUart1RxMsg) { char msg_to_transmit[MAX_BUFFER_SIZE]; uint16_t msg_size = 0; VirtUart1RxMsg = RESET; msg_size = snprintf(msg_to_transmit, MAX_BUFFER_SIZE, "Channel RPMSG1: "); msg_size += snprintf(msg_to_transmit + msg_size, MAX_BUFFER_SIZE, "%s\n", VirtUart1ChannelBuffRx); log_info("size of the message to transmit = %d bytes\n", msg_size); VIRT_UART_Transmit(&huart1, (uint8_t*)msg_to_transmit, msg_size); } /* USER CODE BEGIN 3 */ } /* USER CODE END 3 *//* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { OPENAMP_check_for_message(); /* USER CODE END WHILE */ if (VirtUart0RxMsg) {
- Save your modifications.
10. Testing the modified firmware[edit | edit source]
10.1. Relaunch debug session[edit | edit source]
- By clicking on the "Debug" button, STM32CubeIDE relaunches the debug session after performing an incremental build to take into account your modification .
- If everything is correct, you will be back switch to "Debug Perspective" windows after reload of the new firmware.
10.2. Test[edit | edit source]
- Initialize the ttyRPMSG0 and ttyRPMSG1 configurations
stty -onlcr -echo -F /dev/ttyRPMSG0
stty -onlcr -echo -F /dev/ttyRPMSG1
- Read constantly the ttyRPMSG0 and ttyRPMSG1 channels in background
cat /dev/ttyRPMSG0 &
cat /dev/ttyRPMSG1 &
- Send a message on one ttyRPMSG0 channel and check the echo log
echo "Hello Virtual UART0" > /dev/ttyRPMSG0
Channel RPMSG0: Hello Virtual UART0
- Send a message on one ttyRPMSG1 channel and check the echo log
echo "Hello Virtual UART1" > /dev/ttyRPMSG1
Channel RPMSG1: Hello Virtual UART1
- Terminate the STM32CubeIDE debug session.