This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Usage[edit source]
The U-Boot$ template is used to prefix a command that must be executed on the U-Boot console, with a U-Boot-specific prompt.
Thanks to the u-boot-prompt
class defined in MediaWiki:Common.css, a double (or triple) click to select the command doesn't select the prompt.
Usage: {{U-Boot$}}
2. Basic examples[edit source]
You type | You get |
---|---|
help env command executed on the U-Boot console
{{U-Boot$}}help env<br>
env - environment handling commands
|
help env |
3. More examples[edit source]
You type | You get |
---|---|
2 commands executed on the U-Boot console and preformatted text block (space at the beginning of each line)
{{U-Boot$}}help env env - environment handling commands {{U-Boot$}}env default -a |
help env env - environment handling commands env default -a |
Command executed on the U-Boot console and preformatted text block (space at the beginning of each line)
{{U-Boot$}}help env
env - environment handling commands
|
help env env - environment handling commands |
Long command executed on the U-Boot console and preformatted text block (space at the beginning of each line)
{{U-Boot$}}this is a so long command executed on the U-Boot console that a horizontal scrolling bar is needed |
this is a so long command executed on the U-Boot console that a horizontal scrolling bar is needed
|
Template used within another public message box template
{{Info |
Message before the command
{{U-Boot$}}help env
env - environment handling commands
Message after the command
}}
|
|
Template used within another protected message box template
{{InternalInfo |
Message before the command
{{U-Boot$}}help env
env - environment handling commands
Message after the command
}}
|
4. Maintenance[edit source]
This template is a template common to all ST wikis.
Modifications must be done into the WikiModel. They must be reviewed by all ST wikis maintainers.
When approved, the template can be pushed/merged towards all ST wikis.
5. Code[edit source]