This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Usage
The STTextGrey template is used to get the hexadecimal code of the STMicroelectronics corporate color shade of grey (█) for normal text. Per default, this color is used in the wiki for normal text.
Usage: {{STTextGrey}}
2. Basic examples
You type | You get |
---|---|
Getting the hexadecimal code of the color
{{STTextGrey}} is the hexadecimal code of STMicroelectronics grey for normal text. |
#58585A is the hexadecimal code of STMicroelectronics grey for normal text. |
3. More examples
You type | You get |
---|---|
Parameter is ignored
This is a {{STTextGrey|'''STMicroelectronics'''}} corporate color |
This is a #58585A corporate color |
4. Maintenance
This template is a template common to all ST wikis.
Modifications must be done into the WikiModel. They must be reviewed by all ST wikis maintainers.
When approved, the template can be pushed/merged towards all ST wikis.
5. Code
#58585A