This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Usage
The ArticleToDelete template is used to request the deletion of a page. It should be added as the very first line on the page that you believe should be deleted from the wiki.
It puts a message box with a "pink garbage can" icon in the page, and adds this page to the Candidates for deletion category.
Wiki maintainers periodically have a look at this category, and delete the pages that belong to it.
Usage: {{ArticleToDelete | <reason> | <signature>}}
Where <reason> and <signature> are mandatory parameters:
- <reason> is the reason supplied for the deletion
- <signature> is the signature of the requester. It is recommended to use
~~~~
wiki markup to sign the request
2. Basic examples
You type | You get | ||
---|---|---|---|
Deletion requested: reason and signature supplied
{{ArticleToDelete | This is the reason for this request | ~~~~}} |
|
3. More examples
You type | You get | ||||
---|---|---|---|---|---|
Deletion requested: no reason supplied, no signature supplied
{{ArticleToDelete}} |
| ||||
Deletion requested: reason supplied with few words, no signature supplied
{{ArticleToDelete | This is the reason for this request}} |
| ||||
Deletion requested: no reason supplied, signature supplied
{{ArticleToDelete | | ~~~~}} |
| ||||
Deletion requested: reason supplied with a long sentence, signature supplied
{{ArticleToDelete | The reason is a long sentence. Lorem ipsum: isdem diebus Apollinaris Domitiani gener, paulo ante agens palatii Caesaris curam, ad Mesopotamiam missus a socero per militares numeros immodice scrutabatur, an quaedam altiora meditantis iam Galli. | ~~~~}} |
| ||||
Check that the spaces before and after the message
BEFORE{{ArticleToDelete | Check spaces | ~~~~}}AFTER<br> BEFORE {{ArticleToDelete | Check spaces | ~~~~}} AFTER |
BEFORE
BEFORE
AFTER |
4. Maintenance
This template is a template common to all ST wikis.
Modifications must be done into the WikiModel. They must be reviewed by all ST wikis maintainers.
When approved, the template can be pushed/merged towards all ST wikis.
5. Code
![]() |
This page is a candidate for deletion. No reason supplied! No signature supplied! Wiki maintainers: remember to check if anything links this page before deleting it. |