STM32MP13 Discovery kits - required material

Revision as of 15:38, 29 September 2022 by Registered User
Renaming.png This page is a candidate for renaming (move).
The requested new name is: STM32MP135 Discovery kits - required material .
The supplied reason is: STM32MP13 as such does not exist while STM32MP135 is the name of a line. Such a title is OK as long as it is made clear to the reader that the article applies to STM32MP135x-DK boards with STM32MP135F-DK used as an example. .
-- Registered User (-) 15:38, 29 September 2022 (CEST).
Wiki maintainers: remember to update the pages that link this page before renaming (moving) it.
Applicable for STM32MP13x lines


This article presents the mandatory and optional material needed for an STM32MP135x-DK More info green.png Discovery kit. It is valid for the STM32MP135F-DK Discovery kit More info green.png: the part numbers are specified in the STM32MP13 microprocessor part numbers article.

Warning white.png Warning
For assistance with starting up the boards, it is recommended to go through the related Starter Package articles: Category:Starter Package


Mandatory

PC Linux or Windows operating systems. See PC prerequisites for more details on the required configurations.
STM32MP135x-DK Discovery kit Flexible and complete development platform for the STM32MP135 microprocessor device including:
  • an MB1635 mother board
Power supply Including:
  • a USB Type-C cable (included in the packaging)
  • a USB Type-C charger (5 V, 3 A) (not included in the packaging)
microSD™ card Populated with OpenSTLinux distribution (Linux software), and providing extra storage capacity. A 2-Gbyte minimum microSD card is needed.
USB Micro-B cable In order to connect the STM32MP135x-DK Discovery kit to the PC through the USB Micro-B (ST-LINK/V2-1) connector
USB Type-C cable In order to connect the STM32MP135x-DK Discovery kit to a USB OTG device through the USB Type-C connector


Optional

USB keyboard and mouse Through its USB Type-A connectors, the STM32MP135x-DK Discovery kit can be equipped with a full-size keyboard and mouse
Ethernet cable To connect the STM32MP135x-DK Discovery kit to a network through the RJ45 connector

Optional, more devices and extension boards might be plugged to the STM32MP135x-DK Discovery kit thanks to expansion connectors such as:

  • the GPIO expansion connector
  • ...