This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.
1. Overview[edit source]
This step explains how to connect your board Linux® terminal to your host computer through the ST-LINK/V2-1.
It then describes how to execute basic commands with the Linux command line interface in order to get familiar with the Linux console.
2. Serial terminal[edit source]
The serial terminal allows communicating with the board through a UART serial interface.
- Install minicom
sudo apt-get install minicom
- Get the ttyACM device instance that needs to be used to access the ST-LINK/V2-1
ls /dev/ttyACM* /dev/ttyACM0
- Connect the minicom to the /dev/ttyACM0 device
minicom -D /dev/ttyACM0 Welcome to minicom 2.7 OPTIONS: I18n Compiled on Nov 15 2018, 20:18:47. Port /dev/ttyACM0, 15:56:03 Press CTRL-A Z to get help on special keys
- Press the reset button to reset the board. The boot log should be displayed on the minicom window:
For ecosystem release v3.1.0 :
NOTICE: CPU: STM32MP157CAC Rev.B NOTICE: Model: STMicroelectronics STM32MP157C-DK2 Discovery Board NOTICE: Board: MB1272 Var2.0 Rev.C-01 INFO: Reset reason (0x14): INFO: Pad Reset from NRST INFO: PMIC version = 0x10 INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000 INFO: FCONF: Reading firmware configuration information for: stm32mp_io INFO: Using SDMMC INFO: Instance 1 INFO: Boot used partition fsbl1 NOTICE: BL2: v2.4-r2.0(debug):v2.4-dirty NOTICE: BL2: Built : 16:43:51, Nov 17 2020 INFO: BL2: Doing platform setup INFO: RAM: DDR3-DDR3L 16bits 533000kHz INFO: Memory size = 0x20000000 (512 MB) INFO: BL2: Loading image id 31 INFO: Loading image id=31 at address 0x2ffff000 INFO: Image id=31 loaded: 0x2ffff000 - 0x2ffff226 INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0x2ffff000 INFO: FCONF: Reading firmware configuration information for: dyn_cfg INFO: FCONF: Reading firmware configuration information for: stm32mp1_firewall INFO: BL2: Loading image id 4 INFO: Loading image id=4 at address 0x2ffc5000 INFO: Image id=4 loaded: 0x2ffc5000 - 0x2ffd97ec WARNING: Not a known TEE, use default loading options. INFO: BL2: Skip loading image id 21 INFO: BL2: Skip loading image id 22 INFO: BL2: Loading image id 23 INFO: Loading image id=23 at address 0xc0500000 INFO: Image id=23 loaded: 0xc0500000 - 0xc051d252 INFO: BL2: Loading image id 26 INFO: Loading image id=26 at address 0x2ffc0000 INFO: Image id=26 loaded: 0x2ffc0000 - 0x2ffc46fd INFO: BL2: Loading image id 5 INFO: Loading image id=5 at address 0xc0100000 INFO: Image id=5 loaded: 0xc0100000 - 0xc01d3ee8 NOTICE: BL2: Booting BL32 INFO: Entry point address = 0x2ffc5000 INFO: SPSR = 0x1d3 NOTICE: SP_MIN: v2.4-r2.0(debug):v2.4-dirty NOTICE: SP_MIN: Built : 16:43:51, Nov 17 2020 INFO: ARM GICv2 driver initialized INFO: Set calibration timer to 60 sec INFO: stm32mp1 IWDG1 is secure INFO: SP_MIN: Initializing runtime services INFO: SP_MIN: Preparing exit to normal world U-Boot 2020.10-stm32mp-r2 (Oct 05 2020 - 15:15:32 +0000) CPU: STM32MP157CAC Rev.B Model: STMicroelectronics STM32MP157C-DK2 Discovery Board Board: stm32mp1 in trusted mode (st,stm32mp157c-dk2) Board: MB1272 Var2.0 Rev.C-01 DRAM: 512 MiB Clocks: - MPU : 650 MHz - MCU : 208.878 MHz - AXI : 266.500 MHz - PER : 24 MHz - DDR : 533 MHz WDT: Started with servicing (32s timeout) NAND: 0 MiB MMC: STM32 SD/MMC: 0, STM32 SD/MMC: 1 Loading Environment from MMC... OK In: serial Out: serial Err: serial Net: eth0: ethernet@5800a000 Hit any key to stop autoboot: 0 Boot over mmc0! switch to partitions #0, OK mmc0 is current device Scanning mmc 0:4... Found /mmc0_extlinux/stm32mp157c-dk2_extlinux.conf Retrieving file: /mmc0_extlinux/stm32mp157c-dk2_extlinux.conf 769 bytes read in 46 ms (15.6 KiB/s) Retrieving file: /splash_portrait.bmp 89462 bytes read in 49 ms (1.7 MiB/s) Select the boot mode 1: OpenSTLinux 2: stm32mp157c-dk2-a7-examples 3: stm32mp157c-dk2-m4-examples Enter choice: 1: OpenSTLinux Retrieving file: /st-image-resize-initrd 3635706 bytes read in 199 ms (17.4 MiB/s) Retrieving file: /uImage 7464336 bytes read in 361 ms (19.7 MiB/s) append: root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=ttySTM0,115200 Retrieving file: /stm32mp157c-dk2.dtb 116881 bytes read in 50 ms (2.2 MiB/s) ## Booting kernel from Legacy Image at c2000000 ... Image Name: Linux-5.10.61 Created: 2021-08-26 12:51:21 UTC Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 7464272 Bytes = 7.1 MiB Load Address: c2000040 Entry Point: c2000040 Verifying Checksum ... OK ## Flattened Device Tree blob at c4000000 Booting using the fdt blob at 0xc4000000 XIP Kernel Image Loading Ramdisk to cfc88000, end cffff9fa ... OK Loading Device Tree to cfc68000, end cfc87890 ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 5.10.61 (oe-user@oe-host) (arm-ostl-linux-gnueabi-gcc (GCC) 9.3.0, GNU ld (GNU Binutils) 2.34.0.20200220) #1 SMP PREEMPT Thu Aug 26 12:51:21 UTC 2021 [ 0.000000] CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c5387d [ 0.000000] CPU: div instructions available: patching division code [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] OF: fdt: Machine model: STMicroelectronics STM32MP157C-DK2 Discovery Board [ 0.000000] Memory policy: Data cache writealloc [ 0.000000] Reserved memory: created DMA memory pool at 0x10000000, size 0 MiB [ 0.000000] OF: reserved mem: initialized node mcuram2@10000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x10040000, size 0 MiB [ 0.000000] OF: reserved mem: initialized node vdev0vring0@10040000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x10041000, size 0 MiB [ 0.000000] OF: reserved mem: initialized node vdev0vring1@10041000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x10042000, size 0 MiB [ 0.000000] OF: reserved mem: initialized node vdev0buffer@10042000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x10048000, size 0 MiB [ 0.000000] OF: reserved mem: initialized node mcu_rsc_table@10048000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x30000000, size 0 MiB [ 0.000000] OF: reserved mem: initialized node mcuram@30000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x38000000, size 0 MiB [ 0.000000] OF: reserved mem: initialized node retram@38000000, compatible id shared-dma-pool [ 0.000000] cma: Reserved 128 MiB at 0xc7800000 [ 0.000000] Zone ranges: [ 0.000000] Normal [mem 0x00000000c0000000-0x00000000dfffffff] [ 0.000000] HighMem empty [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x00000000c0000000-0x00000000d3ffffff] [ 0.000000] node 0: [mem 0x00000000d4000000-0x00000000d7ffffff] [ 0.000000] node 0: [mem 0x00000000d8000000-0x00000000dfcfffff] [ 0.000000] node 0: [mem 0x00000000dfd00000-0x00000000dffeffff] [ 0.000000] node 0: [mem 0x00000000dfff0000-0x00000000dfffffff] [ 0.000000] Initmem setup node 0 [mem 0x00000000c0000000-0x00000000dfffffff] [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: MIGRATE_INFO_TYPE not supported. [ 0.000000] psci: SMC Calling Convention v1.2 [ 0.000000] percpu: Embedded 20 pages/cpu s51788 r8192 d21940 u81920 [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 129920 [ 0.000000] Kernel command line: root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=ttySTM0,115200 [ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes, linear) [ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] Memory: 297400K/524288K available (11264K kernel code, 1207K rwdata, 3308K rodata, 1024K init, 239K bss, 95816K reserved, 131072K cma-reserved, 0K highmem) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] rcu: RCU event tracing is enabled. [ 0.000000] Trampoline variant of Tasks RCU enabled. [ 0.000000] Tracing variant of Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 10 jiffies. [ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16 [ 0.000000] random: get_random_bytes called from start_kernel+0x388/0x560 with crng_init=0 [ 0.000000] arch_timer: cp15 timer(s) running at 24.00MHz (virt). [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x588fe9dc0, max_idle_ns: 440795202592 ns [ 0.000010] sched_clock: 56 bits at 24MHz, resolution 41ns, wraps every 4398046511097ns [ 0.000031] Switching to timer-based delay loop, resolution 41ns [ 0.001774] Console: colour dummy device 80x30 [ 0.001836] Calibrating delay loop (skipped), value calculated using timer frequency.. 48.00 BogoMIPS (lpj=240000) [ 0.001867] pid_max: default: 32768 minimum: 301 [ 0.002134] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes, linear) [ 0.002159] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes, linear) [ 0.003520] CPU: Testing write buffer coherency: ok [ 0.003980] /cpus/cpu@0 missing clock-frequency property [ 0.004027] /cpus/cpu@1 missing clock-frequency property [ 0.004049] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000 [ 0.005344] Setting up static identity map for 0xc0100000 - 0xc0100060 [ 0.005553] rcu: Hierarchical SRCU implementation. [ 0.007006] smp: Bringing up secondary CPUs ... [ 0.008237] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001 [ 0.008499] smp: Brought up 1 node, 2 CPUs [ 0.008531] SMP: Total of 2 processors activated (96.00 BogoMIPS). [ 0.008545] CPU: All CPU(s) started in SVC mode. [ 0.009408] devtmpfs: initialized [ 0.047138] VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5 [ 0.047532] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns [ 0.047573] futex hash table entries: 512 (order: 3, 32768 bytes, linear) [ 0.055083] pinctrl core: initialized pinctrl subsystem [ 0.057060] NET: Registered protocol family 16 [ 0.060540] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 0.062457] thermal_sys: Registered thermal governor 'step_wise' [ 0.062872] cpuidle: using governor menu [ 0.063294] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers. [ 0.063317] hw-breakpoint: maximum watchpoint size is 8 bytes. [ 0.063766] Serial: AMBA PL011 UART driver [ 0.119032] stm32-pm-domain pm_domain: domain core-ret-power-domain registered [ 0.119084] stm32-pm-domain pm_domain: subdomain core-power-domain registered [ 0.119104] stm32-pm-domain pm_domain: domains probed [ 0.147707] SCSI subsystem initialized [ 0.148595] usbcore: registered new interface driver usbfs [ 0.148688] usbcore: registered new interface driver hub [ 0.148786] usbcore: registered new device driver usb [ 0.149113] pps_core: LinuxPPS API ver. 1 registered [ 0.149133] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 0.149173] PTP clock support registered [ 0.150100] arm-scmi firmware:scmi0: SCMI Notifications - Core Enabled. [ 0.150329] arm-scmi firmware:scmi0: SCMI Protocol v2.0 'ST:' Firmware version 0x0 [ 0.153834] clocksource: Switched to clocksource arch_sys_counter [ 1.588103] simple-framebuffer dfd00000.framebuffer: framebuffer at 0xdfd00000, 0xbb800 bytes, mapped to 0x(ptrval) [ 1.588142] simple-framebuffer dfd00000.framebuffer: format=r5g6b5, mode=480x800x16, linelength=960 [ 1.588594] simple-framebuffer dfd00000.framebuffer: fb0: simplefb registered! [ 1.603245] NET: Registered protocol family 2 [ 1.603493] IP idents hash table entries: 8192 (order: 4, 65536 bytes, linear) [ 1.605097] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes, linear) [ 1.605271] TCP established hash table entries: 4096 (order: 2, 16384 bytes, linear) [ 1.605348] TCP bind hash table entries: 4096 (order: 3, 32768 bytes, linear) [ 1.605448] TCP: Hash tables configured (established 4096 bind 4096) [ 1.605628] UDP hash table entries: 256 (order: 1, 8192 bytes, linear) [ 1.605683] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes, linear) [ 1.606333] NET: Registered protocol family 1 [ 1.607404] RPC: Registered named UNIX socket transport module. [ 1.607434] RPC: Registered udp transport module. [ 1.607448] RPC: Registered tcp transport module. [ 1.607461] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 1.607859] Trying to unpack rootfs image as initramfs... [ 1.983690] Freeing initrd memory: 3552K [ 1.985037] hw perfevents: enabled with armv7_cortex_a7 PMU driver, 5 counters available [ 1.987148] Initialise system trusted keyrings [ 1.987620] workingset: timestamp_bits=14 max_order=17 bucket_order=3 [ 1.998736] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 2.000250] NFS: Registering the id_resolver key type [ 2.000312] Key type id_resolver registered [ 2.000326] Key type id_legacy registered [ 2.000522] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 2.000544] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering... [ 2.000749] ntfs: driver 2.1.32 [Flags: R/O]. [ 2.001086] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc. [ 2.002011] fuse: init (API version 7.32) [ 2.003145] NET: Registered protocol family 38 [ 2.003176] Key type asymmetric registered [ 2.003191] Asymmetric key parser 'x509' registered [ 2.003264] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246) [ 2.003283] io scheduler mq-deadline registered [ 2.003297] io scheduler kyber registered [ 2.016958] STM32 USART driver initialized [ 2.040640] brd: module loaded [ 2.041089] random: fast init done [ 2.045787] random: crng init done [ 2.055460] loop: module loaded [ 2.061753] libphy: Fixed MDIO Bus: probed [ 2.064171] CAN device driver interface [ 2.066402] pegasus: v0.9.3 (2013/04/25), Pegasus/Pegasus II USB Ethernet driver [ 2.066519] usbcore: registered new interface driver pegasus [ 2.066609] usbcore: registered new interface driver asix [ 2.066678] usbcore: registered new interface driver ax88179_178a [ 2.066746] usbcore: registered new interface driver cdc_ether [ 2.066833] usbcore: registered new interface driver smsc75xx [ 2.066919] usbcore: registered new interface driver smsc95xx [ 2.066998] usbcore: registered new interface driver net1080 [ 2.067066] usbcore: registered new interface driver cdc_subset [ 2.067130] usbcore: registered new interface driver zaurus [ 2.067227] usbcore: registered new interface driver cdc_ncm [ 2.068856] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver [ 2.068920] ehci-platform: EHCI generic platform driver [ 2.069417] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver [ 2.069463] ohci-platform: OHCI generic platform driver [ 2.070266] usbcore: registered new interface driver usb-storage [ 2.074652] i2c /dev entries driver [ 2.079761] stm32-cpufreq stm32-cpufreq: Failed to get chip info: -517 [ 2.081106] sdhci: Secure Digital Host Controller Interface driver [ 2.081128] sdhci: Copyright(c) Pierre Ossman [ 2.081142] Synopsys Designware Multimedia Card Interface Driver [ 2.081653] sdhci-pltfm: SDHCI platform and OF driver helper [ 2.083071] ledtrig-cpu: registered to indicate activity on CPUs [ 2.083337] SMCCC: SOC_ID: ID = jep106:0020:0500 Revision = 0x00002000 [ 2.083918] usbcore: registered new interface driver usbhid [ 2.083939] usbhid: USB HID core driver [ 2.085537] remoteproc remoteproc0: releasing m4 [ 2.088361] NET: Registered protocol family 17 [ 2.088412] can: controller area network core [ 2.088535] NET: Registered protocol family 29 [ 2.088552] can: raw protocol [ 2.088571] can: broadcast manager protocol [ 2.088596] can: netlink gateway - max_hops=1 [ 2.089464] Key type dns_resolver registered [ 2.089657] ThumbEE CPU extension supported. [ 2.089691] Registering SWP/SWPB emulation handler [ 2.090119] registered taskstats version 1 [ 2.090152] Loading compiled-in X.509 certificates [ 2.134694] stm32-mdma 58000000.dma-controller: STM32 MDMA driver registered [ 2.138476] stm32-dma 48000000.dma-controller: STM32 DMA driver registered [ 2.141256] stm32-dma 48001000.dma-controller: STM32 DMA driver registered [ 2.151868] stm_thermal 50028000.thermal: stm_thermal_probe: Driver initialized successfully [ 2.159451] remoteproc remoteproc0: releasing m4 [ 2.160420] /soc/interrupt-controller@5000d000: bank0 [ 2.160453] /soc/interrupt-controller@5000d000: bank1 [ 2.160474] /soc/interrupt-controller@5000d000: bank2 [ 2.165248] stm32mp157-pinctrl soc:pin-controller@50002000: GPIOA bank added [ 2.167792] stm32mp157-pinctrl soc:pin-controller@50002000: GPIOB bank added [ 2.170337] stm32mp157-pinctrl soc:pin-controller@50002000: GPIOC bank added [ 2.172806] stm32mp157-pinctrl soc:pin-controller@50002000: GPIOD bank added [ 2.175405] stm32mp157-pinctrl soc:pin-controller@50002000: GPIOE bank added [ 2.177900] stm32mp157-pinctrl soc:pin-controller@50002000: GPIOF bank added [ 2.180435] stm32mp157-pinctrl soc:pin-controller@50002000: GPIOG bank added [ 2.183197] stm32mp157-pinctrl soc:pin-controller@50002000: GPIOH bank added [ 2.185640] stm32mp157-pinctrl soc:pin-controller@50002000: GPIOI bank added [ 2.185996] stm32mp157-pinctrl soc:pin-controller@50002000: Pinctrl STM32 initialized [ 2.189490] stm32mp157-pinctrl soc:pin-controller-z@54004000: GPIOZ bank added [ 2.189538] stm32mp157-pinctrl soc:pin-controller-z@54004000: Pinctrl STM32 initialized [ 2.193157] 4000e000.serial: ttySTM3 at MMIO 0x4000e000 (irq = 61, base_baud = 4000000) is a stm32-usart [ 2.193506] serial serial0: tty port ttySTM3 registered [ 2.195862] stm32-usart 40010000.serial: interrupt mode for rx (no dma) [ 2.195894] stm32-usart 40010000.serial: interrupt mode for tx (no dma) [ 2.195937] 40010000.serial: ttySTM0 at MMIO 0x40010000 (irq = 62, base_baud = 4000000) is a stm32-usart [ 3.440846] printk: console [ttySTM0] enabled [ 3.452937] stm32-dwmac 5800a000.ethernet: IRQ eth_lpi not found [ 3.457931] stm32-dwmac 5800a000.ethernet: no reset control found [ 3.464491] stm32-dwmac 5800a000.ethernet: User ID: 0x40, Synopsys ID: 0x42 [ 3.470693] stm32-dwmac 5800a000.ethernet: DWMAC4/5 [ 3.475747] stm32-dwmac 5800a000.ethernet: DMA HW capability register supported [ 3.482935] stm32-dwmac 5800a000.ethernet: RX Checksum Offload Engine supported [ 3.490387] stm32-dwmac 5800a000.ethernet: TX Checksum insertion supported [ 3.497197] stm32-dwmac 5800a000.ethernet: Wake-Up On Lan supported [ 3.503613] stm32-dwmac 5800a000.ethernet: TSO supported [ 3.508816] stm32-dwmac 5800a000.ethernet: Enable RX Mitigation via HW Watchdog Timer [ 3.516642] stm32-dwmac 5800a000.ethernet: Enabled Flow TC (entries=2) [ 3.523222] stm32-dwmac 5800a000.ethernet: TSO feature enabled [ 3.529022] stm32-dwmac 5800a000.ethernet: Using 32 bits DMA width [ 3.537556] libphy: stmmac: probed [ 3.555461] stm32_rtc 5c004000.rtc: registered as rtc0 [ 3.559303] stm32_rtc 5c004000.rtc: setting system clock to 2000-01-01T00:52:23 UTC (946687943) [ 3.568835] stm32_rtc 5c004000.rtc: Date/Time must be initialized [ 3.574113] stm32_rtc 5c004000.rtc: registered rev:1.2 [ 3.610067] stm32f7-i2c 40012000.i2c: STM32F7 I2C-0 bus adapter [ 3.643941] stpmic1 1-0033: PMIC Chip Version: 0x10 [ 3.653335] vddcore: supplied by vin [ 3.658670] vdd_ddr: supplied by vin [ 3.663894] vdd: supplied by vin [ 3.668858] v3v3: supplied by vin [ 3.673866] v1v8_audio: supplied by v3v3 [ 3.680403] v3v3_hdmi: supplied by vin [ 3.686331] vtt_ddr: supplied by vdd_ddr [ 3.692147] vdd_usb: supplied by vin [ 3.695135] vdda: supplied by vin [ 3.701004] v1v2_hdmi: supplied by v3v3 [ 3.706731] vref_ddr: supplied by vin [ 3.712386] bst_out: supplied by vin [ 3.715528] vbus_otg: supplied by bst_out [ 3.719479] vbus_sw: supplied by bst_out [ 3.726031] input: pmic_onkey as /devices/platform/soc/5c002000.i2c/i2c-1/1-0033/5c002000.i2c:stpmic@33:onkey/input/input0 [ 3.736935] stm32f7-i2c 5c002000.i2c: STM32F7 I2C-1 bus adapter [ 3.745950] mmci-pl18x 58005000.sdmmc: Got CD GPIO [ 3.750600] mmci-pl18x 58005000.sdmmc: mmc0: PL180 manf 53 rev2 at 0x58005000 irq 54,0 (pio) [ 3.786876] mmci-pl18x 58007000.sdmmc: allocated mmc-pwrseq [ 3.792041] mmci-pl18x 58007000.sdmmc: mmc1: PL180 manf 53 rev1 at 0x58007000 irq 55,0 (pio) [ 3.831392] stm32-ipcc 4c001000.mailbox: ipcc rev:1.0 enabled, 6 chans, proc 0 [ 3.840434] stm32-rproc 10000000.m4: wdg irq registered [ 3.847596] mmc0: new high speed SDHC card at address aaaa [ 3.854106] remoteproc remoteproc0: m4 is available [ 3.857649] mmcblk0: mmc0:aaaa SS16G 14.8 GiB [ 3.862930] reg11: supplied by vdd [ 3.865953] reg18: supplied by vdd [ 3.870743] stm32-usbphyc 5a006000.usbphyc: registered rev:1.0 [ 3.883939] mmc1: queuing unknown CIS tuple 0x80 (2 bytes) [ 3.889546] mmc1: queuing unknown CIS tuple 0x80 (3 bytes) [ 3.895386] mmc1: queuing unknown CIS tuple 0x80 (3 bytes) [ 3.902070] mmcblk0: p1 p2 p3 p4 p5 p6 p7 [ 3.905244] mmc1: queuing unknown CIS tuple 0x80 (7 bytes) [ 3.913412] mmc1: queuing unknown CIS tuple 0x80 (3 bytes) [ 3.923644] dwc2 49000000.usb-otg: supply vusb_d not found, using dummy regulator [ 3.930300] dwc2 49000000.usb-otg: supply vusb_a not found, using dummy regulator [ 3.939189] mmc1: queuing unknown CIS tuple 0x80 (6 bytes) [ 4.028105] mmc1: new high speed SDIO card at address 0001 [ 4.074156] dwc2 49000000.usb-otg: EPs: 9, dedicated fifos, 952 entries in SPRAM [ 4.080866] dwc2 49000000.usb-otg: DWC OTG Controller [ 4.085367] dwc2 49000000.usb-otg: new USB bus registered, assigned bus number 1 [ 4.092713] dwc2 49000000.usb-otg: irq 87, io mem 0x49000000 [ 4.099721] hub 1-0:1.0: USB hub found [ 4.102154] hub 1-0:1.0: 1 port detected [ 4.108740] ehci-platform 5800d000.usbh-ehci: EHCI Host Controller [ 4.113556] ehci-platform 5800d000.usbh-ehci: new USB bus registered, assigned bus number 2 [ 4.122807] ehci-platform 5800d000.usbh-ehci: irq 64, io mem 0x5800d000 [ 4.153888] ehci-platform 5800d000.usbh-ehci: USB 2.0 started, EHCI 1.00 [ 4.160615] hub 2-0:1.0: USB hub found [ 4.163045] hub 2-0:1.0: 2 ports detected [ 4.174201] i2c i2c-0: Added multiplexed i2c bus 2 [ 4.183344] fb0: switching to stmdrmfb from simple [ 4.187614] input: generic ft5x06 (11) as /devices/platform/soc/40012000.i2c/i2c-0/0-002a/input/input1 [ 4.194595] [drm] Initialized stm 1.0.0 20170330 for 5a001000.display-controller on minor 0 [ 4.210373] Freeing unused kernel memory: 1024K [ 4.254271] Run /init as init process [ 4.464017] usb 2-1: new high-speed USB device number 2 using ehci-platform Starting version 244.5+ [ 4.666279] hub 2-1:1.0: USB hub found [ 4.668900] hub 2-1:1.0: 4 ports detected [ 6.032881] EXT4-fs (mmcblk0p6): recovery complete [ 6.051434] EXT4-fs (mmcblk0p6): mounted filesystem with ordered data mode. Opts: (null) [ 6.596338] systemd[1]: System time before build time, advancing clock. [ 6.732214] NET: Registered protocol family 10 [ 6.772361] Segment Routing with IPv6 [ 6.833501] systemd[1]: systemd 244.5+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS -ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid) [ 6.860879] systemd[1]: Detected architecture arm. Welcome to ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17 (dunfell)! [ 6.978306] systemd[1]: Set hostname to <stm32mp1>. [ 6.991891] systemd[1]: Hardware watchdog 'STM32 Independent Watchdog', version 0 [ 6.999214] systemd[1]: Set hardware watchdog to 32s. [ 7.945719] systemd[1]: Unnecessary job for /dev/ttySTM0 was removed. [ 7.959034] systemd[1]: Created slice system-getty.slice. [ OK ] Created slice system-getty.slice. [ 7.996661] systemd[1]: Created slice system-serial\x2dgetty.slice. [ OK ] Created slice system-serial\x2dgetty.slice. [ 8.036312] systemd[1]: Created slice User and Session Slice. [ OK ] Created slice User and Session Slice. [ 8.074810] systemd[1]: Started Dispatch Password Requests to Console Directory Watch. [ OK ] Started Dispatch Password …ts to Console Directory Watch. [ 8.114651] systemd[1]: Started Forward Password Requests to Wall Directory Watch. [ OK ] Started Forward Password R…uests to Wall Directory Watch. [ 8.154491] systemd[1]: Reached target Paths. [ OK ] Reached target Paths. [ 8.184196] systemd[1]: Reached target Remote File Systems. [ OK ] Reached target Remote File Systems. [ 8.224172] systemd[1]: Reached target Slices. [ OK ] Reached target Slices. [ 8.254227] systemd[1]: Reached target Swap. [ OK ] Reached target Swap. [ 8.315557] systemd[1]: Listening on RPCbind Server Activation Socket. [ OK ] Listening on RPCbind Server Activation Socket. [ 8.354253] systemd[1]: Reached target RPC Port Mapper. [ OK ] Reached target RPC Port Mapper. [ 8.395423] systemd[1]: Listening on Syslog Socket. [ OK ] Listening on Syslog Socket. [ 8.451033] systemd[1]: Listening on Process Core Dump Socket. [ OK ] Listening on Process Core Dump Socket. [ 8.484811] systemd[1]: Listening on initctl Compatibility Named Pipe. [ OK ] Listening on initctl Compatibility Named Pipe. [ 8.530894] systemd[1]: Condition check resulted in Journal Audit Socket being skipped. [ 8.538771] systemd[1]: Listening on Journal Socket (/dev/log). [ OK ] Listening on Journal Socket (/dev/log). [ 8.575359] systemd[1]: Listening on Journal Socket. [ OK ] Listening on Journal Socket. [ 8.615652] systemd[1]: Listening on Network Service Netlink Socket. [ OK ] Listening on Network Service Netlink Socket. [ 8.655292] systemd[1]: Listening on udev Control Socket. [ OK ] Listening on udev Control Socket. [ 8.694907] systemd[1]: Listening on udev Kernel Socket. [ OK ] Listening on udev Kernel Socket. [ 8.735331] systemd[1]: Condition check resulted in Huge Pages File System being skipped. [ 8.749795] systemd[1]: Mounting POSIX Message Queue File System... Mounting POSIX Message Queue File System... [ 8.791552] systemd[1]: Mounting Kernel Debug File System... Mounting Kernel Debug File System... [ 8.835978] systemd[1]: Mounting Temporary Directory (/tmp)... Mounting Temporary Directory (/tmp)... [ 8.892332] systemd[1]: Starting Create list of static device nodes for the current kernel... Starting Create list of st…odes for the current kernel... [ 8.941554] systemd[1]: Starting Mount partitions... Starting Mount partitions... [ 8.990559] systemd[1]: Started Hardware RNG Entropy Gatherer Daemon. [ OK ] Started Hardware RNG Entropy Gatherer Daemon. [ 9.033776] systemd[1]: Starting RPC Bind... Starting RPC Bind... [ 9.064670] systemd[1]: Condition check resulted in File System Check on Root Device being skipped. [ 9.086042] systemd[1]: Starting Journal Service... Starting Journal Service... [ 9.110776] systemd[1]: Condition check resulted in Load Kernel Modules being skipped. [ 9.151129] systemd[1]: Mounting FUSE Control File System... Mounting FUSE Control File System... [ 9.203038] systemd[1]: Mounting Kernel Configuration File System... Mounting Kernel Configuration File System... [ 9.269144] systemd[1]: Starting Remount Root and Kernel File Systems... Starting Remount Root and Kernel File Systems... [ 9.321857] systemd[1]: Starting Apply Kernel Variables... Starting Apply Kernel Variables... [ 9.361088] EXT4-fs (mmcblk0p6): re-mounted. Opts: (null) [ 9.418655] systemd[1]: Starting udev Coldplug all Devices... Starting udev Coldplug all Devices... [ 9.475264] systemd[1]: Started RPC Bind. [ OK ] Started RPC Bind. [ 9.495852] systemd[1]: Mounted POSIX Message Queue File System. [ OK ] Mounted POSIX Message Queue File System. [ 9.515231] systemd[1]: Mounted Kernel Debug File System. [ OK ] Mounted Kernel Debug File System. [ 9.565159] systemd[1]: Mounted Temporary Directory (/tmp). [ OK ] Mounted Temporary Directory (/tmp). [ 9.595658] systemd[1]: Started Create list of static device nodes for the current kernel. [ OK ] Started Create list of sta… nodes for the current kernel. [ 9.619981] systemd[1]: Mounted FUSE Control File System. [ OK ] Mounted FUSE Control File System. [ 9.668540] EXT4-fs (mmcblk0p4): recovery complete [ 9.671943] EXT4-fs (mmcblk0p4): mounted filesystem with ordered data mode. Opts: (null) [ 9.705194] systemd[1]: Started Journal Service. [ OK ] Started Journal Service. [ OK ] Mounted Kernel Configuration File System. [ OK ] Started Remount Root and Kernel File Systems. [ OK ] Started Apply Kernel Variables. [ OK ] Started Starts Psplash Boot screen. Starting Flush Journal to Persistent Storage... Starting Create Static Device Nodes in /dev... [ 10.102537] systemd-journald[289]: Received client request to flush runtime journal. [ OK ] Started Flush Journal to Persistent Storage. [ OK ] Started Create Static Device Nodes in /dev. [ OK ] Reached target Local File Systems (Pre). [ 10.270906] EXT4-fs (mmcblk0p5): recovery complete [ 10.287007] EXT4-fs (mmcblk0p5): mounted filesystem with ordered data mode. Opts: (null) Mounting /var/volatile... Starting udev Kernel Device Manager... [ OK ] Mounted /var/volatile. Starting Load/Save Random Seed... [ OK ] Started Load/Save Random Seed. [ OK ] Started udev Kernel Device Manager. [ 11.041091] EXT4-fs (mmcblk0p7): recovery complete [ 11.076716] EXT4-fs (mmcblk0p7): mounted filesystem with ordered data mode. Opts: (null) [ OK ] Started Mount partitions. [ OK ] Reached target Local File Systems. Starting Create Volatile Files and Directories... [ OK ] Started Create Volatile Files and Directories. Starting Network Time Synchronization... Starting Update UTMP about System Boot/Shutdown... [ OK ] Started Update UTMP about System Boot/Shutdown. [ 12.846472] st,stm32-i2s 4000b000.audio-controller: No cache defaults, reading back from HW [ OK ] Reached target Hardware activated USB gadget. [ OK ] Started Network Time Synchronization. [ 13.019059] stm32-hash 54002000.hash: will run requests pump with realtime priority [ OK ] Reached target 13.038293] stm32-cryp 54001000.cryp: will run requests pump with realtime priority 39mSystem Time Set. [ 13.073591] stm32-hash 54002000.hash: Init HASH done HW ver 23 DMA mode 1 [ 13.094995] stm32-cryp 54001000.cryp: Initialized [ OK ] Reached target System Time Synchronized. [ OK ] Started udev Coldplug all Devices. [ 13.150247] Bluetooth: Core ver 2.22 [ 13.176528] NET: Registered protocol family 31 [ 13.179605] Bluetooth: HCI device and connection manager initialized [ OK ] Reached target System Initialization. [ OK ] Started Dail[ 13.228094] Bluetooth: HCI socket layer initialized [ 13.232603] Bluetooth: L2CAP socket layer initialized y apt download activities. [ OK ] Started Daily Cleanup of Temporary Directories. [ OK ] Reached target Timers. [ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket. [ 13.314554] Bluetooth: SCO socket layer initialized [ 13.318475] stm32-crc32 58009000.crc: Initialized [ OK ] Listening on D-Bus System Message Bus Socket. [ 13.362752] Bluetooth: HCI UART driver ver 2.3 [ 13.386459] galcore: loading out-of-tree module taints kernel. [ 13.438729] Bluetooth: HCI UART protocol H4 registered [ 13.494532] Bluetooth: HCI UART protocol Broadcom registered [ OK ] Listening on dropbear.socket. [ 13.581399] Galcore version 6.4.3.279124 [ OK ] Reached target Sockets. [ OK ] Reached target Basic System. [ OK ] Started Kernel Logging Service. [ OK ] Started System Logging Service. [ 13.925158] Bluetooth: hci0: BCM: chip id 94 [ 13.928772] Bluetooth: hci0: BCM: features 0x2e [ 13.934081] Bluetooth: hci0: BCM43430A1 [ 13.936561] Bluetooth: hci0: BCM43430A1 (001.002.009) build 0000 [ OK ] Started D-Bus System Message Bus. [ 13.958684] Bluetooth: hci0: BCM43430A1 'brcm/BCM43430A1.hcd' Patch [ 14.063241] cs42l51 0-004a: Cirrus Logic CS42L51, Revision: 01 [ 14.118266] cfg80211: Loading compiled-in X.509 certificates for regulatory database [ 14.299208] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7' Starting IPv6 Packet Filtering Framework... Starting IPv4 Packet Filtering Framework... [ 14.626533] Bluetooth: hci0: BCM4343WA1 37.4MHz Murata Type-1DX BT4.2-0093 [ 14.632288] Bluetooth: hci0: BCM43430A1 (001.002.009) build 0395 Starting Netdata, Real-time performance monitoring... [ 14.670339] brcmfmac: brcmf_fw_alloc_request: using brcm/brcmfmac43430-sdio for chip BCM43430/1 Starting Login Service... [ OK ] Started TEE Supplicant. Starting Enable USB Ethernet gadget... [ 14.894361] brcmfmac: brcmf_fw_alloc_request: using brcm/brcmfmac43430-sdio for chip BCM43430/1 [ 15.034487] brcmfmac: brcmf_c_preinit_dcmds: Firmware: BCM43430/1 wl0: Feb 16 2020 22:39:24 version 7.45.98.97 (r724416 CY) FWID 01-bf41ed64 [ OK ] Started IPv6 Packet Filtering Framework. [ OK ] Started IPv4 Packet Filtering Framework. [ 15.460865] using random self ethernet address [ 15.469983] using random host ethernet address [ 15.751976] usb0: HOST MAC 40:4d:17:1e:53:f1 [ 15.755103] usb0: MAC 9a:c6:c4:0d:ac:3d [ 15.758730] dwc2 49000000.usb-otg: bound driver configfs-gadget [ OK ] Started Enable USB Ethernet gadget. [ OK ] Started Netdata, Real-time performance monitoring. [ OK ] Started Login Service. [ OK ] Created slice system-systemd\x2dbacklight.slice. [ OK ] Created slice system-weston.slice. [ OK ] Reached target Network (Pre). [ OK ] Listening on Load/Save RF …itch Status /dev/rfkill Watch. Starting Save/Restore Sound Card State... Starting Bluetooth service... Starting Load/Save Screen …of backlight:5a000000.dsi.0... Starting Network Service... [ OK ] Started Save/Restore Sound Card State. [ OK ] Started Load/Save Screen B…s of backlight:5a000000.dsi.0. [ OK ] Reached target Sound Card. Starting Load/Save RF Kill Switch Status... [ OK ] Started Bluetooth service. [ OK ] Started Load/Save RF Kill Switch Status. [ OK ] Reached target Bluetooth. Starting Hostname Service... [ OK ] Started Network Service. [ 19.074044] stm32-dwmac 5800a000.ethernet eth0: PHY [stmmac-0:00] driver [RTL8211F Gigabit Ethernet] (irq=POLL) Starting Network Name Resolution... [ 19.098516] dwmac4: Master AXI performs any burst length [ 19.102443] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found [ 19.144155] stm32-dwmac 5800a000.ethernet eth0: IEEE 1588-2008 Advanced Timestamp supported [ 19.173371] stm32-dwmac 5800a000.ethernet eth0: registered PTP clock [ 19.201721] stm32-dwmac 5800a000.ethernet eth0: configuring for phy/rgmii-id link mode [ OK ] Started Hostname Service. [ OK ] Started Network Name Resolution. [ OK ] Reached target Network. [ OK ] Reached target Host and Network Name Lookups. Starting Avahi mDNS/DNS-SD Stack... [ OK ] Started IIO Daemon. [ OK ] Started Respond to IPv6 Node Information Queries. Starting Sound Service... [ OK ] Started Network Router Discovery Daemon. Starting Permit User Sessions... Starting Target Communication Framework agent... [ OK ] Started Avahi mDNS/DNS-SD Stack. [ OK ] Started Permit User Sessions. [ OK ] Started Getty on tty1. [ OK ] Started Serial Getty on ttySTM0. [ OK ] Reached target Login Prompts. Starting Weston Wayland Compositor (on tty7)... [ OK ] Started Target Communication Framework agent. [ OK ] Started Sound Service. [ OK ] Reached target Multi-User System. Starting Update UTMP about System Runlevel Changes... [ OK ] Started Update UTMP about System Runlevel Changes. [ OK ] Started Weston Wayland Compositor (on tty7). ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17 stm32mp1 ttySTM0 stm32mp1 login: root (automatic login) Last login: Sun Sep 20 10:44:13 UTC 2020 on tty7 root@stm32mp1:~#
3. Basic commands[edit source]
3.1. Printing distribution specific information[edit source]
For ecosystem release v3.1.0 :
root@stm32mp1:~# cat /etc/build
-----------------------
Build Configuration: |
-----------------------
BB_VERSION = 1.46.0
BUILD_SYS = x86_64-linux
NATIVELSBSTRING = universal
TARGET_SYS = arm-ostl-linux-gnueabi
MACHINE = stm32mp1
DISTRO = openstlinux-weston
DISTRO_VERSION = 3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17
TUNE_FEATURES = arm vfp cortexa7 neon vfpv4 thumb callconvention-hard
TARGET_FPU = hard
MANIFESTVERSION = ostl-21-11-17-rc4
DISTRO_CODENAME = dunfell
ACCEPT_EULA_stm32mp1 = 1
GCCVERSION = 9.%
PREFERRED_PROVIDER_virtual/kernel = linux-stm32mp
PREFERRED_VERSION_linux-stm32mp =
-----------------------
Layer Revisions: |
-----------------------
meta-python = default.xml:2e7e98cd0cb82db214b13224c71134b9335a719b
meta-oe = default.xml:2e7e98cd0cb82db214b13224c71134b9335a719b
meta-gnome = default.xml:2e7e98cd0cb82db214b13224c71134b9335a719b
meta-initramfs = default.xml:2e7e98cd0cb82db214b13224c71134b9335a719b
meta-multimedia = default.xml:2e7e98cd0cb82db214b13224c71134b9335a719b
meta-networking = default.xml:2e7e98cd0cb82db214b13224c71134b9335a719b
meta-webserver = default.xml:2e7e98cd0cb82db214b13224c71134b9335a719b
meta-filesystems = default.xml:2e7e98cd0cb82db214b13224c71134b9335a719b
meta-perl = default.xml:2e7e98cd0cb82db214b13224c71134b9335a719b
meta-st-stm32mp = default.xml:3d49b4b37ab3d5b80047e494b3fd459da00ff4ba
meta-qt5 = default.xml:b4d24d70aca75791902df5cd59a4f4a54aa4a125
meta-st-openstlinux = default.xml:9268cd36c765295f1abb8180f08d5502af2d1fd9
meta = default.xml:c7d2281eb6cda9c1637c20b3540b142073bca235
For ecosystem release v3.0.0 :
cat /etc/build
-----------------------
Build Configuration: |
-----------------------
BB_VERSION = 1.46.0
BUILD_SYS = x86_64-linux
NATIVELSBSTRING = universal
TARGET_SYS = arm-ostl-linux-gnueabi
MACHINE = stm32mp1
DISTRO = openstlinux-weston
DISTRO_VERSION = 3.1-openstlinux-5.10-dunfell-mp1-21-03-31
TUNE_FEATURES = arm vfp cortexa7 neon vfpv4 thumb callconvention-hard
TARGET_FPU = hard
MANIFESTVERSION = ostl-21-03-31-rc4-2-g7ef7d27
DISTRO_CODENAME = dunfell
ACCEPT_EULA_stm32mp1 = 1
GCCVERSION = 9.%
PREFERRED_PROVIDER_virtual/kernel = linux-stm32mp
PREFERRED_VERSION_linux-stm32mp =
-----------------------
Layer Revisions: |
-----------------------
meta-python = default.xml:5bba79488b7d393d2258d6e917f7bf7b0d7c4073
meta-oe = default.xml:5bba79488b7d393d2258d6e917f7bf7b0d7c4073
meta-gnome = default.xml:5bba79488b7d393d2258d6e917f7bf7b0d7c4073
meta-initramfs = default.xml:5bba79488b7d393d2258d6e917f7bf7b0d7c4073
meta-multimedia = default.xml:5bba79488b7d393d2258d6e917f7bf7b0d7c4073
meta-networking = default.xml:5bba79488b7d393d2258d6e917f7bf7b0d7c4073
meta-webserver = default.xml:5bba79488b7d393d2258d6e917f7bf7b0d7c4073
meta-filesystems = default.xml:5bba79488b7d393d2258d6e917f7bf7b0d7c4073
meta-perl = default.xml:5bba79488b7d393d2258d6e917f7bf7b0d7c4073
meta-st-stm32mp = default.xml:2e80e33539a193c6a8add6131c4c760009c49cea
meta-qt5 = default.xml:0d8eb956015acdea7e77cd6672d08dce18061510
meta-st-openstlinux = default.xml:673d7ee4572e3faadec3e43d5f0fa004465b78d9
meta = default.xml:72431ee8de5e3a53d259cebf420a7713ac9e1f14
3.2. Printing system information[edit source]
For ecosystem release v3.1.0 :
root@stm32mp1:~# uname -a Linux stm32mp1 5.10.61 #1 SMP PREEMPT Thu Aug 26 12:51:21 UTC 2021 armv7l armv7l armv7l GNU/Linux
For ecosystem release v3.0.0 :
uname -a Linux stm32mp1 5.10.10 #1 SMP PREEMPT Sat Jan 23 15:04:06 UTC 2021 armv7l armv7l armv7l GNU/Linux
3.3. Printing Linux kernel and GCC versions[edit source]
For ecosystem release v3.1.0 :
root@stm32mp1:~# cat /proc/version Linux version 5.10.61 (oe-user@oe-host) (arm-ostl-linux-gnueabi-gcc (GCC) 9.3.0, GNU ld (GNU Binutils) 2.34.0.20200220) #1 SMP PREEMPT Thu Aug 26 12:51:21 UTC 2021
For ecosystem release v3.0.0 :
cat /proc/version Linux version 5.10.10 (oe-user@oe-host) (arm-ostl-linux-gnueabi-gcc (GCC) 9.3.0, GNU ld (GNU Binutils) 2.34.0.20200220) #1 SMP PREEMPT Sat Jan 23 15:04:06 UTC 2021
3.4. Printing the amount of disk space available on all mounted file systems[edit source]
For ecosystem release v3.1.0 :
root@stm32mp1:~# df -h
Filesystem Size Used Avail Use% Mounted on
devtmpfs 146M 0 146M 0% /dev
/dev/mmcblk0p6 683M 471M 164M 75% /
tmpfs 212M 64K 212M 1% /dev/shm
tmpfs 212M 8.8M 203M 5% /run
tmpfs 212M 0 212M 0% /sys/fs/cgroup
tmpfs 212M 20K 212M 1% /tmp
/dev/mmcblk0p4 56M 15M 38M 28% /boot
/dev/mmcblk0p5 14M 6.8M 6.2M 53% /vendor
tmpfs 212M 156K 212M 1% /var/volatile
/dev/mmcblk0p7 14G 39M 13G 1% /usr/local
tmpfs 43M 0 43M 0% /run/user/0
For ecosystem release v3.0.0 :
df -h
Filesystem Size Used Avail Use% Mounted on
devtmpfs 147M 0 147M 0% /dev
/dev/mmcblk0p6 690M 424M 220M 66% /
tmpfs 214M 64K 214M 1% /dev/shm
tmpfs 214M 8.8M 205M 5% /run
tmpfs 214M 0 214M 0% /sys/fs/cgroup
tmpfs 214M 20K 214M 1% /tmp
/dev/mmcblk0p4 58M 14M 40M 27% /boot
/dev/mmcblk0p5 15M 6.8M 6.7M 51% /vendor
tmpfs 214M 144K 214M 1% /var/volatile
/dev/mmcblk0p7 28G 38M 26G 1% /usr/local
tmpfs 43M 0 43M 0% /run/user/0
3.5. ssh connection (only if the Ethernet cable connected)[edit source]
- Get the IP address of your board
ip addr show eth0 3: eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc mq state UP group default qlen 1000 link/ether xx:xx:xx:xx:xx:xx brd ff:ff:ff:ff:ff:ff inet xx.xx.xx.xx/xx brd xx.xx.xx.xx scope global dynamic eth0 valid_lft 159045sec preferred_lft 159045sec inet6 xxxx::xx:xx:xx:xx/64 scope link valid_lft forever preferred_lft forever
- On the host computer, connect the terminal to the board using ssh
ssh root@xx.xx.xx.xx
root@stm32mp1:~#