Revision

Revision as of 15:39, 21 February 2022 by Registered User (→‎Code)

1. Usage

The EcosystemRelease/Revision template returns the status for an ecosystem release revision in the flow associated with this wiki (e.g. v1.y.z ,or v2.y.z, or...), or the revision (x.y.z) of the latest ecosystem release.

Usage: {{EcosystemRelease/Revision | revision=<revision>}}

Where:

  • <revision> is the mandatory revision of the ecosystem release for which a status is requested. The possible values are:
    • latest to get the revision (x.y.z) of the latest ecosystem release.
    • 2.0.0 (June 2020 ecosystem release revision).
    • 2.1.0 (November 2020 ecosystem release revision).
    • 3.0.0 (March 2021 ecosystem release revision).
    • 3.1.0 (November 2021 ecosystem release revision).
    • 3.1.0.ALPHA (December 2021 ecosystem release revision for ALPHA customers).
    • 4.0.0 (June 2022 ecosystem release revision).
    • x.0.0, x.1.0, x.2.0 and 0.y.0 values are reserved to the examples and the helper files.

The returned value is:

  • x.y.z (revision of the latest ecosystem release), if <revision> is set to latest.
  • latest, if <revision> is the latest one, in the flow associated with this wiki.
  • legacy, if <revision> is a legacy one, in the flow associated with this wiki.
  • next, if <revision> is a planned one, in the flow associated with this wiki. eg during 3.1.0 preparation next is 3.1.0,
  • former, if <revision> is part of a former flow that is not the one associated with this wiki.
  • unknown, if <revision> is not supported.

E.g.

  • During 3.1.0 preparation : next is 3.1.0, legacy is 3.0.0, latest is 3.0.0, former 1.x.y, 2.x.y.
  • During 3.0.0 preparation : next : none, legacy :none, latest :3.0.0, former 1.x.y, 2.x.y.

2. Basic examples

You type You get
vx.0.0 revision (legacy)
{{EcosystemRelease/Revision | revision=x.0.0}}

legacy

Revision (x.y.z) of the latest ecosystem release
{{EcosystemRelease/Revision | revision=latest}}

4.0.0

Revision (x.y.z) of the 4.0.0 ecosystem release (latest)
{{EcosystemRelease/Revision | revision=4.0.0}}

latest

Revision (x.y.z) of the 3.1.0 ecosystem release (former)
{{EcosystemRelease/Revision | revision=3.1.0}}

former

Revision (x.y.z) of the 3.0.0 ecosystem release (former)
{{EcosystemRelease/Revision | revision=3.0.0}}

former

Revision (x.y.z) of the 2.1.0 ecosystem release (former)
{{EcosystemRelease/Revision | revision=2.1.0}}

former

Revision (x.y.z) of the 2.0.0 ecosystem release (former)
{{EcosystemRelease/Revision | revision=2.0.0}}

former

Revision (x.y.z) of the 1.0.0 ecosystem release (former)
{{EcosystemRelease/Revision | revision=1.0.0}}

former

3. More examples

You type You get
vx.2.0 revision (next)
{{EcosystemRelease/Revision | revision=x.2.0}}

next

vx.1.0 revision (latest)
{{EcosystemRelease/Revision | revision=x.1.0}}

latest

v0.y.0 revision (former)
{{EcosystemRelease/Revision | revision=0.y.0}}

former

Unknown revision
{{EcosystemRelease/Revision | revision=10.20.30}}

unknown

Unspecified revision
{{EcosystemRelease/Revision}}

unknown

4. Code

unknown