Unpack the STM32MP157x-DK2 board



1. Overview

This first step explains how to unpack the STM32MP157x-DK2 Discovery kit and the additional equipment you need.
The following block diagram provides high-level information on how to connect them together.

STM32MP1 connection block diagram

2. Out-of-the-box kit

STM32MP157x-DK2 side view
STM32MP157x-DK2 back view

3. Required equipment

The following table lists the equipment required to start playing with your STM32MP157x-DK2 board.
Some of them are delivered within the STM32MP157x-DK2 Discovery kit. The others need to be purchased separately.


4. Connection

  • Connect your laptop to the board ST-LINK/V2-1 port through the micro USB Type-B to USB Type-A cable.
  • Connect the USB Type-C™ to USB Type-C™ cable to the 5V/3A power supply.
  • Connect your laptop to the board USB Type-C™ OTG port through the USB Type-C™ to USB Type-A cable.
  • Optionally connect your Ethernet network to the board Ethernet port through the Ethernet cable.
STM32MP157x-DK2 Discovery kit connection
(The LCD display has been removed in the above view to better see the connectors)