This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Usage[edit source]
The ApplicableFor/CategoryAssignment template is used to format the applicability infobox that indicates for which microprocessor device(s) a page is applicable.
This template is called by the ApplicableFor template
Usage: {{ApplicableFor/CategoryAssignment | <MPU>}}
Where:
- <MPU> is the mandatory microprocessor device for which the page is applicable. The possible values for this parameter are the allowed values for the Has applicability specified for property. The page is automatically added to the transversal category associated to the microprocessor device (for example, Category:STM32MP15x).
The returned value is a link to the transversal category associated to the microprocessor device for which the page is applicable.
2. Basic examples[edit source]
You type | You get |
---|---|
A specific MPU
{{ApplicableFor/CategoryAssignment | STM32MP13x}}<br> {{ApplicableFor/CategoryAssignment | STM32MP15x}} |
3. More examples[edit source]
You type | You get |
---|---|
Unknown MPU
{{ApplicableFor/CategoryAssignment | STM32MP0x}} |
Unknown MPU |
Unspecified MPU
{{ApplicableFor/CategoryAssignment}}<br> {{ApplicableFor/CategoryAssignment | }}<br> {{ApplicableFor/CategoryAssignment | 1=}} |
Unknown MPU |
Check the spaces before and after the text
BEFORE{{ApplicableFor/CategoryAssignment| STM32MP13x}}AFTER<br> BEFORE{{ApplicableFor/CategoryAssignment | STM32MP1x}}AFTER |
BEFORE STM32MP13x linesAFTER |
4. Code[edit source]
Unknown MPU