This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Usage[edit source]
The EcosystemFlow/Warning template is used to insert a message about the current status of the article or chapter containing it.
Usage: {{EcosystemFlow/Warning| flow=<flow> }}
Where:
- <flow> is the identifier of the wiki. 2 values are possible:
- Current: the meaning of message associated to the Current flow (here v3) highlights the fact that the article or chapter has not been updated for the Current version (here v3). To be used when the article should have been updated for the Current version (here v3) but the update has not been done yet.
- Next : the meaning of message associated to the Next flow (here v4) highlights that the article has been updated for Next version (here v4) in Current version (here v3) . Consequently, this updated version must not be published yet.
Generally speaking, Current corresponds to current flow, and Next corresponds to the up coming flow.
The returned value is:
- a generic or custom message depending on the parameters
- "unknown flow", if <flow> is not supported.
2. Basic examples[edit source]
You type | You get | ||
---|---|---|---|
Generic message
{{EcosystemFlow/Warning}} |
unknown flow | ||
Message when flow is Current
{{EcosystemFlow/Warning | flow=Current}} |
| ||
Message when flow is Next
{{EcosystemFlow/Warning | flow=Next}} |
3. More examples[edit source]
You type | You get | ||
---|---|---|---|
Unknown flow
{{EcosystemFlow/Warning | flow=v0}} |
unknown flow | ||
Unspecified flow
{{EcosystemFlow/Warning}} |
unknown flow | ||
Check that there's no space before and after the text
BEFORE{{EcosystemFlow/Warning}}AFTER<br> BEFORE{{EcosystemFlow/Warning | flow=Current}}AFTER<br> BEFORE{{EcosystemFlow/Warning |flow=Next}}AFTER |
BEFOREunknown flow
BEFOREAFTER |
4. Code[edit source]
unknown flow