1. Overview[edit source]

This stage explains how to connect the Linux terminal of your board to your host computer through the ST-LINK/V2-1.
Then you will see how to execute basic commands with the Linux command line interface in order to be familiarized with the Linux console.

2. The serial terminal[edit source]

The serial terminal allows to communicate with the board trough a UART serial interface.

  • Install minicom
 sudo apt-get install minicom
  • Get the ttyACM device instance that need to be used to access the ST-LINK/V2-1
 ls /dev/ttyACM*
/dev/ttyACM0
  • Connect the minicom to the /dev/ttyACM0 device
 minicom -D /dev/ttyACM0
Welcome to minicom 2.7

OPTIONS: I18n 
Compiled on Nov 15 2018, 20:18:47.
Port /dev/ttyACM0, 15:56:03

Press CTRL-A Z for help on special keys
  • Press the reset button to reset the board. You should see boot log displayed in the minicom window

For ecosystem release v1.2.0 :

NOTICE:  CPU: STM32MP157CAC Rev.B
NOTICE:  Model: STMicroelectronics STM32MP157C-DK2 Discovery Board
NOTICE:  Board: MB1272 Var2 Rev.C-01
INFO:    Reset reason (0x14):
INFO:      Pad Reset from NRST
INFO:    PMIC version = 0x10
INFO:    Using SDMMC
INFO:      Instance 1
INFO:    Boot used partition fsbl1
NOTICE:  BL2: v2.0-r3.0(debug):                                                 
NOTICE:  BL2: Built : 13:13:37, Oct  2 2018                                     
INFO:    BL2: Doing platform setup                                              
INFO:    RAM: DDR3-1066/888 bin G 1x4Gb 533MHz v1.45                            
INFO:    Memory size = 0x20000000 (512 MB)                                      
INFO:    BL2 runs SP_MIN setup                                                  
INFO:    BL2: Loading image id 4                                                
INFO:    Loading image id=4 at address 0x2ffef000                               
INFO:    Image id=4 loaded: 0x2ffef000 - 0x30000000                             
INFO:    BL2: Loading image id 5                                                
INFO:    Loading image id=5 at address 0xc0100000                               
INFO:    STM32 Image size : 810245                                              
WARNING: Skip signature check (header option)                                   
INFO:    Image id=5 loaded: 0xc0100000 - 0xc01c5d05                             
NOTICE:  BL2: Booting BL32                                                      
INFO:    Entry point address = 0x2ffef000                                       
INFO:    SPSR = 0x1d3                                                           
NOTICE:  SP_MIN: v2.0-r3.0(debug):                                              
NOTICE:  SP_MIN: Built : 13:13:37, Oct  2 2018                                  
INFO:    ARM GICv2 driver initialized                                           
INFO:    stm32mp HSI (18): Secure only                                          
INFO:    stm32mp HSE (20): Secure only                                          
INFO:    stm32mp PLL2 (27): Secure only                                         
INFO:    stm32mp PLL2_R (30): Secure only                                       
INFO:    SP_MIN: Initializing runtime services                                  
INFO:    SP_MIN: Preparing exit to normal world                                 
                                                                               
                                                                               
U-Boot 2018.11-stm32mp-r4 (Nov 14 2018 - 16:10:06 +0000)                        
                                                                               
CPU: STM32MP157CAC Rev.B                                                        
Model: STMicroelectronics STM32MP157C-DK2 Discovery Board                       
Board: stm32mp1 in trusted mode (st,stm32mp157c-dk2)                            
Board: MB1272 Var2 Rev.C-01                                                     
DRAM:  512 MiB                                                                  
Clocks:                                                                         
- MPU : 650 MHz                                                                 
- MCU : 208.878 MHz                                                             
- AXI : 266.500 MHz                                                             
- PER : 24 MHz                                                                  
- DDR : 533 MHz                                                                 
NAND:  0 MiB                                                                    
MMC:   STM32 SDMMC2: 0, STM32 SDMMC2: 1                                         
Loading Environment from EXT4... OK                                             
In:    serial                                                                   
Out:   serial                                                                   
Err:   serial                                                                   
Net:   eth0: ethernet@5800a000                                                  
Hit any key to stop autoboot:  0                                                
Boot over mmc0!                                                                 
switch to partitions #0, OK                                                     
mmc0 is current device                                                          
Scanning mmc 0:4...                                                             
Found U-Boot script /boot.scr.uimg                                              
1628 bytes read in 1 ms (1.6 MiB/s)                                             
## Executing script at c4100000                                                 
Scanning mmc 0:4...                                                             
Found /mmc0_stm32mp157c-dk2_extlinux/extlinux.conf                              
Retrieving file: /mmc0_stm32mp157c-dk2_extlinux/extlinux.conf                   
614 bytes read in 0 ms                                                          
Retrieving file: /splash.bmp                                                    
46180 bytes read in 3 ms (14.7 MiB/s)                                           
Select the boot mode                                                            
1:      stm32mp157c-dk2-sdcard                                                  
2:      stm32mp157c-dk2-a7-examples-sdcard                                      
3:      stm32mp157c-dk2-m4-examples-sdcard                                      
Enter choice: 1:        stm32mp157c-dk2-sdcard                                  
Retrieving file: /uImage                                                        
6722112 bytes read in 305 ms (21 MiB/s)                                         
append: root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200                  
Retrieving file: /stm32mp157c-dk2.dtb                                           
73578 bytes read in 5 ms (14 MiB/s)                                             
## Booting kernel from Legacy Image at c2000000 ...                             
 Image Name:   Linux-4.19.94                                                  
   Created:      2020-01-09   9:19:10 UTC                                       
   Image Type:   ARM Linux Kernel Image (uncompressed)                          
   Data Size:    6722048 Bytes = 6.4 MiB                                        
   Load Address: c2000040                                                       
   Entry Point:  c2000040                                                       
   Verifying Checksum ... OK                                                    
## Flattened Device Tree blob at c4000000                                       
   Booting using the fdt blob at 0xc4000000                                     
   XIP Kernel Image ... OK                                                      
   Using Device Tree in place at c4000000, end c4014f69                         
                                                                               
Starting kernel ...                                                             
                                                                               
[    0.000000] Booting Linux on physical CPU 0x0                                
[    0.000000] Linux version 4.19.94 (oe-user@oe-host) (gcc version 8.2.0 (GCC)0
[    0.000000] CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c5387d  
[    0.000000] CPU: div instructions available: patching division code          
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instructie
[    0.000000] OF: fdt: Machine model: STMicroelectronics STM32MP157C-DK2 Discod
[    0.000000] Memory policy: Data cache writealloc                             
[    0.000000] efi: Getting EFI parameters from FDT:                            
[    0.000000] efi: UEFI not found.                                             
[    0.000000] Reserved memory: created DMA memory pool at 0x10000000, size 0 MB
[...]
[    3.764425] systemd[1]: Detected architecture arm.                           
                                                                               
Welcome to ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 2.6-openstl!
                                                                               
                                                                                              
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 2.6-openstlinux-20-02-19
                                                                               
stm32mp1 login: root (automatic login)                                          
                                                                               
root@stm32mp1:~#                                             


For ecosystem release v1.1.0 :

For ecosystem release v1.0.0 :

3. Basic commands[edit source]

3.1. Printing distribution specific information[edit source]

For ecosystem release v1.2.0 :

 lsb_release -a
LSB Version:    core-5.0-noarch:core-5.0-arm
Distributor ID: openstlinux-weston
Description:    ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 2.6-openstlinux-20-02-19
Release:        2.6-openstlinux-20-02-19                                        
Codename:       thud  

For ecosystem release v1.1.0 :

For ecosystem release v1.0.0 :

3.2. Printing system information[edit source]

For ecosystem release v1.2.0 :

 uname -a
Linux stm32mp1 4.19.94 #1 SMP PREEMPT Thu Jan 9 09:19:10 UTC 2020 armv7l armv7l armv7l GNU/Linux

For ecosystem release v1.1.0 :

For ecosystem release v1.0.0 :

3.3. Printing Linux kernel and GCC versions[edit source]

For ecosystem release v1.2.0 :

 cat /proc/version
Linux version 4.19.94 (oe-user@oe-host) (gcc version 8.2.0 (GCC)) #1 SMP PREEMPT Thu Jan 9 09:19:10 UTC 2020     

For ecosystem release v1.1.0 :

For ecosystem release v1.0.0 :

3.4. Printing the amount of disk space available on all mounted file systems[edit source]

 df -h
Filesystem      Size  Used Avail Use% Mounted on
/dev/root       715M  348M  328M  52% /
devtmpfs        150M     0  150M   0% /dev
tmpfs           214M     0  214M   0% /dev/shm
tmpfs           214M   12M  203M   6% /run
tmpfs           214M     0  214M   0% /sys/fs/cgroup
tmpfs           214M  4.0K  214M   1% /tmp
tmpfs           214M   76K  214M   1% /var/volatile
/dev/mmcblk0p4   58M  8.4M   46M  16% /boot
/dev/mmcblk0p7   14G   67M   13G   1% /usr/local
/dev/mmcblk0p5   15M  8.4M  5.1M  63% /vendor

3.5. ssh connection (only if Ethernet cable is connected)[edit source]

  • Get the IP address of your board
 ip addr show eth0                                                                           
3: eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc mq state UP group default qlen 1000
    link/ether xx:xx:xx:xx:xx:xx brd ff:ff:ff:ff:ff:ff
    inet xx.xx.xx.xx/xx brd xx.xx.xx.xx scope global dynamic eth0
       valid_lft 159045sec preferred_lft 159045sec
    inet6 xxxx::xx:xx:xx:xx/64 scope link 
       valid_lft forever preferred_lft forever
  • On the host computer connect the terminal to the board using ssh
 ssh root@xx.xx.xx.xx
root@stm32mp1:~#