This article aims to give the following information:
- How to download and install the latest SDK for the STM32 microprocessor Series
- Where to find the associated release note
- Where to find the previous releases (archives)
1. STM32MP15-Ecosystem-v1.2.0 release[edit source]
- The STM32MP1 SDK is delivered through a tarball file named : en.SDK-x86_64-stm32mp1-openstlinux-4.19-thud-mp1-20-02-19.tar.xz
- Download and install the STM32MP1 SDK.
- The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here
STM32MP1 Developer Package SDK - STM32MP15-Ecosystem-v1.2.0 release | |
---|---|
Download |
You need to be logged on my.st.com before accessing the following link: |
Installation |
$ tar xvf en.SDK-x86_64-stm32mp1-openstlinux-4.19-thud-mp1-20-02-19.tar.xz
$ chmod +x stm32mp1-openstlinux-4.19-thud-mp1-20-02-19/sdk/st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-2.6-openstlinux-4.19-thud-mp1-20-02-19.sh
$ ./stm32mp1-openstlinux-4.19-thud-mp1-20-02-19/sdk/st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-2.6-openstlinux-4.19-thud-mp1-20-02-19.sh -d <working directory absolute path>/Developer-Package/SDK
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version 2.6-openstlinux-4.19-thud-mp1-20-02-19 ====================================================================================================================== You are about to install the SDK to "<working directory absolute path>/Developer-Package/SDK". Proceed[Y/n]? Y Extracting SDK.......................................................................................................done Setting it up...done SDK has been successfully set up and is ready to be used. Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g. $ . /<working directory absolute path>/Developer-Package/SDK/environment-setup-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi |
Release note |
Details about the content of the SDK are available in the associated STM32MP15 ecosystem release note. If you are interested in older releases, please have a look into the section Archives. |
- The SDK is in the <SDK installation directory>:
<SDK installation directory> SDK for OpenSTLinux distribution: details in Standard SDK directory structure article ├── environment-setup-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi Environment setup script for Developer Package ├── site-config-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi ├── sysroots │ ├── cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi Target sysroot (libraries, headers, and symbols) │ │ └── [...] │ └── x86_64-openstlinux_weston_sdk-linux Native sysroot (libraries, headers, and symbols) │ └── [...] └── version-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi
2. Archives [edit source]
2.1. STM32MP15-Ecosystem-v1.1.0 release[edit source]
- The STM32MP1 SDK is delivered through a tarball file named : en.SDK-x86_64-stm32mp1-openstlinux-4.19-thud-mp1-19-10-09.tar.xz
- Download and install the STM32MP1 SDK.
- By downloading this software package, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here
STM32MP1 Developer Package SDK - STM32MP15-Ecosystem-v1.1.0 release | |
---|---|
Download |
You need to be logged on my.st.com before accessing the following link: |
Installation |
$ tar xvf en.SDK-x86_64-stm32mp1-openstlinux-4.19-thud-mp1-19-10-09.tar.xz
$ chmod +x stm32mp1-openstlinux-4.19-thud-mp1-19-10-09/sdk/st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-2.6-openstlinux-4.19-thud-mp1-19-10-09.sh
$ ./stm32mp1-openstlinux-4.19-thud-mp1-19-10-09/sdk/st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-2.6-openstlinux-4.19-thud-mp1-19-10-09.sh -d <working directory absolute path>/Developer-Package/SDK
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version 2.6-openstlinux-4.19-thud-mp1-19-10-09 ====================================================================================================================== You are about to install the SDK to "<working directory absolute path>/Developer-Package/SDK". Proceed[Y/n]? Y Extracting SDK.......................................................................................................done Setting it up...done SDK has been successfully set up and is ready to be used. Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g. $ . /<working directory absolute path>/Developer-Package/SDK/environment-setup-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi |
Release note |
Details about the content of the SDK are available in the associated STM32MP15 ecosystem release note. If you are interested in older releases, please have a look into the section Archives. |
- The SDK is in the <SDK installation directory>:
<SDK installation directory> SDK for OpenSTLinux distribution: details in Standard SDK directory structure article ├── environment-setup-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi Environment setup script for Developer Package ├── site-config-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi ├── sysroots │ ├── cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi Target sysroot (libraries, headers, and symbols) │ │ └── [...] │ └── x86_64-openstlinux_weston_sdk-linux Native sysroot (libraries, headers, and symbols) │ └── [...] └── version-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi
2.2. STM32MP15-Ecosystem-v1.0.0 release[edit source]
- The STM32MP1 SDK is delivered through a tarball file named : en.SDK-x86_64-stm32mp1-openstlinux-4.19-thud-mp1-19-02-20.tar.xz
- Download and install the STM32MP1 SDK.
- By downloading this software package, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here
STM32MP1 Developer Package SDK - STM32MP15-Ecosystem-v1.0.0 release | |
---|---|
Download |
You need to be logged on my.st.com before accessing the following link: |
Installation |
$ tar xvf en.SDK-x86_64-stm32mp1-openstlinux-4.19-thud-mp1-19-02-20.tar.xz
$ chmod +x stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/sdk/st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-2.6-openstlinux-4.19-thud-mp1-19-02-20.sh
$ ./stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/sdk/st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-2.6-openstlinux-4.19-thud-mp1-19-02-20.sh -d <working directory absolute path>/Developer-Package/SDK
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version 2.4-openstlinux-4.19-thud-mp1-19-02-20 ====================================================================================================================== You are about to install the SDK to "<working directory absolute path>/Developer-Package/SDK". Proceed[Y/n]? Y Extracting SDK.......................................................................................................done Setting it up...done SDK has been successfully set up and is ready to be used. Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g. $ . /<working directory absolute path>/Developer-Package/SDK/environment-setup-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi |
Release note |
Details about the content of the SDK are available in the associated STM32MP15 ecosystem release note. |
- The SDK is in the <SDK installation directory>:
<SDK installation directory> SDK for OpenSTLinux distribution: details in Standard SDK directory structure article ├── environment-setup-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi Environment setup script for Developer Package ├── site-config-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi ├── sysroots │ ├── cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi Target sysroot (libraries, headers, and symbols) │ │ └── [...] │ └── x86_64-openstlinux_weston_sdk-linux Native sysroot (libraries, headers, and symbols) │ └── [...] └── version-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi