1. Usage
The MicroprocessorDevice template is used to indicate for which microprocessor device(s), an article part (chapter, paragraph, table...) is valid. Per default (i.e. if this template is not used), any part of an article is valid for all microprocessor devices for which the entire article is valid.
It outputs a "standardized" string that might be used to name an article part.
Usage: {{MicroprocessorDevice | device=<device> | security=<security>}}
- Where:
- <device> is the mandatory identifier (one to three digits) that specify the Series, the lines or the line.The possible values are:
- 1: STM32MP1 Series
- 15: STM32MP15x lines
- 151: STM32MP151 access line
- 153: STM32MP153 foundation line
- 157: STM32MP157 advanced line
- 15: STM32MP15x lines
- 1: STM32MP1 Series
- <security> is the optional identifier (one letter) that specifies the security. The possible values are:
- A: Basic
- C: Secure boot and cryptography
Clicking on the File:Info.png icon displays the article about the microprocessor device lines (e.g. STM32MP15 microprocessor).
2. Basic examples
You type | You get |
---|---|
STM32MP1 Series
{{MicroprocessorDevice | device=1}} |
STM32MP1 Series |
STM32MP15x lines
{{MicroprocessorDevice | device=15}} |
STM32MP15x linesFile:Info.png |
STM32MP157 line
{{MicroprocessorDevice | device=157}} |
STM32MP157 lineFile:Info.png |
STM32MP15x lines with basic security
{{MicroprocessorDevice | device=15 | security=A}} |
STM32MP15xA linesFile:Info.png |
STM32MP157 line with secure boot and cryptography
{{MicroprocessorDevice | device=157 | security=C}} |
STM32MP157C lineFile:Info.png |
3. More examples
You type | You get |
---|---|
Unspecified microprocessor device
{{MicroprocessorDevice}} |
STM32MP unknown microprocessor device |
Unknown Series
{{MicroprocessorDevice | device=0}} |
STM32MP0 unknown microprocessor device |
Unknown lines
{{MicroprocessorDevice | device=11}} |
STM32MP11 unknown microprocessor device |
Unknown line
{{MicroprocessorDevice | device=154}} |
STM32MP154 unknown microprocessor device |
Unknown line
{{MicroprocessorDevice | device=1531}} |
STM32MP1531 unknown microprocessor device |
Unknown security
{{MicroprocessorDevice | device=15 | security=Z}} |
unknown security STM32MP15xZ linesFile:Info.png |
Unknown line and security
{{MicroprocessorDevice | device=152 | security=Z}} |
unknown security STM32MP152 unknown microprocessor device |
4. Code
STM32MP unknown microprocessor device