This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.
1. Overview[edit source]
This first step explains how to unpack the STM32MP135x-DK Discovery kit and the additional equipment you need.
The following block diagram provides high-level information on how to connect them together.
![](/stm32mpu-ecosystem-v4/nsfr_img_auth.php/e/e1/STM32MP1_connection_block_diagram.png)
STM32MP1 connection block diagram
2. Out-of-the-box kit[edit source]
File:STM32MP135F-DK angle2.jpg
STM32MP135x-DK back view
File:STM32MP135F-DK verso.jpg
STM32MP135x-DK front view
3. Required equipment[edit source]
The following table lists the equipment required to start playing with your STM32MP135x-DK board.
Some of them are delivered within the STM32MP135x-DK Discovery kit. The others need to be purchased separately.
STM32MP135x-DK Discovery kit | Flexible development platform for STM32MP13 microprocessor devices | Delivered |
MicroSD card | To be populated with the OpenSTLinux Distribution (Linux software), and providing extra storage capacity. A 2-Gbyte minimum microSD card is required. |
Delivered |
USB Type-C™ to USB Type-C™ cable | Used to connect the STM32MP135x-DK Discovery kit to the power supply | Delivered |
Micro USB Type-B to USB Type-A cable | Used to connect the STM32MP135x-DK Discovery kit to the PC through the USB micro-B (ST-LINK/V3E) |
Not delivered |
USB Type-C™ to USB Type-A cable | Used to connect the STM32MP135x-DK Discovery kit to a USB OTG device. | Not delivered |
5V/3A power supply | The power supply should be able to output 5V / 3A (15W) | Not delivered |
Laptop | A Linux PC running Ubuntu 16.04 is required. | Not delivered |
Ethernet cable (optional) | Used to connect the STM32MP135x-DK Discovery kit through ssh | Not delivered |
4. Connection[edit source]
- Connect your laptop to the board ST-LINK/V3E port through the micro USB Type-B to USB Type-A cable.
- Connect the USB Type-C™ to USB Type-C™ cable to the 5V/3A power supply.
- Connect your laptop to the board USB Type-C™ OTG port through the USB Type-C™ to USB Type-A cable.
- Optionally connect your Ethernet network to the board Ethernet port through the Ethernet cable.