Revision as of 11:32, 24 March 2021 by Registered User (Nathalie Sangouard moved page STM32CubeIDE user space project to How to debug a user space application with STM32CubeIDE/User space project without leaving a redirect)
Renaming.png This page is a candidate for renaming (move).
The requested new name is: How to debug a user space application with STM32CubeIDE/User space project in STM32CubeIDE.
The supplied reason is: visibility.
-- Registered User (-) 14:52, 22 March 2021 (CET).
Wiki maintainers: remember to update the pages that link this page before renaming (moving) it.

1. Create a user space executable project[edit source]

In context of Cortex-A7 sub-project, MP157C-DK2_CA7 here, right click and select Create a userspace Project..

User space project wizard shortcut

We select here Executable project type, in C language. Note that our user space project will use by default the SDK version associated to Cortex-A7 sub-project.

User space project creation wizard

2. Build[edit source]

  • Select your project, right-click and then Build Project.
Executable Build


3. Preparing Debug Configuration[edit source]

Your target must be Linux booted and network connected. Please, start Target Status widget on the bottom right and check for the green light.

Target Status - green


Please also check How to set up proxy and P2P Ethernet connection with STM32CubeIDE if you are in that case.

4. Debug Configuration[edit source]

Select your project, right-click Debug as... > Debug Configurations, then select STM32 Cortex-A Remote Application'.

Debug configuration shortcut


The default Connection proposed is "MPU SSH", corresponding to the target IP address discovered by Target Status. The default destination directory is /home/root.

User space debug configuration - main tab

5. Debug[edit source]

Click Debug :

  1. Executable is downloaded to the target,
  2. GDBServer is launched on the target,
  3. GDBClient is launched on the workstation and can exchange via network with GDBServer,
User space debug
Info white.png Information
in case of error; please stop any GDBServer running on the target before launching a new debug session.