STM32MPU distribution for Android

Revision as of 14:18, 5 September 2019 by Registered User

The STM32MPU distribution for Android™ runs on Arm® Cortex®-A processors. It is a subset of the STM32MPU Embedded Software distribution for Android.

It includes the following collection of software components:

  • OpenSTLinux BSP that offers services for the application frameworks in the same context:
    • boot chain based on TF-A and U-Boot.
    • OP-TEE secure OS running on the Cortex-A core in Secure mode
    • Linux® kernel running on the Arm® Cortex®-A core in Non-secure mode
  • Application frameworks that rely on the services provided by the OpenSTLinux BSP, to provide specific functionalities (code libraries, APIs, tool sets...) to ease the development of software applications:
    • OP-TEE application frameworks running in the secure OS user space (e.g. TEE Internal core API for the development of Trusted Applications (TA))
    • Android application frameworks running in Linux OS user space (see AOSP[1] for more details)

The OpenSTLinux BSP for Android has some specificities:

  • The Linux kernel source is based on the Common Kernel available in AOSP[2]
  • The Linux kernel configuration is based on the reference configuration available in AOSP[3]

Android application frameworks are based on the AOSP platform manifest[4]. By default, one of the Google tags[5] is used as a reference.

The Google services (ex: Cast, Drive, Maps...) are neither embedded nor validated within this STM32MPU distribution for Android™.

1. How to get the software for this distribution?[edit source]

The STM32MPU distribution for Android™ is available through the three Packages (Starter, Developer, and Distribution) of the STM32MPU Embedded Software distribution for Android.

2. References[edit source]