This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Template:ArticleMainWriter Template:ArticleProposedVersion
Develop on Arm® Cortex®-M4 | What's next | |||||
Install the IDE | Install STM32Cube MP1 package | Modify, rebuild and reload a firmware |
1. Overview[edit source]
This stage will explain you how to modify, rebuild and reload a STM32MP1 Arm® Cortex®-M4 coprocessor firmware.
2. Import an existing example in SW4STM32 IDE[edit source]
- Open System Workbench for STM32 IDE
- Open the import screen File > Import... and select Existing Project into Workspace
- Browse and select OpenAMP_TTY_echo application example
$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package/STM32Cube_FW_MP1_V1.0.0/Projects/STM32MP157C-DK2/Applications/OpenAMP/OpenAMP_TTY_echo - Click finish
- The OpenAMP_TTY_echo project is open and you can browse inside using the left pan
3. Build the example[edit source]
- Click the build button (the little hammer in the toolbar)
- If the following screen appear, click OK
- Build is finished with no error
4. Execute the example[edit source]
5. Modify the example[edit source]
6. Rebuild and reload the example[edit source]