1. Article purpose[edit source]
The article aims to help to rebase an STM32 MPU project on a new ecosystem release by focusing on main changes impacts.
2. Scope of this article[edit source]
This article provides some details for main changes between STM32 MPU ecosystem release v3.1.0 and new STM32
MPU ecosystem release v4.0.0 to help for migrating your project.
All Informations about the features delivered in the new release is also available in the OpenSTLinux release note.
3. Impacted domains[edit source]
3.1. Yocto build environment for Distribution Package[edit source]
These are Yocto layers/recipes to update for the new Kirkstone version. Follow scripts available in the OpenEmbedded-Core layer to help the user:
- ./layers/openembedded-core/scripts/contrib/convert-overrides.py
- ./layers/openembedded-core/scripts/contrib/convert-spdx-licenses.py
- ./layers/openembedded-core/scripts/contrib/convert-srcuri.py
- ./layers/openembedded-core/scripts/contrib/convert-variable-renames.py
- (See Yocto Kirkstone release note[1] for more information.)
3.2. Hardware configuration[edit source]
Check the device tree files for the STMP32 MPU board: Linux Kernel: between Linux kernel v5.15-stm32mp-r1 (v5.15.24) and previous Linux kernel v5.10-stm32mp-r2 (v5.10.61)
U-Boot: between U-Boot v2021.10-stm32mp-r1 and previous U-Boot v2020.10-stm32mp-r2
OP-TEE: between OP-TEE 3.16.0-stm32mp-r1 and previous OP-TEE 3.12.0-stm32mp-r2
- New STM32MP135x-DK Discovery kit
- Update the device tree to use a bus controller configuration in order to manage secure/nonsecure IP.
- Remove the secure-status.
- Remove the unused nodes in OP-TEE.
- Define the GPIO secure configuration in the device tree.
- I2C compatible update for STM32MP15 lines to manage nonsecure PMIC in OP-TEE (st,stm32mp15-i2c-non-secure)
- Remove the nvmem_layout bindings.
- Reduce the device tree and only keep the securable peripheral nodes.
- New STM32MP135x-DK Discovery kit
TF-A: between TF-A v2.6-stm32mp-r1 and previous TF-A v2.4-stm32mp-r2
3.3. System configuration[edit source]
- FIP only on STM32 MPU ecosystem release v4.0.0
. NoFIP is no more supported
- FOTA (memory mapping if activated and GPT UUID partition fixed). If no FOTA activated, no change at driver level. Impact on flashlayout.
- Memory mapping update linked to OP-TEE
3.4. Boot stages[edit source]
BL2
- BL2 more hardcoded configuration values such as early console default parameters
- Remove STM32 image management (parsing and authentication)
- Introduce PSA_FWU support: Fix specific UUID for GPT partitions when used
- Update the NAND core driver to allow external memory usage for temporary buffer
SP-MIN boot chain deprecated replaced by OP-TEE.
3.5. Security[edit source]
- Rework firewall control management: use bus controller to add device tree node to probe list
- TZC400 configuration managed in OP-TEE
- Calibration binding updated: Use a dedicated binding for the calibration, out from RCC node
- Remove proprietary SMC access replaced by SCMI access or dedicated PTA.
- Move RNG to secure RNG by default
- Remove SCMI channel 1 (unused) and rename SCMI0 to SCMI
- New BSEC PTA for OTP management
- New Introduce Trusted UI framework
- New SCMI performance for STM32MP13 lines
- New Use clock framework to manage clocks
3.6. User space and applications[edit source]
New "weston" user now required for "wayland", which avoids executing some application with root profile for security reasons
- su -l weston -c "<command>" could be used to specify the user profile
which mainly impacts Graphic and Audio frameworks usage.
4. References[edit source]