This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This article proposes to manage a Linux® user space application for STM32 MPU, using the standard Eclipse® CDT™ wizard.
1. Create a "user space" project[edit source]
- Open the new C project wizard: File -> New -> Project... C Project.
![New C project wizard New C project wizard](/stm32mpu-ecosystem-v4/nsfr_img_auth.php/5/55/CDTExeCreation.png)
- In the first window, choose OpenSTLinux SDK
![New C project wizard New C project wizard](/stm32mpu-ecosystem-v4/nsfr_img_auth.php/2/27/CDTExeCreationCProject.png)
- Then Next to set up configuration
![New C project wizard New C project wizard](/stm32mpu-ecosystem-v4/nsfr_img_auth.php/e/e8/CDTExeCreationCProjectNext.png)
- and Next to choose the SDK version
![New C project wizard New C project wizard](/stm32mpu-ecosystem-v4/nsfr_img_auth.php/7/72/CDTExeCreationCProjectNextNext.png)
- To populate this project with file "main.c", first select project, then right-click New -> File -> main.c, and then fill it with some C code.
2. Build[edit source]
- Select your project, right-click and then Build Project.
![C project build C project build](/stm32mpu-ecosystem-v4/nsfr_img_auth.php/3/34/CDTExeBuild.png)
3. Prepare Debug Configuration[edit source]
You can check boot messages via Linux® console opened with butterfly icon (shown below), but remember this console cannot be shared outside STM32CubeIDE (minicom,...).
![CubeIDELinuxConsole.png](/stm32mpu-ecosystem-v4/nsfr_img_auth.php/0/0b/CubeIDELinuxConsole.png)
In order to debug user space application, your target must be Linux® booted and network connected.
To check network connection, start the Target Status widget in the bottom right corner of the window.
![Target Status - green Target Status - green](/stm32mpu-ecosystem-v4/nsfr_img_auth.php/2/2b/CubeIDE-UserSpace-Debug1.png)
Check How to set up proxy and P2P Ethernet connection with STM32CubeIDE if you have some proxy problem.
4. Set Debug Configuration[edit source]
- Select your project, right-click Debug as... > Debug Configurations.
- Then create an STM32 Cortex-A Remote Application debug configuration, and double-click on it.
![C Project debug C Project debug](/stm32mpu-ecosystem-v4/nsfr_img_auth.php/4/4d/CDTExeDebugCfg.png)
5. Debug[edit source]
Click on Debug:
- Executable is downloaded to the target,
- GDBServer is launched on the target,
- GDBClient is launched on the workstation and can exchange via network with GDBServer.
![C project debug C project debug](/stm32mpu-ecosystem-v4/nsfr_img_auth.php/3/34/CDTExeDebug.png)