This article proposes to manage a shared library, dynamically linked with a Linux® user space application on STM32 MPU.
[edit source]
In the Cortex®-A7 sub-project context, named here MP157C-DK2_CA7, right-click and select Create a userspace Project...
![User space project wizard shortcut User space project wizard shortcut](/stm32mpu-ecosystem-v4/nsfr_img_auth.php/8/8d/UserSpaceShortCut.png)
A Shared Library project type, in C language, is selected.
Note that the user space project uses by default the SDK version associated to the Cortex®-A7 sub-project.
![User space shared library creation User space shared library creation](/stm32mpu-ecosystem-v4/nsfr_img_auth.php/5/51/CubeIDEUserSpaceSharedLibCreation.png)
2. Build[edit source]
- Select your project, right-click and then Build Project.
![Shared library build Shared library build](/stm32mpu-ecosystem-v4/nsfr_img_auth.php/2/2e/CubeIDEUserSpaceSharedLibBuild.png)
[edit source]
Hereafter is an updated code for main() to call mySharedLib function say_hello().
You must also reference mySharedLib project inside myExe properties: C/C++ General > Paths and Symbols > References, as depicted below.
![Executable source & properties update Executable source & properties update](/stm32mpu-ecosystem-v4/nsfr_img_auth.php/1/12/CubeIDEUserSpaceSharedLibExeBuild.png)
4. Prepare Debug Configuration[edit source]
You can check boot messages via Linux® console opened with butterfly icon, but remember this console cannot be shared outside STM32CubeIDE (minicom,...).
In order to debug user space application, your target must be Linux® booted and network connected.
In order to check network connection, start the Target Status widget in the bottom right corner of the window.
![Target Status - green Target Status - green](/stm32mpu-ecosystem-v4/nsfr_img_auth.php/2/2b/CubeIDE-UserSpace-Debug1.png)
Check How to set up proxy and P2P Ethernet connection with STM32CubeIDE if you are in that case.
5. Linux® deployment configuration[edit source]
To run or debug the executable myExe and its shared library mySharedLib, it is required to download the shared library object (.so) to the STM32MP15x lines .
Select the shared library project, right-click Run as... > Run Configurations, then select STM32 Cortex-A Linux Deployment'.
![Run configuration shortcut Run configuration shortcut](/stm32mpu-ecosystem-v4/nsfr_img_auth.php/e/ef/CubeIDEUserSpaceSharedLibRun.png)
![Linux deployment configuration Linux deployment configuration](/stm32mpu-ecosystem-v4/nsfr_img_auth.php/a/a8/CubeIDEUserSpaceSharedLibRunSetup.png)
6. Debug Configuration[edit source]
Select your project, right-click Debug as... > Debug Configurations, then select STM32 Cortex-A Remote Application'.
The default connection proposed is "MPU SSH", corresponding to the target IP address discovered by the Target Status widget. The default destination directory is /home/root.
For the executable myExe to load the mySharedLib dynamic library, a setup of LD_LIBRARY_PATH with the path to mySharedLib is needed before starting debug.
![Debug configuration setup Debug configuration setup](/stm32mpu-ecosystem-v4/nsfr_img_auth.php/5/5d/CubeIDEUserSpaceSharedLibExeDebugSetup.png)
[edit source]
Click Debug :
- Executable is downloaded to the target,
- GDBServer is launched on the target,
- GDBClient is launched on the workstation and can exchange via the network with GDBServer.
![User space shared library debug User space shared library debug](/stm32mpu-ecosystem-v4/nsfr_img_auth.php/f/f8/CubeIDEUserSpaceSharedLibExeDebug.png)