1. Overview[edit source]
This step explains how to get the Starter Package, then install and boot the STM32MP15 Discovery kit with the Starter Package.
2. Open a terminal[edit source]
Open a terminal on the host computer.
All the commands preceded by have to be executed from the host computer terminal.
- Create your STM32MPU workspace directory on the host computer:
mkdir $HOME/STM32MPU_workspace cd $HOME/STM32MPU_workspace
3. Check the host computer Internet access[edit source]
- An Internet access through http and https protocols must be provided.
The command below enables checking for Internet access through http/https protocols:
wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy."
If an 'OK' message is returned, the network is correctly configured.
In this case, skip the rest of this section.
Otherwise, a proxy for http/https protocols is required.
The best solution is to set this proxy through the shell variables http_proxy and https_proxy:
export http_proxy=http://<MyProxyLogin>:<MyProxyPassword>@<MyProxyServerUrl>:<MyProxyPort> export https_proxy=http://<MyProxyLogin>:<MyProxyPassword>@<MyProxyServerUrl>:<MyProxyPort>
Check again the Internet access using the command:
wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy."
4. Install the tools[edit source]
4.1. STM32CubeProgrammer[edit source]
- Create your STM32MPU tools directory on the host computer:
mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z
- Create a temporary directory in your STM32MPU workspace:
mkdir $HOME/STM32MPU_workspace/tmp
- Download STM32CubeProgrammer in the following directory : $HOME/STM32MPU_workspace/tmp
STM32CubeProgrammer v2.12.0 is recommended for ecosystem release v4.1.0 .
- Uncompress the archive file to get the STM32CubeProgrammer installers:
cd $HOME/STM32MPU_workspace/tmp unzip SetupSTM32CubeProgrammer.zip
- Execute the Linux® installer, which guides you through the installation process. Select "$HOME/STM32MPU-Tools/STM32CubeProgrammer-x.y.z" as installation directory when it is requested by the installer.
./SetupSTM32CubeProgrammer-x.y.z.linux
The screenshots below have been obtained with old STM32CubeProgrammer V2.7.0. They are provided as examples and are still valid for higher versions :
- Add the STM32CubeProgrammer binary path to your PATH environment variable:
export PATH=$HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z/bin:$PATH
- Check that the STM32CubeProgrammer tool is properly installed and accessible:
STM32_Programmer_CLI --h ------------------------------------------------------------------- STM32CubeProgrammer vx.y.z -------------------------------------------------------------------
4.2. USB serial link[edit source]
- Install the libusb on your host computer:
sudo apt-get install libusb-1.0-0
- To allow STM32CubeProgrammer to access the USB port through low-level commands, proceed as follows:
cd $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z/Drivers/rules sudo cp *.* /etc/udev/rules.d/
5. Download the image[edit source]
- Create your STM32MP1 Starter Package directory on the host computer:
mkdir $HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0 mkdir $HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Starter-Package cd $HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Starter-Package
- Download the STM32MP1-Ecosystem-v4.1.0 Starter Package into the following directory:
$HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Starter-Package - Uncompress the tarball file to get the binaries for the different partitions of the image, and the Flash layout files
tar xvf en.FLASH-stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23.tar.gz
6. Populate the SDCard[edit source]
- Set the boot switches (located at the back of the board) to the OFF position.
- Connect the PC to the CN7/USB_OTG port of the STM32MP157x-DK2 board through the USB Type A to Type C cable.
- Power on the board.
- Press the reset button to reset the board.
- Launch STM32CubeProgrammer to get the GUI:
- On the right of the window, select USB (instead of STLINK, set by default) in the connection picklist and click the "Refresh" button. The serial number is displayed if the USB is detected. Then click "Connect".
- Select the "Open File" tab and choose the "FlashLayout_sdcard_stm32mp157x-dk2-trusted.tsv" file in the Starter Package installation folder ("$HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v4.0.0/Starter-Package/stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23/images/stm32mp1/flashlayout_st-image-weston/trusted")
- Fill the "Binaries Path" by browsing to the $[Starter_Pack_Path]/images/stm32mp1 folder.
- Click "Download" to start the flashing process.
- A progress bar indicates the process progress until a completion pop-up message is displayed.
7. Boot the board[edit source]
- Set the boot switches (located at the back of the board) to the ON position:
- Power on the board.
- Press the "Reset "button to reset the board.
- After few seconds, the board starts and automatically goes through the following screens
- If the board power supply does not supply enough current (3A), the red LED indicates the issue following the rules below:
LED blinking mode Console message Boot process Twice WARNING 500mA power supply detected Current too low, use a 3A power supply!
Continue and red LED stays ON 3 times WARNING 1500mA power supply detected Current too low, use a 3A power supply!
Continue and red LED stays ON forever ERROR USB TYPE-C connection in unattached mode Check that USB TYPE-C cable is correctly plugged
stop forever USB TYPE-C charger not compliant with USB specification stop