1. Usage[edit source]
The DocSource template is used to indicate the URL of any Linux® kernel, Yocto Project, and AWS IoT Greengrass document used in this wiki.
Usage: {{DocSource | domain=<domain> | path=<path> | text=<link text> | version=<version>}}
- Where:
- <domain> is the mandatory string that identifies the domain of the document. The possible values are:
- Linux kernel: the document belongs to the Linux kernel domain.
- Yocto Project: the document belongs to the Yocto Project domain.
- AWS Greengrass: the document belongs to the AWS IoT Greengrass domain.
- U-Boot: the document belongs to U-Boot domain
- TF-A: the document belongs to TF-A domain.
- OP-TEE_OS: the document belongs to OP-TEE OS domain.
- <path> is the mandatory relative path of the document from the root URL of the domain. The root URLs are:
- https://www.kernel.org/doc/html/ for the Linux kernel domain
- https://docs.yoctoproject.org/ for the Yocto Project domain
- https://docs.aws.amazon.com/greengrass/ for the AWS IoT Greengrass domain
- https://u-boot.readthedocs.io for the U-Boot domain
- https://trustedfirmware-a.readthedocs.io for the TF-A domain
- https://optee.readthedocs.io for the OP-TEE OS domain
- <link text> is an optional link text (text that is displayed instead of the URL).
- <version> is an optional version number (branch or tag) if the default one doesn't fit. Per default, the URL points to:
- the v5.15 branch of the Linux kernel
- the 4.0 branch of the Yocto Project TBC
- the latest branch of the AWS IoT Greengrass
- the v2021.07 branch of the U-Boot documentation
2. Basic examples[edit source]
You type | You get |
---|---|
Linux kernel
1- {{DocSource | domain=Linux kernel | path=crypto/index.html}}<br /> 2- {{DocSource | domain=Linux kernel | path=gpu/drm-uapi.html}} |
|
Yocto Project
1- {{DocSource | domain=Yocto Project | path=overview-manual/overview-manual.html}}<br /> 2- {{DocSource | domain=Yocto Project | path=brief-yoctoprojectqs/brief-yoctoprojectqs.html}} |
1- overview-manual/overview-manual.html |
AWS IoT Greengrass
1- {{DocSource | domain=AWS Greengrass | path=developerguide/what-is-gg.html}}<br /> 2- {{DocSource | domain=AWS Greengrass | path=developerguide/device-config-setup.html}} |
1- developerguide/what-is-gg.html |
U-Boot
1- {{DocSource | domain=U-Boot | path=index.html}}<br /> 2- {{DocSource | domain=U-Boot | path=build/index.html}} |
1- index.html |
TF-A
1- {{DocSource | domain=TF-A | path=index.html}}<br /> 2- {{DocSource | domain=TF-A | path=getting_started/index.html}} |
|
OP-TEE_OS
1- {{DocSource | domain=OP-TEE_OS | path=general/index.html}}<br /> 2- {{DocSource | domain=OP-TEE_OS| path=index.html}} |
1- general/index.html |
3. More examples[edit source]
You type | You get |
---|---|
Linux kernel
1- {{DocSource | domain=Linux kernel | path=crypto/index.html}}<br /> 2- {{DocSource | domain=Linux kernel | path=crypto/index.html | text=Linux Kernel Crypto API}}<br /> 3- {{DocSource | domain=Linux kernel | path=crypto/index.html | version=4.19}}<br /> 4- {{DocSource | domain=Linux kernel | path=crypto/index.html | text=Linux Kernel Crypto API | version=4.19}} |
1- crypto/index.html |
Yocto Project
1- {{DocSource | domain=Yocto Project | path=overview-manual/overview-manual.html}}<br /> 2- {{DocSource | domain=Yocto Project | path=overview-manual/overview-manual.html | text=Yocto Project Overview and Concepts Manual}}<br /> 3- {{DocSource | domain=Yocto Project | path=overview-manual/overview-manual.html | version=3.0}}<br /> 4- {{DocSource | domain=Yocto Project | path=overview-manual/overview-manual.html | text=Yocto Project Overview and Concepts Manual | version=3.0}} |
1- overview-manual/overview-manual.html |
AWS IoT Greengrass
1- {{DocSource | domain=AWS Greengrass | path=developerguide/what-is-gg.html}}<br /> 2- {{DocSource | domain=AWS Greengrass | path=developerguide/what-is-gg.html | text=What is AWS IoT Greengrass?}}<br /> 3- {{DocSource | domain=AWS Greengrass | path=developerguide/what-is-gg.html | version=2.0}}<br /> 4- {{DocSource | domain=AWS Greengrass | path=developerguide/what-is-gg.html | text=What is AWS IoT Greengrass? | version=2.0}} |
1- developerguide/what-is-gg.html |
U-Boot
1- {{DocSource | domain=U-Boot | path=build/index.html}}<br /> 2- {{DocSource | domain=U-Boot | path=build/index.html | text=How to build U-Boot?}}<br /> 3- {{DocSource | domain=U-Boot | path=build/index.html | version=2021.01}}<br /> 4- {{DocSource | domain=U-Boot | path=build/index.html | text=How to build U-Boot? | version=2021.01}} |
1- build/index.html |
TF-A
1- {{DocSource | domain=TF-A| path=getting_started/docs-build.html}}<br /> 2- {{DocSource | domain=TF-A| path=getting_started/docs-build.html| text=Building Documentation}}<br /> 3- {{DocSource | domain=TF-A| path=getting_started/docs-build.html| version=2.5}}<br /> 4- {{DocSource | domain=TF-A| path=getting_started/docs-build.html| text=Building Documentation| version=2.5}} |
1- getting_started/docs-build.html |
OP-TEE_OS
1- {{DocSource | domain=OP-TEE_OS| path=architecture/index.html}}<br /> 2- {{DocSource | domain=OP-TEE_OS| path=architecture/index.html | text=Architecture}}<br /> 3- {{DocSource | domain=OP-TEE_OS| path=architecture/index.html| version=3.14.0}}<br /> 4- {{DocSource | domain=OP-TEE_OS| path=architecture/index.html | text=Architecture | version=3.14.0}} |
1- architecture/index.html |
Check that there's no space before and after the text
1- BEFORE{{DocSource | domain=Linux kernel | path=crypto/index.html}}AFTER<br /> 2- BEFORE{{DocSource | domain=Linux kernel | path=crypto/index.html | text=Linux Kernel Crypto API}}AFTER<br /> 3- BEFORE{{DocSource | domain=Linux kernel | path=crypto/index.html | version=4.19}}AFTER<br /> 4- BEFORE{{DocSource | domain=Linux kernel | path=crypto/index.html | text=Linux Kernel Crypto API | version=4.19}}AFTER |
1- BEFOREcrypto/index.htmlAFTER |
Unsupported domain
{{DocSource | domain=Unsupported domain | path=Document}} |
Unsupported domain! |
4. Code[edit source]
Linux kernel: [https://www.kernel.org/doc/html/{{#if: {{{version|}}}|v{{#replace:{{{version|}}}| |}}|v5.15}}/{{#replace:{{{path|}}}| |}} {{#if: {{{text|}}}|{{{text}}}|{{{path}}}}}{{#if: {{{version|}}}| (v{{#replace:{{{version|}}}| |}})}}]
Yocto Project: [https://docs.yoctoproject.org/{{#if: {{{version|}}}|{{#replace:{{{version|}}}| |}}|4.0}}/{{#replace:{{{path|}}}| |}} {{#if: {{{text|}}}|{{{text}}}|{{{path}}}}}{{#if: {{{version|}}}| (v{{#replace:{{{version|}}}| |}})}}]
AWS IoT Greengrass [https://docs.aws.amazon.com/greengrass/{{#if: {{{version|}}}|{{#replace:{{{version|}}}| |}}|latest}}/{{#replace:{{{path|}}}| |}} {{#if: {{{text|}}}|{{{text}}}|{{{path}}}}}{{#if: {{{version|}}}| v({{#replace:{{{version|}}}| |}})}}]
U-Boot: [https://u-boot.readthedocs.io/en/{{#if: {{{version|}}}|{{#replace:{{{version|}}}| |}}|v2021.07}}/{{#replace:{{{path|}}}| |}} {{#if: {{{text|}}}|{{{text}}}|{{{path}}}}}{{#if: {{{version|}}}| (v{{#replace:{{{version|}}}| |}})}}]
TF-A: [https://trustedfirmware-a.readthedocs.io/en/{{#if: {{{version|}}}|{{#replace:{{{version|}}}| |}}|v2.6}}/{{#replace:{{{path|}}}| |}} {{#if: {{{text|}}}|{{{text}}}|{{{path}}}}}{{#if: {{{version|}}}| (v{{#replace:{{{version|}}}| |}})}}]
OP-TEE_OS: [https://optee.readthedocs.io/en/{{#if: {{{version|}}}|{{#replace:{{{version|}}}| |}}|3.16.0}}/{{#replace:{{{path|}}}| |}} {{#if: {{{text|}}}|{{{text}}}|{{{path}}}}}{{#if: {{{version|}}}| (v{{#replace:{{{version|}}}| |}})}}]
Unsupported domain!