Populate the target and boot the image

Revision as of 12:22, 17 February 2020 by Registered User (→‎Populate the SDCard)

STM32MP157C-EV1.png
Let's start Develop on Arm® Cortex®-A7
Step category in.png Unpack the board Step.png Populate the target and boot the image Step.png Execute basic commands Step.png Use the demo launcher Step category out.png


1. Overview[edit source]

This stage explains how to get, install and boot the STM32MP15 Evaluation boards with the Starter Package.

2. Open a terminal[edit source]

Open a terminal on the host computer.

Ubuntu terminal

All the commands preceded by have to be executed from the host computer terminal.

  • Create your STM32MPU workspace directory on the host computer:
 mkdir $HOME/STM32MPU_workspace
 cd $HOME/STM32MPU_workspace

3. Check the host computer Internet access[edit source]

  • An Internet access through http and https protocols must be provided.

The command below enables checking for Internet access through http/https protocols:

 wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy."

If an 'OK' message is returned, the network is correctly configured.
In this case, skip the rest of this section.

Otherwise, a proxy for http/https protocols is required.
The best solution is to set this proxy through the shell variables http_proxy and https_proxy:

 export http_proxy=http://<MyProxyLogin>:<MyProxyPassword>@<MyProxyServerUrl>:<MyProxyPort>
 export https_proxy=http://<MyProxyLogin>:<MyProxyPassword>@<MyProxyServerUrl>:<MyProxyPort>

Check again the Internet access using the command:

 wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy."

4. Install the tools[edit source]

4.1. STM32CubeProgrammer[edit source]

  • Create your STM32MPU tools directory on the host computer:
 mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools
 mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z
  • Create a temporary directory in your STM32MPU workspace:
 mkdir $HOME/STM32MPU_workspace/tmp
  • Uncompress the archive file to get the STM32CubeProgrammer installers:
 cd $HOME/STM32MPU_workspace/tmp
 unzip SetupSTM32CubeProgrammer.zip
  • Execute the Linux® installer, which guides you through the installation process. Select "$HOME/STM32MPU-Tools/STM32CubeProgrammer-x.y.z" as installation directory when it is requested by the installer.
 ./SetupSTM32CubeProgrammer-x.y.z.linux

The screenshots below have been obtained with old STM32CubeProgrammer V2.7.0. They are provided as examples and are still valid for higher versions :

Splash screen
Welcome page
Installation path
  • Add the STM32CubeProgrammer binary path to your PATH environment variable:
export PATH=$HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z/bin:$PATH
  • Check that the STM32CubeProgrammer tool is properly installed and accessible:
 STM32_Programmer_CLI --h
     -------------------------------------------------------------------
                       STM32CubeProgrammer vx.y.z                  
     -------------------------------------------------------------------

4.2. USB serial link[edit source]

  • Install the libusb on your host computer:
 sudo apt-get install libusb-1.0-0
  • To allow STM32CubeProgrammer to access the USB port through low-level commands, proceed as follows:
 cd $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z/Drivers/rules
 sudo cp *.* /etc/udev/rules.d/

5. Download the image[edit source]

  • Create your STM32MP1 Starter Package directory on the host computer:
 mkdir $HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0
 mkdir $HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Starter-Package
 cd $HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Starter-Package
  • Download the STM32MP1-Ecosystem-v4.1.0 Starter Package into the following directory:
    $HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Starter-Package
  • Uncompress the tarball file to get the binaries for the different partitions of the image, and the Flash layout files
 tar xvf en.FLASH-stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23.tar.gz


6. Populate the SDCard[edit source]

  • Set the boot switches (located at the back of the board) to the off position
boot switches position to flash the board
  • Connect USB Type A to Type C cable between PC and CN7/USB_OTG port of the DK2
  • Power up the board
  • Press the reset button to reset the board
  • Launch STM32CubeProgrammer to get the GUI
  • On the right select USB ( not STLINK ! ) in the connexion pick list and click on refresh button. Serial Number is displayed if USB is detected. Click on "Connect"
  • Select "Open File" tab and pick in the Starter Package installation folder in $[Starter_Pack_Path]/images/stm32mp1/flashlayout_st-image-weston the FlashLayout_sdcard_stm32mp157c-ev1-trusted.tsv.
  • Fill the "Binaries Path" by browsing up to folder $[Starter_Pack_Path]/images/stm32mp1
  • Click on "Download" to start the flashing process.
  • Progress is displayed with progress bar till completion popup message.

7. Boot the board[edit source]

  • Set the boot switches (located at the back of the board) to the on position
boot switches position to boot the board
  • Power up the board
  • Press the reset button to reset the board
  • After few seconds, the board starts and automatically go through the following screens
UBoot splash screen
Linux splash screen
Weston desktop
GTK demo launcher


Back button.png Overview button.png Next button.png