This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Usage
The Board template is used to indicate for which board(s), an article part (chapter, paragraph, table...) is valid. Per default (i.e. if this template is not used), any part of an article is valid for all boards for which the entire article is valid.
It outputs a "standardized" string that might be used to name an article part.
Usage: {{Board | type=<type>}}
- Where:
- <type> is the mandatory identifier of the board type. The possible values are:
- 157A-EV1: STM32MP157A-EV1 Evaluation board
- 157C-EV1: STM32MP157C-EV1 Evaluation board
- 157x-EV1: any of the previous two
- 157A-DK1: STM32MP157A-DK1 Discovery kit
- 157C-DK2: STM32MP157C-DK2 Discovery kit
- 157x-DKx: any of the previous two
Clicking on the File:Info.png icon displays the article about the board (e.g. STM32MP157X-DKX - hardware description).
2. Basic examples
You type | You get |
---|---|
STM32MP157C-EV1 Evaluation board
{{Board | type=157C-EV1}} |
STM32MP157C-EV1 Evaluation boardFile:Info.png |
STM32MP157C-DK2 Discovery kit
{{Board | type=157C-DK2}} |
STM32MP157C-DK2 Discovery kitFile:Info.png |
3. More examples
You type | You get |
---|---|
Unspecified board
{{Board}} |
STM32MP unknown board type identifier |
Unknown board
{{Board | type=153C-EV1}} |
STM32MP153C-EV1 unknown board type identifier |
Unknown lines
{{Board | type=157C-DK3}} |
STM32MP157C-DK3 unknown board type identifier |
4. Code
STM32MP unknown board type identifier