This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User (Created page with "<noinclude> ==Usage== The GDB$ template is used '''to prefix a command that must be executed on GDB, with a GDB-specific prompt'''. Usage: <nowiki>{{</now...") |
Registered User (Merge articles) |
||
(2 intermediate revisions by the same user not shown) | |||
Line 1: | Line 1: | ||
<noinclude> | <noinclude> | ||
==Usage== | ==Usage== | ||
The [[Template:GDB$|GDB$]] template is used '''to prefix a command that must be executed on GDB, with a GDB-specific prompt'''. | The [[Template:GDB$|GDB$]] template is used '''to prefix a command that must be executed on GDB, with a GDB-specific prompt'''.<br> | ||
Thanks to the <code>gdb-prompt</code> class defined in [[MediaWiki:Common.css]], a double (or triple) click to select the command doesn't select the prompt. | |||
Usage: <nowiki>{{</nowiki>GDB$}} | Usage: <nowiki>{{</nowiki>GDB$}} | ||
{{Important | Do not insert any space between "<nowiki>{{GDB$}}</nowiki>" and the command.}} | |||
==Basic examples== | ==Basic examples== | ||
Line 9: | Line 12: | ||
! You type !! You get | ! You type !! You get | ||
|- | |- | ||
| <code> | | <code>info break</code> command executed on GDB | ||
<pre style="white-space: pre-wrap;"> | <pre style="white-space: pre-wrap;"> | ||
{{GDB$}} | {{GDB$}}show listsize<br> | ||
Number of source lines gdb will list by default is 10. | |||
</pre> | </pre> | ||
| | | | ||
{{GDB$}} | {{GDB$}}show listsize<br> | ||
Number of source lines gdb will list by default is 10. | |||
|} | |} | ||
==More examples== | |||
{| class="st-table" | |||
! You type !! You get | |||
|- | |||
| 2 commands executed on GDB and preformatted text block (space at the beginning of each line) | |||
<pre style="white-space: pre-wrap;"> | |||
{{GDB$}}show listsize | |||
Number of source lines gdb will list by default is 10. | |||
{{GDB$}}continue | |||
</pre> | |||
| | |||
{{GDB$}}show listsize | |||
Number of source lines gdb will list by default is 10. | |||
{{GDB$}}continue | |||
|- | |||
| Command executed on GDB and preformatted text block (space at the beginning of each line) | |||
<pre style="white-space: pre-wrap;"> | |||
{{GDB$}}show listsize | |||
Number of source lines gdb will list by default is 10. | |||
</pre> | |||
| | |||
{{GDB$}}show listsize | |||
Number of source lines gdb will list by default is 10. | |||
|- | |||
| Long command executed on GDB and preformatted text block (space at the beginning of each line) | |||
<pre style="white-space: pre-wrap;"> | |||
{{GDB$}}this is a so long command executed on GDB that a horizontal scrolling bar is needed | |||
</pre> | |||
| style="max-width:30em;" | | |||
{{GDB$}}this is a so long command executed on GDB that a horizontal scrolling bar is needed | |||
|- | |||
| Template used within another public message box template | |||
<pre style="white-space: pre-wrap;"> | |||
{{Info | | |||
Message before the command | |||
{{GDB$}}show listsize | |||
Number of source lines gdb will list by default is 10. | |||
Message after the command | |||
}} | |||
</pre> | |||
| | |||
{{Info | | |||
Message before the command | |||
{{GDB$}}show listsize | |||
Number of source lines gdb will list by default is 10. | |||
Message after the command | |||
}} | |||
|- | |||
| Template used within another protected message box template | |||
<pre style="white-space: pre-wrap;"> | |||
{{InternalInfo | | |||
Message before the command | |||
{{GDB$}}show listsize | |||
Number of source lines gdb will list by default is 10. | |||
Message after the command | |||
}} | |||
</pre> | |||
| | |||
{{InternalInfo | | |||
Message before the command | |||
{{GDB$}}show listsize | |||
Number of source lines gdb will list by default is 10. | |||
Message after the command | |||
}} | |||
|} | |||
==Maintenance== | |||
This template is a template common to all ST wikis. <br> | |||
Modifications must be done into the [[stwikimodel:Template:GDB$|WikiModel]]. They must be reviewed by all ST wikis maintainers.<br> | |||
When approved, the template can be pushed/merged towards all ST wikis. | |||
==Code== | ==Code== | ||
</noinclude> | </noinclude><span class{{=}}"gdb-prompt"></span> |
Latest revision as of 17:58, 16 March 2023
1. Usage[edit source]
The GDB$ template is used to prefix a command that must be executed on GDB, with a GDB-specific prompt.
Thanks to the gdb-prompt
class defined in MediaWiki:Common.css, a double (or triple) click to select the command doesn't select the prompt.
GDB$}}Usage: {{
2. Basic examples[edit source]
You type | You get |
---|---|
info break command executed on GDB
GDB$}}show listsize<br> Number of source lines gdb will list by default is 10.{{ |
show listsize |
3. More examples[edit source]
You type | You get |
---|---|
2 commands executed on GDB and preformatted text block (space at the beginning of each line)
GDB$}}show listsize Number of source lines gdb will list by default is 10. {{GDB$}}continue{{ |
show listsize
Number of source lines gdb will list by default is 10.
continue
|
Command executed on GDB and preformatted text block (space at the beginning of each line)
GDB$}}show listsize Number of source lines gdb will list by default is 10.{{ |
show listsize
Number of source lines gdb will list by default is 10.
|
Long command executed on GDB and preformatted text block (space at the beginning of each line)
GDB$}}this is a so long command executed on GDB that a horizontal scrolling bar is needed{{ |
GDB that a horizontal scrolling bar is neededthis is a so long command executed on |
Template used within another public message box template
GDB$}}show listsize Number of source lines gdb will list by default is 10. Message after the command }}{{Info | Message before the command {{ |
|
Template used within another protected message box template
GDB$}}show listsize Number of source lines gdb will list by default is 10. Message after the command }}{{InternalInfo | Message before the command {{ |
4. Maintenance[edit source]
This template is a template common to all ST wikis.
Modifications must be done into the WikiModel. They must be reviewed by all ST wikis maintainers.
When approved, the template can be pushed/merged towards all ST wikis.
5. Code[edit source]