Last edited 2 years ago

STM32MPU distribution for Android: Difference between revisions

Registered User
No edit summary
Registered User
mNo edit summary
 
(6 intermediate revisions by 3 users not shown)
Line 1: Line 1:
The '''STM32MPU distribution for Android&trade;''' runs on Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-A processors. It is a subset of the [[:Category:STM32MPU Embedded Software distribution for Android|STM32MPU Embedded Software distribution for Android]].
<noinclude>{{ApplicableFor
[[File:STM32MPU_distribution_for_Android.png|thumb|100px|link=]]
|MPUs list=STM32MP15x
 
|MPUs checklist=STM32MP13x, STM32MP15x
It includes the following collection of software components:
}}</noinclude>
* The '''OpenSTLinux BSP''' that offers services for the application frameworks in the same context:
** The [[Boot_chains_overview|boot chain]] based on [[TF-A overview|TF-A]] and [[U-Boot overview|U-Boot]].
** The [[OP-TEE overview|OP-TEE ]] secure OS running on the Cortex-A core in Secure mode.
** The '''Linux<sup>&reg;</sup> kernel''' running on the Arm® Cortex®-A core in Non-secure mode.
* '''Application frameworks''' that rely on the services provided by the '''OpenSTLinux BSP''' to provide specific functionalities (such as code libraries, APIs and tool sets) to ease the development of software applications:
** '''OP-TEE''' application frameworks running in the secure OS user space (eg TEE Internal core API for the development of Trusted Applications (TA)).
** '''Android''' application frameworks running in Linux OS user space (see AOSP<ref>https://source.android.com/</ref> for more details).
 
The '''OpenSTLinux BSP for Android''' has some specificities:
* The Linux kernel source is based on the Common Kernel available in AOSP<ref>https://android.googlesource.com/kernel/common/</ref>.
* The Linux kernel configuration is based on the reference configuration available in AOSP<ref>https://android.googlesource.com/kernel/configs/</ref>.
 
'''Android''' application frameworks are based on the AOSP platform manifest<ref>https://android.googlesource.com/platform/manifest/</ref>. By default, one of the Google tags<ref>https://source.android.com/setup/start/build-numbers#source-code-tags-and-builds</ref> is used as a reference.
 
The '''Google services''' (ex: Cast, Drive, Maps...) are neither embedded nor validated within this '''STM32MPU distribution for Android&trade;'''.
 
==How to get the software for this distribution?==
The '''STM32MPU distribution for Android&trade;''' is available through the three Packages (Starter, Developer, and Distribution) of the [[:Category:STM32MPU Embedded Software distribution for Android|STM32MPU Embedded Software distribution for Android]].
 
==References==
<references/>


{{EcosystemFlow/Archives | custom=Android | flow=v2}}
<noinclude>
<noinclude>
[[Category:Android distribution|0]]
{{NoIndex}}
[[Category:Android]]
[[Category:Android]]
{{PublicationRequestId | 12864 | 30Jul'19}}
</noinclude>
</noinclude>

Latest revision as of 17:16, 30 January 2023

Applicable for STM32MP15x lines

STM32MPU Embedded Software distribution for Android™ is no more supported by ST. You can contact our ST partner, Witekio, who can help you to port and maintain it on STM32MP15 platform.