This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User m (→Usage) |
Registered User mNo edit summary |
||
(9 intermediate revisions by 2 users not shown) | |||
Line 6: | Line 6: | ||
Where: | Where: | ||
* {{HighlightParam|<flow>}} is the identifier of the wiki. 2 values are possible: | * {{HighlightParam|<flow>}} is the identifier of the wiki. 2 values are possible: | ||
** '''Current''': the meaning of message associated to the ''Current'' flow (here | ** '''Current''': the meaning of message associated to the ''Current'' flow (here v4) highlights the fact that the article or chapter has not been updated for the Current version (here v4). To be used when the article should have been updated for the Current version (here v4) but the update has not been done yet. | ||
** '''Next''' : the meaning of message associated to the ''Next'' flow (here | ** '''Next''' : the meaning of message associated to the ''Next'' flow (here v5) highlights that the article has been updated for ''Next'' version (here v5) in ''Current'' version (here v4) . Consequently, this updated version must not be published yet. | ||
Generally speaking, Current corresponds to current flow, and Next corresponds to the up coming flow. | Generally speaking, Current corresponds to current flow, and Next corresponds to the up coming flow. | ||
Line 73: | Line 73: | ||
==Code== | ==Code== | ||
</noinclude>{{#switch: {{{flow|}}} | </noinclude>{{#switch: {{{flow|}}} | ||
| Current= {{Warning|This section has not been yet updated for the STM32 MPU ecosystem- | | Current= {{Warning|This section has not been yet updated/tested for/with the STM32 MPU ecosystem-v4.<br> Information provided in this section may not be fully applicable for v4 and you may need to proceed to some adaptations. <br>We apologize for this inconvenient.}} | ||
| Next= {{InternalInfo|Warning for the maintainer(s) of this article: this article has been updated for | | Next= {{InternalInfo|Warning for the maintainer(s) of this article: this article has been updated for v5.}} | ||
| #default = {{Highlight|unknown flow}}</br> | | #default = {{Highlight|unknown flow}}</br> | ||
}} | }} |
Latest revision as of 13:49, 28 March 2022
1. Usage[edit source]
The EcosystemFlow/Warning template is used to insert a message about the current status of the article or chapter containing it.
<flow> }}Usage: {{EcosystemFlow/Warning| flow=
Where:
- <flow> is the identifier of the wiki. 2 values are possible:
- Current: the meaning of message associated to the Current flow (here v4) highlights the fact that the article or chapter has not been updated for the Current version (here v4). To be used when the article should have been updated for the Current version (here v4) but the update has not been done yet.
- Next : the meaning of message associated to the Next flow (here v5) highlights that the article has been updated for Next version (here v5) in Current version (here v4) . Consequently, this updated version must not be published yet.
Generally speaking, Current corresponds to current flow, and Next corresponds to the up coming flow.
The returned value is:
- a generic or custom message depending on the parameters
- "unknown flow", if <flow> is not supported.
2. Basic examples[edit source]
You type | You get | ||
---|---|---|---|
Generic message
{{EcosystemFlow/Warning}}
|
unknown flow | ||
Message when flow is Current
{{EcosystemFlow/Warning | flow=Current}}
|
| ||
Message when flow is Next
{{EcosystemFlow/Warning | flow=Next}}
|
3. More examples[edit source]
You type | You get | ||
---|---|---|---|
Unknown flow
{{EcosystemFlow/Warning | flow=v0}}
|
unknown flow | ||
Unspecified flow
{{EcosystemFlow/Warning}}
|
unknown flow | ||
Check that there's no space before and after the text
BEFORE{{EcosystemFlow/Warning}}AFTER<br>
BEFORE{{EcosystemFlow/Warning | flow=Current}}AFTER<br>
BEFORE{{EcosystemFlow/Warning |flow=Next}}AFTER
|
BEFOREunknown flow
BEFOREAFTER |
4. Code[edit source]
unknown flow