This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User mNo edit summary |
Registered User mNo edit summary |
||
(13 intermediate revisions by 4 users not shown) | |||
Line 1: | Line 1: | ||
<noinclude>{{ApplicableFor | |||
|MPUs list=STM32MP15x | |||
|MPUs checklist=STM32MP13x, STM32MP15x | |||
}}</noinclude> | |||
<bookshelf src="Book:Getting started" /> | <bookshelf src="Book:Getting started" /> | ||
<center> | <center> | ||
Line 12: | Line 16: | ||
<br> | <br> | ||
The | The STM32MP157x-DK2 Discovery kit is a flexible and complete solution for evaluating the capabilities of STM32MP15 microprocessor devices.<br> | ||
This module explains the basic steps to | This module explains the basic steps to control your STM32MP157x-DK2 board. | ||
{{Info|To complete this module, it is assumed a Linux<sup>®</sup> PC running under Ubuntu<sup>®</sup> 20.04 is used. | |||
Refer to [[PC_prerequisites]] }} | |||
<br> | <br> | ||
{| class="st-table" style="margin: auto" | {| class="st-table" style="margin: auto" | ||
| style="border-style: hidden; width:120px; text-align:left" | [[Image:back_button.png|link=Getting started/STM32MP1 boards/STM32MP157x-DK2]] | | style="border-style: hidden; width:120px; text-align:left" | [[Image:back_button.png|link=Getting started/STM32MP1 boards/STM32MP157x-DK2]] | ||
Line 25: | Line 32: | ||
<noinclude> | <noinclude> | ||
{{DISPLAYTITLE:{{SUBPAGENAME}}}} | {{DISPLAYTITLE:{{SUBPAGENAME}}}} | ||
[[Category:STM32MP157x-DK2 - let's start | 00]] | [[Category:STM32MP157x-DK2 - let's start|00]] | ||
{{PublicationRequestId | | {{PublicationRequestId | 19645 | 2021-04-19}} | ||
</noinclude> | </noinclude> |
Latest revision as of 20:34, 2 December 2021

The STM32MP157x-DK2 Discovery kit is a flexible and complete solution for evaluating the capabilities of STM32MP15 microprocessor devices.
This module explains the basic steps to control your STM32MP157x-DK2 board.
File:Info.png | To complete this module, it is assumed a Linux® PC running under Ubuntu® 20.04 is used.
Refer to PC_prerequisites |