This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Usage
The Info template is used to draw attention to a particularly important point.
It puts a message box with a "dark blue info" icon in the page.
Usage: {{Info | <message>}}
Where <message> is the optional info message. If this parameter is not set, the default message is "Info".
2. Basic examples
You type | You get |
---|---|
Info without specific info message
{{Info}} |
|
Info with specific Info message
{{Info | Note that the below actions are optional but recommended}} |
|
3. More examples
You type | You get |
---|---|
Info with a long info message
{{Info | The info message is a long sentence. Lorem ipsum: isdem diebus Apollinaris Domitiani gener, paulo ante agens palatii Caesaris curam, ad Mesopotamiam missus a socero per militares numeros immodice scrutabatur, an quaedam altiora meditantis iam Galli.}} |
|
Check that the spaces before and after the info message
BEFORE{{Info | Check spaces}}AFTER<br> BEFORE {{Info | Check spaces}} AFTER |
BEFORE AFTER BEFORE AFTER |
4. Maintenance
This template is a template common to all ST wikis.
Modifications must be done into the WikiModel. They must be reviewed by all ST wikis maintainers.
When approved, the template can be pushed/merged towards all ST wikis.