1. Usage[edit source]
The DocSource template is used to indicate the URL of any Linux® kernel, Yocto Project, and AWS IoT Greengrass document used in this wiki.
Usage: {{DocSource | domain=<domain> | path=<path> | text=<link text> | version=<version>}}
- Where:
- <domain> is the mandatory string that identifies the domain of the document. The possible values are:
- Linux kernel: the document belongs to the Linux kernel domain.
- Yocto Project: the document belongs to the Yocto Project domain.
- AWS Greengrass: the document belongs to the AWS IoT Greengrass domain.
- <path> is the mandatory relative path of the document from the root URL of the domain. The root URLs are:
- https://www.kernel.org/doc/html/ for the Linux kernel domain
- https://www.yoctoproject.org/docs/ for the Yocto Project domain
- https://docs.aws.amazon.com/greengrass/ for the AWS IoT Greengrass domain
- <link text> is an optional link text (text that is displayed instead of the URL).
- <version> is an optional version number (branch or tag) if the default one doesn't fit. Per default, the URL points to:
- the v5.4 branch of the Linux kernel
- the 3.1 branch of the Yocto Project
- the latest branch of the AWS IoT Greengrass
2. Basic examples[edit source]
You type | You get |
---|---|
Linux kernel
1- {{DocSource | domain=Linux kernel | path=crypto/index.html}} 2- {{DocSource | domain=Linux kernel | path=gpu/drm-uapi.html}} |
|
Yocto Project
1- {{DocSource | domain=Yocto Project | path=overview-manual/overview-manual.html}} 2- {{DocSource | domain=Yocto Project | path=brief-yoctoprojectqs/brief-yoctoprojectqs.html}} |
1- overview-manual/overview-manual.html |
AWS IoT Greengrass
1- {{DocSource | domain=AWS Greengrass | path=developerguide/what-is-gg.html}} 2- {{DocSource | domain=AWS Greengrass | path=developerguide/device-config-setup.html}} |
1- developerguide/what-is-gg.html |
3. More examples[edit source]
You type | You get |
---|---|
Linux kernel
1- {{DocSource | domain=Linux kernel | path=crypto/index.html}} 2- {{DocSource | domain=Linux kernel | path=crypto/index.html | text=Linux Kernel Crypto API}} 3- {{DocSource | domain=Linux kernel | path=crypto/index.html | version=4.19}} 4- {{DocSource | domain=Linux kernel | path=crypto/index.html | text=Linux Kernel Crypto API | version=4.19}} |
1- crypto/index.html |
Yocto Project
1- {{DocSource | domain=Yocto Project | path=overview-manual/overview-manual.html}} 2- {{DocSource | domain=Yocto Project | path=overview-manual/overview-manual.html | text=Yocto Project Overview and Concepts Manual}} 3- {{DocSource | domain=Yocto Project | path=overview-manual/overview-manual.html | version=3.0}} 4- {{DocSource | domain=Yocto Project | path=overview-manual/overview-manual.html | text=Yocto Project Overview and Concepts Manual | version=3.0}} |
1- overview-manual/overview-manual.html |
AWS IoT Greengrass
1- {{DocSource | domain=AWS Greengrass | path=developerguide/what-is-gg.html}} 2- {{DocSource | domain=AWS Greengrass | path=developerguide/what-is-gg.html | text=What is AWS IoT Greengrass?}} 3- {{DocSource | domain=AWS Greengrass | path=developerguide/what-is-gg.html | version=2.0}} 4- {{DocSource | domain=AWS Greengrass | path=developerguide/what-is-gg.html | text=What is AWS IoT Greengrass? | version=2.0}} |
1- developerguide/what-is-gg.html |
Unsupported domain
{{DocSource | domain=Unsupported domain | path=Document}} |
Unsupported domain! |
4. Code[edit source]
Linux kernel: [https://www.kernel.org/doc/html/{{#if: {{{version|}}}|v{{#replace:{{{version|}}}| |}}|v5.4}}/{{#replace:{{{path|}}}| |}} {{#if: {{{text|}}}|{{{text}}}|{{{path}}}}} {{#if: {{{version|}}}|(v{{#replace:{{{version|}}}| |}})}}]
Yocto Project: [https://www.yoctoproject.org/docs/{{#if: {{{version|}}}|{{#replace:{{{version|}}}| |}}|3.1}}/{{#replace:{{{path|}}}| |}} {{#if: {{{text|}}}|{{{text}}}|{{{path}}}}} {{#if: {{{version|}}}|(v{{#replace:{{{version|}}}| |}})}}]
AWS IoT Greengrass [https://docs.aws.amazon.com/greengrass/{{#if: {{{version|}}}|{{#replace:{{{version|}}}| |}}|latest}}/{{#replace:{{{path|}}}| |}} {{#if: {{{text|}}}|{{{text}}}|{{{path}}}}} {{#if: {{{version|}}}|({{#replace:{{{version|}}}| |}})}}]
Unsupported domain!