This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This article provides the following information:
- How to download and install the latest Linux kernel for the STM32 microprocessor Series used
- Where to find the associated release note
- Where to find the previous releases (archives)
1. STM32MP15-Ecosystem-v2.0.0 release[edit source]
- The STM32MP1 Linux kernel is delivered through a tarball file named :
- 'en.SOURCES-kernel-stm32mp1-openstlinux-20-02-19.tar.xz for STM32MP157C-EV1 and STM32MP157X-DKX boards
- Download and install the STM32MP1 Linux kernel
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here.
STM32MP1 Developer Package Linux kernel - STM32MP15-Ecosystem-v2.0.0 release | |
---|---|
Download |
You need to be logged on to my.st.com before accessing the following link |
Installation |
$ cd <working directory path>/Developer-Package
$ tar xvf en.SOURCES-kernel-stm32mp1-openstlinux-20-02-19.tar.xz $ cd stm32mp1-openstlinux-20-02-19/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.4-r0/ $ tar xvf linux-5.4.31.tar.xz |
Release note |
Details of the content of the Linux kernel are available in the associated STM32MP15 OpenSTLinux release note. |
- The Linux kernel installation directory is in the <Developer Package installation directory>/stm32mp1-openstlinux-20-02-19/sources/arm-ostl-linux-gnueabi directory, and is named linux-stm32mp-<kernel version>:
linux-stm32mp-5.4-r0 Linux kernel installation directory ├── [*].patch ST patches to apply during the Linux kernel preparation (see next chapter) ├── fragment-[*].config ST configuration fragments to apply during the Linux kernel configuration (see next chapter) ├── linux-5.4.31 Linux kernel source code directory ├── linux-5.4.31.tar.xz Tarball file of the Linux kernel source code ├── README.HOW_TO.txt Helper file for Linux kernel management: reference for Linux kernel build └── series List of all ST patches to apply