This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Usage[edit source]
This template is used to indicate that the command that follows, must be executed on the U-boot board prompt
{{U-Boot$}} h
2. Example[edit source]
h command executed on the board U-boot prompt
Board STM32MP> h
3. Code[edit source]
Board STM32MP>