This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Usage
The Android template is used to store, in a page, information that is related to the Android™ distribution.
It puts a message box with a "green Android" icon in the page, adds this page to the Android category.
Usage: {{Android | <message>}}
Where <message> is the optional information related to the Android™ distribution. If this parameter is not set, the default message is "Below information is related to the Android™ distribution".
2. Basic examples
You type | You get | ||
---|---|---|---|
Android without specific message
{{Android}} |
| ||
Android with specific message
{{Android | Note that the following packages are required to build an environment for Android™}} |
|
3. More examples
You type | You get | ||||
---|---|---|---|---|---|
Android with a long message
{{Android | The message is a long sentence. Lorem ipsum: isdem diebus Apollinaris Domitiani gener, paulo ante agens palatii Caesaris curam, ad Mesopotamiam missus a socero per militares numeros immodice scrutabatur, an quaedam altiora meditantis iam Galli.}} |
| ||||
Check that the spaces before and after the Android message
BEFORE{{Android | Check spaces}}AFTER<br> BEFORE {{Android | Check spaces}} AFTER |
BEFORE
BEFORE
AFTER |
4. Code
![]() |
Below information is related to the Android™ distribution, which is not available in the v3 ecosystem releases: refer to the Android page for the v2 ecosystem releases (in archived wiki) . |