eMMC update with customized trusted image

Revision as of 16:28, 20 January 2022 by Registered User

This article gives details about updating the bootloader objects of eMMC memory, located onto STM32MP157x-EV1 (e.g.), using STM32CubeIDE.

BackToNavigationTree button.png

1. Overview[edit source]

The different steps to update eMMC with customized trusted image are the following ones:

  • Initialize the eMMC with Starter Package image thanks to STM32CubeProgrammer.
  • Within STM32CubeIDE:
    • customize the trusted image, thanks to embedded STM32CubeMX generating device trees
    • compile corresponding Linux® device tree & bootloader images
    • update them on running STM32MP15 board
  • Check the new customization is correctly set up

All those steps are explained in chapters below.

2. Initialize eMMC with Starter Package[edit source]

Initialize the eMMC with Starter Package image thanks to STM32CubeProgrammer.
For that select the Starter package corresponding to the targeted STM32MP1 board and jump to chapter Downloading the image and flashing it on the board (e.g. here for STM32MP15 Evaluation board).

Before executing the next step, check the bootloader version, visible in boot messages:

  • TF-A BL2 version, booting from eMMC memory
eMMC initial setting: TF-A BL2 version
  • U-boot version & extlinux.conf file used, booting from NAND memory
eMMC initial setting: U-boot version & extlinux.conf
  • extlinux.conf content before update
eMMC initial setting: extlinux.conf content

3. Customize bootloader images and update them on running STM32MP15 board[edit source]

3.1. Build the trusted image inside STM32CubeIDE with the new expected device trees[edit source]

After customization of hardware resources within embedded STM32CubeMX, new device trees for Linux® and for bootloader are generated.
Next step is to build an update of the new trusted image; this is covered also within STM32CubeIDE with:

Note that for Linux®, only device tree has to be updated as described hereafter.

3.2. STM32MP1 board update with new Linux® device tree[edit source]

In this step, STM32MP15 board is up and running with network access: target status is green. After having compiled device tree generated by STM32CubeMX , you need to :

  • update MP15 target bootfs with new .dtb under /boot
  • and adjust /boot/mmc1_extlinux/extlinux.conf in order to declare new device tree and set it as default.

For that, follow steps explained below:

  • select the Cortex-A Linux® Deployment shortcut configuration available from Linux® project Run As... menu.
Linux® deployment configuration


  • Validate your choice and use Run button. You get in a dedicated Linux® Deployment console a message like this:
eMMC Linux® deployment message


  • Check extlinux.conf content after NAND Linux® device tree update (DEFAULT and LABEL have changed)
eMMC Linux® device tree update



Then, select Cortex-A project and right click to get Cortex-A Bootloader Deployment shortcut.

Bootloader update shortcut

Connection is automatically set and you need to scan MP15 target storage. This storage list depends on the board and on boot storage used. Then, select:

  • the storage to update, eMMC #0 here;
  • TF-A BL2 & FIP image to update from FIP_artifacts/ .


  • eMMC bootloader deployment configuration
eMMC Bootloader deployment configuration
  • eMMC bootloader deployment message
eMMC Bootloader deployment message

4. Bootloader version after customization wit STM32CubeIDE[edit source]

After the update, TF-A BL2 and U-Boot versions are modified and Linux® uses the generated Device Tree. Here are the boot messages now:

  • TF-A BL2 updated version, booting from eMMC memory
eMMC updated TF-A BL2 version
  • U-Boot updated version & Linux® device tree, booting from eMMC memory
eMMC updated U-Boot version & Linux® Device Tree

BackToNavigationTree button.png

No categories assignedEdit