This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This article provides the following information:
- How to download and install the latest U-Boot for the STM32 microprocessor Series used
- Where to find the associated release note
1. STM32MP15-Ecosystem-v3.0.0 release[edit source]
- The STM32MP1 U-Boot is delivered through a tarball file named en.SOURCES-u-boot-stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31.tar.xz for STM32MP157x-EV1 and STM32MP157x-DKx boards.
- Download and install the STM32MP1 U-Boot
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here.
STM32MP1 Developer Package U-Boot - STM32MP15-Ecosystem-v3.0.0 release | |
---|---|
Download |
You need to be logged on to my.st.com before accessing the following link |
Installation |
cd <working directory path>/Developer-Package
tar xvf en.SOURCES-u-boot-stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31.tar.xz cd stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-2020.10.r1-r0 tar xvf u-boot-stm32mp-2020.10.r1-r0.tar.gz |
Release note |
Details of the content of the U-Boot are available in the associated STM32MP15 OpenSTLinux release note. If you are interested in older releases, please have a look into the section Archives. |
- In the <Developer Package installation directory>/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-312/sources/arm-ostl-linux-gnueabi directory
- The U-Boot installation directory is named u-boot-stm32mp-<U-Boot version>:
u-boot-stm32mp-2020.10.r1-r0 U-Boot installation directory ├── [*].patch ST patches to apply during the U-Boot preparation (see next chapter) ├── u-boot-stm32mp-2020.10.r1 U-Boot source code directory ├── Makefile.sdk Makefile for the U-Boot compilation ├── README.HOW_TO.txt Helper file for U-Boot management: reference for U-Boot build ├── series List of all ST patches to apply └── u-boot-stm32mp-2020.10.r1-r0.tar.gz Tarball file of the U-Boot source code
- The FIP artifacts directory is named FIP_artifacts:
2. Archives [edit source]
This wiki is for the v3 ecosystem releases. For information about the previous ecosystem releases, go through the Wiki archives.