How to integrate LoRaWAN gateway

Revision as of 15:53, 29 July 2022 by Registered User (→‎ChirpStack server configuration)

1. Article purpose[edit source]

The purpose of this article is to explain how to integrate LoRa concentrator module to STM32MP157F-DK2 to execute application such as LoRaWAN® gateway and ChirpStack .

ChirpStack provides open source LoRaWAN® components such Network Server, Application Server, Gateway Bridge. The network server is responsible to manage the LoRaWAN® network. It also communicates with other server such as Join server and application server. Application server manages the application data of gateway ,end node devices . It also provided an interface to output the device data to third party cloud services.

LoRaWAN® Gateway transmit/receive LoRa packets from end node device to network server. It acts as a packet forwarder.

This article provides step-by-step instructions to:

  • run the ChirpStack application on STM32MP1 discovery kit.
  • to configure STM32MP1 discovery kit as LoRaWAN® Gateway/packet forwarder.

To know more about the LoRaWAN® architecture , refer the article LoRaWAN Overview.

2. Prerequisites[edit source]

2.1. Software prerequisites[edit source]

2.2. Hardware prerequisites[edit source]

2.2.1. ST hardware[edit source]

  • STM32MP157F-DK2 Discovery kit More info green.png.

The STM32MP157D-DK1 and STM32MP157F-DK2 Discovery kits leverage the capabilities of the increased-frequency 800 MHz microprocessors in the STM32MP1 Series to allow users easily develop applications using STM32 MPU OpenSTLinux Distribution software for the main processor and STM32CubeMP1 software for the co-processor.

STM32MP157F-DK2

For more information about the STM32 discovery board and how to start it up, jump to this section
Getting_started/STM32MP1_boards/STM32MP157F-DK2

  • NUCLEO-WL55JC1.

The NUCLEO-WL55JC STM32WL Nucleo-64 board provides an affordable and flexible way for users to try out new concepts and build prototypes with the STM32WL Series microcontroller, choosing from the various combinations of performance, power consumption, and features.

NUCLEO-WL55JC1

For more information about the STM32WL nucleo kit and refer the webpage
NUCLEO-WL55JC

2.2.2. Additional hardware[edit source]

  • LoRa Concentrator Module.

The concentrator module is based on Semtech SX130x digital base band chip. It has multiple channels to transmit/receive the LoRa packets from several end node devices.To know more about the baseband chip visit Semtech website
RAKWireless provides several module based on SX1301, SX1302 and SX1303 digital band band chips such as RAK2245, RAK2287, RAK5146. To know more about these modules visit the RAKwireless website.

RAKModule0.png
  • Extension Board.

It helps to connect the RAKModules to STM32MP1 Discovery kit by mapping the signal of module to 40 pin connector.

RAKModule 1.png


3. Hardware setup[edit source]

Step 1. Mount the RAK Module on the RAK extension Board.

RAKModule 2.png


Step 2. Connect the LoRa and GPS antenna to UFL connector of RAK module.

RAKModule 3.png

Step 3. Mount the RAK extension board on STM32MP1 discovery kit.

RAKModule 4.png
RAKModule 6.png

Step 4. Connect the power supply, USB cable and ethernet to discover kit.

RAKModule 5.png

4. Software setup[edit source]

To run the application, **meta-st-loragateway** layer needs to be added to OpenSTLinux distribution package . Please follow the steps given below to integrate the **meta-st-loragateway** in OpenSTLInux distribution package.

Step 1. Download and compile the STM32MP1 Distribution Package.
Step 2. Follow the default Example_of_directory_structure_for_Packages suggested by ST wiki page to follow this document synchronously.
Step 3. Download and clone the layer "meta-st-loragateway" to "meta-st" layer.

 cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystemv3.1.0/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-11-17/layers/meta-st
git clone https://github.com/amitemrkumar/meta-st-loragateway

Step 4. Set up the build configuration.

 DISTRO=openstlinux-weston MACHINE=stm32mp1 source layers/meta-st/scripts/envsetup.sh

Step 5. Add the meta-st-loragateway layer to build configuration.

 bitbake-layers add-layer ../layers/meta-st/meta-st-loragateway/

Step 6. Build your layer separately and then build the complete Distribution Layer.


 bitbake st-image-weston

Note: Building the Distribution Package for the first time may take several hours. Once the build is complete, the images are present in the following directory: build-<distro>-<machine>/tmp-glibc/deploy/images/stm32mp1.

Step 7. Follow instructions on Flashing the built image to program the new built images onto the Discovery kit.

Step 8. Now that the image is flashed on the STM32MP157F-DK2 Discovery kit . Please change the position of the boot switches in order to boot from the microSD card.

Step 9. Press the "Reset" button to reset the board.

Step 10. Now connect the minicom to the /dev/ttyACM0 device.

 minicom -D /dev/ttyACM0

Step 11. Read the IP address of the STM32MP157 discovery kit.

 ifconfig

Step 12. Connect the STM32MP157F-DK2 board using ssh connection.

 ssh root@xxx.xxx.xxx.xxx

Step 13. Run the stm32mp1-config.sh script to configure the discovery kit.

  cd /usr/local/lorawan-gateway
 ./stm32mp1-config.sh 

Loragatewayimage 1.png

5. How to run the ChirpStack application on STM32MP157F-DK2 discovery kit.[edit source]

5.1. ChirpStack Configuration[edit source]

Step 1. Select "chirpstack" option and press enter key to proceed further.
Loragatewayimage 2.png

5.1.1. Lora concentrator module configuration[edit source]

Step 1. Select "Concentrator Selection" option and press enter key to proceed further.
Loragatewayimage 3.png

Step 2. Select "RAK2287 SPI with GPS" to configure the rak2287 module and press enter key to proceed further.
Loragatewayimage 4.png

Step 3. Select "EU868" ISM band and press enter key to proceed further.
Loragatewayimage 5.png

Step 4. Select "EU863_870_1" and press enter key to proceed further.
Loragatewayimage 6.png

Step 5. Wait to complete the frequency configuration.
Loragatewayimage 8.png

Step 6. Frequency channel details will be displayed. Press enter key to proceed further.
Loragatewayimage 7.png

Step 7. If frequency configuration is correct then select Yes and press enter key to proceed further else select No and press enter key to redo the frequency configuration.
Loragatewayimage 9.png

Step 8. Please wait to complete the Frequency configuration. Once it completes then press enter key to proceed with next step.
Loragatewayimage 10.png

5.1.2. Gateway ID configuration[edit source]

Step 1. Select "Gateway ID Configuration" from the menu and press enter key to proceed with next step.
Loragatewayimage 11.png

Step 2. You have the option to enter the Gateway EUI either in auto or manual mode. In the auto configuration mode it will use mac id to generate the gateway eui. Please follow steps 3a-3b to select auto configuration mode and steps 4a-4d to configure the eui in manual mode

Step 3a. Select the "Auto configuration" mode and press enter key.
Loragatewayimage 12.png


Step 3b. Gateway eui will be displayed on the screen. Please store the gateway eui for later use. Press enter key to move to next step.
Loragatewayimage 13.png

Step 4a. Select the "Manual configuration" mode and press enter key.
Loragatewayimage 12a.png

Step 4b. Enter the gateway eui and press enter key to continue further.
Loragatewayimage 13a.png

Step 4c. Message will be displayed to show the entered value of gateway eui. If it is correct then select yes and press enter key to continue further. Otherwise select No and press enter key to enter the new value.
Loragatewayimage 13b.png

Step 4d. Gateway id configured message will appear on the screen. Press enter key to move to next configuration.
Loragatewayimage 13c.png


5.1.3. Server address and port configuration[edit source]

Step 1. Now we have to configure the server details. Select "Server configuration" and press enter key to proceed further.
Loragatewayimage 14.png

Step 2. Server address for ChirpStack is localhost and it uses port number 1700 for up/down. If the displayed values is matching then click back to move next step. Otherwise follow steps 3a-3m to modify the details of local host.
Loragatewayimage 15.png

Step 3a. To modify the server host name, please select hostname and press enter key.
Loragatewayimage 15a.png

Step 3b. Enter the server address as local host and then press enter key.
Loragatewayimage 15b.png

Step 3c. If the displayed value of hostname is correct then press enter key else select back and press enter key to change the value.
Loragatewayimage 15c.png

Step 3d. confirmation message will be displayed. Press enter key to proceed further.
Loragatewayimage 15d.png

Step 3e. To modify the port up value, select server port up and press enter key.
Loragatewayimage 15e.png

Step 3f. Enter the port up value as 1700 and then press enter key.
Loragatewayimage 15f.png

Step 3g. If the displayed value of server port up is correct then press enter key else select back and press enter key to change the value.
Loragatewayimage 15g.png

Step 3h. confirmation message will be displayed. Press enter key to proceed further.
Loragatewayimage 15h.png


Step 3i. To modify the port down value, please select server port down and press enter key.
Loragatewayimage 15i.png

Step 3j. Enter the port down value as 1700 and then press enter key.
Loragatewayimage 15j.png

Step 3k. If the displayed value of server port down is correct then press enter key else select back and press enter key to change the value.
Loragatewayimage 15k.png



Step 3l. Confirmation message will be displayed. Press enter key to proceed further.
Loragatewayimage 15l.png

Step 3m. ChirpStack hostname, port up/down is configured. Select back and press enter key to proceed next step.
Loragatewayimage 15m.png

5.1.4. Communication mode configuration[edit source]

Step 1. Select "Communication mode" from the menu and press enter key to proceed further.
Loragatewayimage 16.png

Step 2. You have an option to select either "lan" or "wlan" for the communication. Follow steps 3a-3b to configure "lan" and 4a-4e to select "wlan" mode for server communication.

Step 3a. To use lan, you have to select communication mode as "lan" from the menu and press enter key to proceed further.
Loragatewayimage 17.png

Step 3b. Confirmation message for lan selection will be displayed. Press enter key to proceed further to configure the database.
Loragatewayimage 17a.png

Step 4a. To use wifi, you have to select communication mode as "wlan" from the menu and press enter key to proceed further.
Loragatewayimage 18.png

Step 4b. Enter the ssid and press enter key to proceed further.
Loragatewayimage 19.png

Step 4c. Enter the password and press enter key to proceed further.
Loragatewayimage 20.png

Step 4d. A note for wifi will be displayed, press enter key to proceed further.
Loragatewayimage 21.png

Step 4e. Wifi selection confirmation will be appear on screen. Press enter key to proceed further.
Loragatewayimage 22.png

5.1.5. Database configuration[edit source]

Step 1. Select the "Database configuration" from the menu and press enter key to proceed further.
Loragatewayimage 23.png

Step 2. Database Password Configuration menu gives an option to modify the database password. Follow the steps3a-3i to modify the password. Otherwise select back and press enter key to proceed step.
Loragatewayimage 32.png


Step 3a. Select ChirpStack application server option from the menu to modify the password of application server and press enter key to proceed further.
Loragatewayimage 24.png

Step 3b. Enter the password and press enter key.
Loragatewayimage 25.png

Step 3c. To proceed with the modification select yes and then press enter key.
Loragatewayimage 26.png

Step 3d. Confirmation message will be displayed. Press enter key to move to next steps
Loragatewayimage 27.png

Step 3e. Select ChirpStack network server option from the menu to modify the password of network server and press enter key to proceed further.
Loragatewayimage 28.png

Step 3f. Enter the password and press enter key.
Loragatewayimage 29.png

Step 3g. To proceed with the modification select yes and press enter key.
Loragatewayimage 30.png

Step 3h. Confirmation message will be displayed. Press enter key to move to next steps.
Loragatewayimage 31.png

Step 3i. Database passwords are now successfully modified. Select back and press enter key to proceed with further configuration.
Loragatewayimage 32.png

5.1.6. Save ChirpStack configuration[edit source]

Step 1. Select the "Start ChirpStack" from the menu and press enter key to continue with the configuration. Passwords are now successfully modified.
Loragatewayimage 33.png

Step 2. Wait to complete the gateway confirmation.
Loragatewayimage 34.png

Step 3. Gateway configuration done in the previous steps will be displayed. Press enter key to continue.
Loragatewayimage 35.png

Step 4. Press enter key to proceed with selected configuration.
Loragatewayimage 36.png

Step 5. Wait for the configuration to complete.
Loragatewayimage 37.png

Step 6. Message to restart will be displayed. Press enter key to continue.
Loragatewayimage 38.png

Step 7. After the system reboots, you have to configure the chirptack webserver to connect with the end device. Please follow the section "How to configure ChirpStack server to register gateways and endnode.


5.2. ChirpStack server configuration[edit source]

Step 1. Open the ChirpStack webpage using IP address. Enter user name and password as admin.


Chirpstackserver 1.png

Step 2. Click on the "network server".

Chirpstackserver 2.png

Step 3. Click on ADD tab.

Chirpstackserver 3.png

Step 4. Enter "network server name" to identify the server and its host name along with port number. Then click on ADD NETWORK SERVER


Chirpstackserver 4.png

stm32mp1-networkserver created successfully.

Chirpstackserver 5.png

Step 5. Select "service-profiles" from the left menu. Click on + CREATE tab.

Chirpstackserver 6.png

Step 6.Enter service-profile name, select "network server" from the drop down menu. Check the Add gateway meta-data box. Click on CREATE SERVICE-PROFILE.

Chirpstackserver 7.png

service profile created successfully.

Chirpstackserver 7a.png

Step 7. Select "Device-profiles" from left menu . Then click on + CREATE tab.
Chirpstackserver 8.png

Step 8. Enter device profile information. Then click on CREATE DEVICE-PROFILE tab.
Chirpstackserver 9.png

Chirpstackserver 10.png

Device profile created successfully. Chirpstackserver 11.png

Step 9. Select "Device supports OTAA" in “JOIN(OTAA/ABP)” tab. Then click on UPDATE-DEVICE-PROFILE tab.
Chirpstackserver 12.png

Step 10. Select "Cayenne LLP" from Payload codec drop down menu in “ CODEC ” tab. Then click on UPDATE-DEVICE-PROFILE tab.
Chirpstackserver 13.png

Step 11. Select "Gateways" from left menu. Then click on + CREATE tab.
Chirpstackserver 14.png

Step 12a. Enter gateway details in the general tab.
Chirpstackserver 15.png

Step 12b. Select "Network-server" and "Service-profile" from the dropdown tab. Click on CREATE GATEWAY tab.
Chirpstackserver 16.png

Gateway configuration done successfully. Chirpstackserver 17.png

Step 13. Select "Applications" from the left menu and click on “+ CREATE” tab.
Chirpstackserver 18.png

Step 14. Enter Application details and click on “CREATE APPLICATION” tab.
Chirpstackserver 19.png

Step 14a. Click on Application name to configure the Device details.
Chirpstackserver 20.png

Step 14b. Click on “+ CREATE” tab to configure the device.
Chirpstackserver 21.png

Step 14c. Enter device details.
Chirpstackserver 22.png

Step 14d. Select "Device-profile" from the drop down menu and Click on “CREATE DEVICE.
Chirpstackserver 23.png

Step 14e.Enter Application Key in the KEYS(OTAA) tab. Click on SET DEVICE-KEYS.
Chirpstackserver 24.png

Step 14f. Device created successfully.
Chirpstackserver 25.png

""Gateway details after successful configuration.""
Chirpstackserver 26.png

""LIVE LORAWAN FRAMES captured by gateway.""
Chirpstackserver 27.png

DEVICE DATA is available at Applications. "'
Chirpstackserver 28.png

Device data captured for end nodes.
Chirpstackserver 29.png


5.3. STM32CubeMonitor Dashboard[edit source]

Step 1. Open STM32CubeMonitor Application.
Chirpstackserver 39.png

Step 2. Import stm32wl-dashboard.json in stm32cubemonitor. Click Import tab .
Chirpstackserver 40.png

Chirpstackserver 41.png

Chirpstackserver 42.png

Step 3.Open the LoRa Dashboard .
Chirpstackserver 43.png

Step 4. Double Click on application/1/device/+event/up and Enter Server Address of the gateway.
Chirpstackserver 44.png

Step 5. Enter the path to store the endnode data in json format.
Chirpstackserver 45.png

Step 6. Click on DEPLOY tab and then open DASHBOARD to view the data
Chirpstackserver 46.png

Step 7. Device details and chart will be available on the dashboard
Chirpstackserver 47.png


5.4. Cayenne integration[edit source]

Step 1. Click on INTEGRATION tab in application . Click on EDIT in myDevices.

Chirpstackserver 30.png

Step 2. Select Cayenne as myDevices endpoint from the drop down menu. Click on ADD INTEGRATION TAB.

Chirpstackserver 31.png

Step 3. Create an account at cayenne .

Chirpstackserver 32.png

Step 4. Sign-in at cayenne with your user ID.

Chirpstackserver 33.png

Step 5. Select All Device from to configure devices .

Chirpstackserver 34.png

Step 6. Search P-NCLEO-LRWAN1 in the Devices and widgets .Then select ChirpStack from LoRa drop down window .

Chirpstackserver 35.png

Step 7. Enter Device EUI then click Add device tab .

Chirpstackserver 36.png

Open the Data tab to see the dashboard.

Chirpstackserver 37.png

Live data is available in live tab.

Chirpstackserver 38.png

6. How to configure STM32MP1 discovery kit as LoRaWAN® gateway/packet forwarder[edit source]

Step 1. Select Loragateway and press enter key to proceed further.
Loragatewayimage 1.png

6.1. Lora concentrator module configuration[edit source]

Step 1. Select concentrator selection option and press enter key to proceed further.
Loragatewayimage 3a.png

Step 2. Select RAK2287 SPI with GPS to configure the rak2287 module and press enter key to proceed further.
Loragatewayimage 4.png

Step 3. Select EU868 ISM band and press enter key to proceed further.
Loragatewayimage 5.png

Step 4. Select EU863_870_1 and and press enter key to proceed further.
Loragatewayimage 6.png

Step 5. Wait to complete the frequency configuration.
Loragatewayimage 7.png

Step 6. Frequency channel details will be displayed. Press enter key to proceed further.
Loragatewayimage 8a.png

Step 7. If frequency configuration is correct then select Yes and press enter key to proceed further else select No and press enter key to redo the frequency configuration.
Loragatewayimage 9.png

Step 8. Please wait to complete the Frequency configuration. Once it completes then press enter key to proceed with next step.
Loragatewayimage 10.png

6.2. Gateway ID configuration[edit source]

Step 1. Select Gateway ID Configuration from the menu and press enter key to proceed with next step.
Loragatewayimage 11a.png

Step 2. You have the option to enter the Gateway EUI either in auto or manual mode . In the auto configuration mode it will use mac id to generate the gateway eui. Follow steps 3a-3b to select auto configuration mode and steps 4a-4d to configure the eui in manual mode

Step 3a. Select the auto configuration mode and press enter key.
Loragatewayimage 12.png

Step 3b. Gateway eui will be displayed on the screen. Please store the gateway eui for later use. Press enter key to move to next step.
Loragatewayimage 13.png

Step 4a. Select the Manual configuration mode and press enter key.
Loragatewayimage 12a.png

Step 4b. Enter the gateway eui and press enter key to continue further.
Loragatewayimage 13a.png

Step 4c. Message will be displayed to show the entered value of gateway eui. If it is correct then select yes and press enter key to continue further. Otherwise select No and press enter key to change value.
Loragatewayimage 13b.png

Step 4d. Gateway id configured message will appear on the screen. Press enter key to move to next configuration.
Loragatewayimage 13c.png.

6.3. Server address and port configuration[edit source]

Step 1. Now we have to configure the server details. Select server configuration and press enter key to proceed further.
Loragatewayimage 14a.png

Step 2. You can use either TTN or loriot as network server. Refer the respective options for configuration.

6.3.1. Loriot server configuration[edit source]

Step 1. Enter the loriot server address as per the region.
server address ---> ap3.loriot.io
port up --->1780
port down --->1780

Step 2. To modify the server host name, please select hostname and press enter key.
Loragatewayimage 15.png

Step 3. Enter the server address as ap3.loriot.io and then press enter key.
Loragatewayimage 15bal.png

Step 4. If the displayed value of hostname is correct then press enter key, otherwise select and press enter key to modify the value.
Loragatewayimage 15cal.png

Step 5. confirmation message will be displayed. press enter key to proceed further.
Loragatewayimage 15dal.png

Step 6. To modify the port up value , please select server port up and press enter key.
Loragatewayimage 15eal.png

Step 7. Enter the port up value as 1780 and then press enter key.
Loragatewayimage 15fl.png

Step 8. If the displayed value of server port up is correct then press enter key else select back and press enter key to modify the value.
Loragatewayimage 15gl.png

Step 9. confirmation message will be displayed. press enter key to proceed further.
Loragatewayimage 15hl.png

Step 10. To modify the port down value, select server port down and press enter key.
Loragatewayimage 15ial.png

Step 11. Enter the port down value as 1780 and then press enter key.
Loragatewayimage 15jl.png

Step 12. If the displayed value of server port down is correct then press enter key else select back and press enter key to modify the value.
Loragatewayimage 15kl.png

Step 13. Confirmation message will be displayed. press enter key to proceed further.
Loragatewayimage 15ll.png

Step 14. ChirpStack hostname, port up/down is configured . Select back and press enter key to proceed further.
Loragatewayimage 15ml.png

6.3.2. Things network server(TTN) configuration[edit source]

Step 1. Enter the TTN server address as selected on the things network website .As an example server address of Australia region is as follows.
server address ---> au1.cloud.thethings.network
port up --->1700
port down --->1700

Step 2. To modify the server host name , Select hostname and press enter key.
Loragatewayimage 15.png

Step 3. Enter the server address as au1.cloud.thethings.network and then press enter key.
Loragatewayimage 15ba.png

Step 4. If the displayed value of hostname is correct then press enter key else select back and press enter key to modify the value.
Loragatewayimage 15ca.png

Step 5. confirmation message will be displayed. press enter key to proceed further.
Loragatewayimage 15da.png

Step 6. To modify the port up value, select server port up and press enter key.
Loragatewayimage 15ea.png

Step 7. Enter the port up value as 1700 and then press enter key.
Loragatewayimage 15f.png

Step 8. If the displayed value of server port up is correct then press enter key else select back and press enter key to modify the value.
Loragatewayimage 15g.png

Step 9. confirmation message will be displayed. Press enter key to proceed further.
Loragatewayimage 15h.png

Step 10. To modify the port down value, please select server port down and press enter key.
Loragatewayimage 15ia.png

Step 11. Enter the port down value as 1700 and then press enter key.
Loragatewayimage 15j.png

Step 12. If the displayed value of server port down is correct then press enter key else select back and press enter key to change the value.
Loragatewayimage 15k.png

Step 13. Confirmation message will be displayed. Press enter key to proceed further.
Loragatewayimage 15l.png

Step 14. ChirpStack hostname, port up/down is configured . Select back and press enter key to move to next step
Loragatewayimage 15m.png

6.4. Communication mode configuration[edit source]

Step 1. Select Communication mode from the menu and press enter key to proceed further.
Loragatewayimage 16a.png

Step 2. You have an option to select either lan or wlan for the communication. Follow steps 3a-3b to configure LAN and 4a-4e to select wlan mode for server communication.

Step 3a. To use lan, you have to select communication mode as lan from the menu and press enter key to proceed further.
Loragatewayimage 17.png

Step 3b. Confirmation message for lan selection will be displayed. Press enter key to proceed further to configure the database.
Loragatewayimage 17a.png

Step 4a. To use wifi, you have to select communication mode as wlan from the menu and press enter key to proceed further.
Loragatewayimage 18.png

Step 4b. Enter the ssid and press enter key to proceed further.
Loragatewayimage 19.png

Step 4c. Enter the password and press enter key to proceed further.
Loragatewayimage 20.png

Step 4d. A note for wifi will be displayed then press enter key to proceed further.
Loragatewayimage 21.png

Step 4e. Wifi selection confirmation will be appear on screen. press enter key to proceed further.
Loragatewayimage 22.png

6.5. Save lorawan gateway configuration[edit source]

Step 1. Select the start loragateway from the menu and press enter key to continue with the configuration. Passwords are now successfully modified.
Loragatewayimage 33a.png

Step 2. Wait to complete the gateway confirmation.
Loragatewayimage 34.png

Step 3.Gateway configuration done in the previous steps will be displayed. Press enter key to continue.
Loragatewayimage 35a.png

Step 4. Press enter key to proceed with selected configuration.
Loragatewayimage 36.png

Step 5. Wait for the configuration to complete.
Loragatewayimage 37.png

Step 6. Message to restart will be displayed. Press enter key to continue.
Loragatewayimage 38.png

Step 7. After the system reboots, you have to register the gateway on the TTN or Loriot as per your selection.


7. How to register Lora end node device and gateway to Loriot network server[edit source]

7.1. Loriot network server setup[edit source]

Step 1. Go to the Loriot website at www.loriot.io/ and create an account on the preferred Loriot server, such as EU1 – Frankfurt, Germany, or AP3-Mumbai, India.

Step 2 Click on "Register a new gateway" tab.
LoriotImage 2.png

Step 3. Select the base platform as "packet forwarder STM".
LoriotImage 3.png

Step 4. Enter the ethernet mac address to generate the gateway eui.
LoriotImage 4.png

Step 5.Select the region EU863-870 from the region and select channel as EU868_RX2SF9 from Add Band option .
LoriotImage 5.png

Step 6.'. Open the sample network to see the status of register gateway.
LoriotImage 5a.png


7.2. Device registration to Loriot[edit source]

Step 1. Open the Application from Loriot Dashboard and click on Sample App.
LoriotImage 6.png

Step 2. Click on Enroll device from Loriot Dashboard to enroll the device . Select the enrollment process as OTAA .
Enter the device details.
LoriotImage 7.png

Step 3. Click on Device Activity in the Loriot Dashboard to see the status.
LoriotImage 9.png

Step 4. To view the device data select "WebsocketApplication" and click on "Websocket sample by Loriot ".
LoriotImage 9a.png
LoriotImage 9b.png

7.3. Cayenne integration in Loriot[edit source]

Step 1.Go to Application in Loriot Dashboard .Click on SampleApp and then select output.
LoriotImage 10.png

Step 2. Click on "+Add new output " tab and select cayenne from output type.
LoriotImage 11.png LoriotImage 12.png

Step 3. Go to Loriot Dashboard and open the SampleApp in the Application.Copy and store the Application ID required for registration on cayenne webportal.
LoriotImage 12a.png

Step 4. Now click on "Access Tokens" in the Loriot dashboard. Copy and store the Access token required for registration on cayenne portal.
LoriotImage 12b.png

7.4. Configuration on Cayenne[edit source]

Step 1. Go to Cayenne website "https://cayenne.mydevices.com" . Click on "Add new..." tab and select "Device Widget" from the options . In the Device&Widgets.
LoriotImage 13.png

Step 2. Enter the DevEUI , Loriot server , Loriot AppID and Loriot Token . Then click on "Add device" tab.
LoriotImage 14.png

Step 3. Device data will be updated on cayenne dashboard.
LoriotImage 15.png

8. How to register the Lora end node device and gateway to the The things Network(TTN) v3 server[edit source]

8.1. The Things Network (TTN) v3 server setup[edit source]

Step 1. Open the website https://www.thethingsnetwork.org/ . First you have to create an account on TTN.
TTNImage 1.png

Step 2. Open the console to select the cluster after sign-in .
TTNImage 2.png TTNImage 3.png

Step 3. Select cluster as per your region.
TTNImage 4.png

Step 4. Click on register a gateway.
TTNImage 6.png

Step 5. Enter the Gateway ID, Gateway EUI , Gateway name , Gateway Description .
TTNImage 7a.png

Step 6. Select the frequency plan as shown in the image .Then click on Create gateway tab to register the gateway
TTNImage 8.png

Step 7. Lora gateway activity will be visible after successful registration.
TTNImage 9.png

Step 8. Now proceed with device registration as explained in the next section.

8.2. Device registration to The Things Network v3 server[edit source]

Step 1. Open the console and click on "Create an application ".
TTNImage 10.png

Step 2. Enter the Application ID, Application name and Description .Click on the tab "Create application".
TTNImage 11.png

Step 3. Click on "+ Add end device" tab to register the device.
TTNImage 12.png

Step 4. Select the end device from drop down list as shown in the image.
TTNImage 13.png

Step 5. Enter the registration data and click on "Register end device".
TTNImage 14.png

Step 6. The device activity will be visible as soon as device joins the network.

TTNImage 15.png

TTNImage 16.png

8.3. Cayenne integration in The Things Network v3[edit source]

Step 1. Select webhooks from the integration .Click on the "+ Add webbook" tab.
TTNImage 17.png

Step 2. Select Caynee from the webhook template.
TTNImage 18.png

Step 3. Enter the webhook id and click on "Create cayenne webhook" tab.
TTNImage 19.png

Step 4. Cayenne webhook will be added and its status will be updated .
TTNImage 20.png

8.4. Configuration on Cayenne[edit source]

Step 1. Go to Cayenne website "https://cayenne.mydevices.com" . Click on "Add new..." tab and select "Device Widget" from the options . In the Device&Widgets.
TTNImage 21.png

Step 2. Enter the DevEUI and click on "Add device" tab.
TTNImage 22.png

Step 3. Device data will be updated on cayenne dashboard.
TTNImage 23.png


9. How to configure Nucleo-WL55JC1 as LoRa end node device[edit source]

Step 1. Download the STM32CubeWL firmware repository from the link.
STM32CubeWL v1.20

Step 2. Import/Open the LoRaWAN_End_Node project in the STM32CubeIDE.
~\STM32Cube_FW_WL_V1.2.0\Projects\NUCLEO-WL55JC\Applications\LoRaWAN\LoRaWAN_End_Node\STM32CubeIDE
Note : Workspace is available for STM32CubeIDE , EWARM and MDK-ARM.

Step 3. Configure the EU868 region in lora_app.h file . Enable myDevices Application server as shown below.
Stm32wlimage 1.png

Step 4. Define the region in lorawan_conf.h file.
Stm32wlimage 2.png

Step 5.Open the se-identity.h file to enter the device eui , join -eui , application key etc.
These values should be unique in each device. The values shown below are only for reference.
Stm32wlimage 3.png

Step 6. Enable the generation of hex and binary file as shown below.
Stm32wlimage 4.png Stm32wlimage 5.png

Step 7. After these modification , You have to build the target . After successful build, hex file will be generated at following path.
~\STM32Cube_FW_WL_V1.2.0\Projects\NUCLEO-WL55JC\Applications\LoRaWAN\LoRaWAN_End_Node\STM32CubeIDE\Debug

Step 8. Now program the generated hex file 'LoRaWAN_End_Node.hex' in Nucleo-WL55JC1 kit using stm32cubeprogrammer.
Stm32programmer 1.png

Step 9. Reset the hardware and open the tera-term to view the debug messages . You can also verify the configured parameter in IDE with the values displayed on the screen.
TeratermImage 1.png

Step 10. Now the device is ready for registration.

10. See also[edit source]

LoRaWAN Overview

No categories assignedEdit