NAND update with customized trusted image

Revision as of 10:34, 5 January 2022 by Registered User

This article gives details about updating the bootloader objects of NAND memory, located onto STM32MP157x-EV1 (e.g.), using STM32CubeIDE.

BackToNavigationTree button.png

1. Overview[edit source]

Here is the differnt step to follow to update NAND with customized trusted image:

  • Initialize the NAND with Starter Package image thanks to STM32CubeProgrammer.
  • Build the trusted image inside STM32CubeIDE with device tree configured using embedded STM32CubeMX. For that follow explanationation given in [How to manage OpenSTLinux projects in STM32CubeIDE
  • Update STM32MP15 board; this means the STM32MP15 board is up and running with network access: target status is green.
  • Check this customization is correctly set by comparing version appearing in boot message (see chapter below).

2. Bootloader version after update with Starter Package[edit source]

Below, the bootloader version appearing in boot messages:

  • TF-A BL2 version, booting from NAND memory
NAND initial setting: TF-A BL2 version
  • U-boot version & extlinux.conf file used, booting from NAND memory
NAND initial setting: U-boot version & extlinux.conf
  • extlinux.conf content before update
NAND initial setting: extlinux.conf content

3. Customizing bootloader with STM32CubeIDE[edit source]

After compiling device tree generated by STM32CubeMX , you need to :

  • update MP15 target bootfs with new .dtb under /boot
  • and adjust /boot/nand0_extlinux/stm32mp157c-ev1_extlinux.conf in order to declare new device tree and set it as default.

This is done thanks to "Cortex-A Linux® Deployment" shortcut configuration available from Linux® project Run As... menu.

  • Linux® deployment configuration
Linux® deployment configuration


  • NAND Linux® deployment message
NAND Linux® deployment message


  • NAND Linux® device tree update
NAND Linux® device tree update


Then, select Cortex-A project and right click to get Cortex-A Bootloader Deployment shortcut.

Bootloader update shortcut


Connection is automatically set and you need to scan STM32MP15 target storage. This storage list depends on the board and on the used boot storage . Then, select:

  • the storage to update, NAND #0 here;
  • TF-A BL2 & FIP image to update from FIP_artifacts/ .


  • NAND bootloader deployment configuration
NAND Bootloader deployment configuration


  • NAND bootloader deployment message
NAND Bootloader deployment message


4. Bootloader version after customization wit STM32CubeIDE[edit source]

After the update, TF-A BL2 and U-Boot versions are modified and Linux® uses the generated device tree.
Here are the boot messages now:

  • TF-A BL2 updated version, booting from NAND memory
NAND updated TF-A BL2 version


  • U-Boot updated version & Linux® device tree, booting from NAND memory
NAND updated U-Boot version & Linux® device tree

BackToNavigationTree button.png

No categories assignedEdit