SD card update with customized trusted image

Revision as of 14:57, 1 December 2021 by Registered User

This article gives details about updating the bootloader objects of SD card memory, located onto STM32MP157x-EV1 (e.g.), using STM32CubeIDE.

BackToNavigationTree button.png

1. Overview[edit source]

Here is the process used:

  • SD card is first initialized with Starter Package image thanks to STM32CubeProgrammer.
  • The trusted image is built inside STM32CubeIDE with device tree configured using embedded STM32CubeMX.
  • Next step is to update STM32MP15 board; this means the STM32MP15 board is up and running with network access: target status is green.
  • The way to check this customization is to compare version appearing in boot message.


2. Bootloader version after update with Starter Package[edit source]

Here are the TF-A BL2, U-boot version and the used extlinux.conf file used in Starter Package.
They all appear in boot messages.

  • TF-A BL2 version, booting from SD card memory
SD-Card initial setting: TF-A BL2 version
  • U-boot version & extlinux.conf file used, booting from SD card memory
SD-Card initial setting: U-boot version & extlinux.conf
  • extlinux.conf content before update.
SD-Card initial setting: extlinux.conf content


3. Customizing bootloader with STM32CubeIDE[edit source]

First, after compiling Device Tree from STM32CubeMX we need to update MP15 target bootfs with new .dtb under /boot and adjust /boot/mmc0_extlinux/extlinux.conf. This is done thanks to Cortex-A Linux® Deployment shortcut configuration available from Linux® project Run As... .

After compiling device tree generated by STM32CubeMX we need to :

  • update MP15 target bootfs with new .dtb under /boot
  • and adjust /boot/mmc0_extlinux/extlinux.conf in order to declare new device tree and set it as default.

This is done thanks to Cortex-A Linux® Deployment shortcut configuration available from Linux® project Run As... menu.

  • Linux® deployment configuration
Linux® deployment configuration
  • SD card Linux® deployment message
Linux® deployment message
  • SD card Linux® device tree update
Linux® device tree update

Then, select Cortex-A project and right click to get Cortex-A Bootloader Deployment shortcut.

Bootloader update shortcut

Connection is automatically set and you need to scan MP15 target storage. This storage list depends on the board and on boot storage used. Then select :

  • the storage to update, SD-Card here;
  • TF-A BL2 & FIP image to update.
  • SD card bootloader deployment configuration
Bootloader deployment configuration
  • SD card bootloader deployment configuration
Bootloader deployment message


4. Bootloader version after customization wit STM32CubeIDE[edit source]

After the update, TF-A BL2 and U-Boot versions are modified and Linux® uses the generated Device Tree. Here are the boot messages now:

  • TF-A BL2 updated version, booting from SD card memory
SD-Card updated TF-A BL2
  • U-Boot updated version & Linux® device tree, booting from SD card memory
SD-Card updated U-Boot version & Linux® Device Tree


BackToNavigationTree button.png

No categories assignedEdit