Wiki archives

Revision as of 18:29, 17 June 2020 by Registered User

An ecosystem releases flow designates all the ecosystem releases which are based on the same versions of the major software components (e.g. Linux® kernel) of the OpenSTLinux distribution (see details in the below table).
Each vx flow groups together all the vx.y.z ecosystem releases, and has its own wiki.
The most recent flow is associated with the flagship wiki (whose URL is "https://wiki.st.com/stm32mpu"), while the previous flows are associated with archived wikis (whose URLs are "https://wiki.st.com/stm32mpu-vx").


This flagship wiki is for the v2 flow (v2.y.z ecosystem releases): if you discover the STM32 Arm® Cortex®-based MPUs, keep browsing this wiki that contains the latest major ecosystem release.


However, if you need information about any previous ecosystem release, browse the associated wiki thanks to the below table:

STM32 MPU wiki by ST.png

Ecosystem-v1

STM32 MPU archived wiki for the v1.y.z ecosystem releases


Wikis and software components
Wiki Major ecosystem releases Major software components (OpenSTLinux distribution)
This wiki

v2.0.0

Linux® kernel v5.4 (LTS)
U-Boot v2020.01
TF-A v2.2
OP-TEE v3.9.0
OpenEmbedded v3.1 (Dunfell)

Archived wiki for the v1 flow

v1.2.0
v1.1.0
v1.0.0

Linux® kernel v4.19 (LTS)
U-Boot v2018.11
TF-A v2.0
OP-TEE v3.3.0
OpenEmbedded v2.6 (Thud)