ImageMap

Revision as of 10:53, 15 October 2019 by Registered User

1. Usage[edit source]

The ImageMap template is used to enhance images with dynamic contents (explanations and links) using image maps (aka "clickable images"). An image map is a list of coordinates in an image, that links areas of the image to multiple destinations. In the STM32 MPU wiki, the image maps rely on:

Usage:  {{ImageMap | File:<filename>.<extension>{{!}}<options>{{!}}<caption>
        <list of coordinates> <list of explanations and links>
        }}

Where:

  • <filename>, <extension>, <options> and <caption> are defined in the images help page
  • <list of coordinates> are the coordinates of forms (rectangles, circles...) in the image
  • <list of explanations and links> are the explanations and links associated with these forms

2. Basic examples[edit source]

Example of image map
You type
{{ImageMap|File: Image_map_example.png{{!}}thumb{{!}}center{{!}}Add your text legend here
rect 160 2 248 77 [[Contributors:Fake article | Step 1 (rectangle example)]]
poly 292 228 312 187 387 188 407 229 386 271 313 269 292 228 [[Contributors:Fake article | Step 2 (Polygon example)]]
circle 47 225 44 [[Contributors:Fake article | Step 3 (circle example)]]
poly 87 155 129 105 120 96 160 93 162 130 152 125 108 180 83 159 83 160 [[Contributors:Fake article | Arrows (multiple polygons example)]]
poly 137 225 162 199 163 212 253 212 252 243 163 242 163 253 137 225 [[Contributors:Fake article | Arrows (multiple polygons example)]]
poly 261 110 300 162 294 167 290 168 330 176 334 140 334 137 325 144 283 88 259 106 [[Contributors:Fake article | Arrows (multiple polygons example)]]
}}
You get
Step 1 (rectangle example)Step 2 (Polygon example)Step 3 (circle example)Arrows (multiple polygons example)Arrows (multiple polygons example)Arrows (multiple polygons example)
Add your text legend here
Info white.png Information
  • Areas which overlap give precedence to the first link listed: this gives the possibilities to create links on boxes that are drawn inside a bigger one, declaring the biggest box at the end of the list
  • Do not use <br>, but <br/> in image maps

3. References[edit source]

4. Code[edit source]

Error: Must specify an image in the first line.

No categories assignedEdit